powered by CADENAS

Social Share

Amazon

Autotrax (5683 views - EDA & PCB (Electronics))

AutoTRAX is the name of one of the first ever professional printed circuit board CAD apps available for personal computers. It ran on DOS on an IBM or compatible PC. AutoTRAX was sold widely throughout the world in the mid 1980s and early 1990s until Protel International Pty. Ltd. (the proprietor) ported the app to Windows 3.1 to create the first Windows-based PCB CAD tool, Protel 1.0 for Windows. Since then Protel International became Altium Ltd. after a successful IPO and later on made AutoTRAX a freeware download on their web site. It will run in a DOS window under Windows 9x and Windows NT up to XP. It does not run on Windows Vista and later, but can be run successfully using generic VESA video drivers in a DOS virtual machine.
Go to Article

Autotrax

Autotrax

Protel AutoTRAX
AutoTRAX freeware versions 1.61ND running in a VM on Windows 7
Original author(s) Protel International Pty. Ltd. (now Altium Ltd.)
Stable release
1.61
Development status Historical
Operating system DOS
Platform IBM PC and compatible
Type EDA
License Commercial proprietary software
Website techdocs.altium.com/display/ALEG/Legacy+Downloads

AutoTRAX is the name of one of the first ever professional printed circuit board CAD apps available for personal computers. It ran on DOS on an IBM or compatible PC. AutoTRAX was sold widely throughout the world in the mid 1980s and early 1990s until Protel International Pty. Ltd. (the proprietor) ported the app to Windows 3.1 to create the first Windows-based PCB CAD tool, Protel 1.0 for Windows. Since then Protel International became Altium Ltd. after a successful IPO and later on made AutoTRAX a freeware download on their web site.

It will run in a DOS window under Windows 9x and Windows NT up to XP. It does not run on Windows Vista and later, but can be run successfully using generic VESA video drivers in a DOS virtual machine.



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

EDA & PCB (Electronics)

Electronics, Electro, EDA, PCB, Circuit, Schematics