powered by CADENAS

Social Share

Cunife (13971 views - Material Database)

Cunife is an alloy of copper (Cu), nickel (Ni), iron (Fe), and in some cases cobalt (Co). The alloy has the same linear coefficient of expansion as certain types of glass, and thus makes an ideal material for the lead out wires in light bulbs and thermionic valves. Fernico exhibits a similar property. It is a magnetic alloy and can be used for making magnets. Cunife has a magnetic coercivity of several hundred oersteds. Unlike most high coercivity magnetic materials which are hard and brittle and need to be cast into shape, cunife can be drawn into thin wires. Wires as thin as five thou can be produced this way. Cunife 1 consists of 60% Cu, 20% Ni, and 20% Fe. Cunife 2 consists of 60% Cu, 20% Ni, 17.5% Fe, and 2.5% Co. At one point Fender Musical Instruments Corporation used Cunife magnets in their Wide-Range humbucking pickups, however discontinued use, due to Cunife being hard to source.
Go to Article

Cunife

Cunife

Cunife is an alloy of copper (Cu), nickel (Ni), iron (Fe), and in some cases cobalt (Co). The alloy has the same linear coefficient of expansion as certain types of glass, and thus makes an ideal material for the lead out wires in light bulbs and thermionic valves. Fernico exhibits a similar property. It is a magnetic alloy and can be used for making magnets.

Cunife has a magnetic coercivity of several hundred oersteds. Unlike most high coercivity magnetic materials which are hard and brittle and need to be cast into shape, cunife can be drawn into thin wires. Wires as thin as five thou can be produced this way.[1]


  • Cunife 1 consists of 60% Cu, 20% Ni, and 20% Fe.
  • Cunife 2 consists of 60% Cu, 20% Ni, 17.5% Fe, and 2.5% Co.

At one point Fender Musical Instruments Corporation used Cunife magnets in their Wide-Range humbucking pickups, however discontinued use, due to Cunife being hard to source.[citation needed]

  1. ^ Irvin L. Cooter, Robert E. Mundy, "Cunife wire magnets of small size", Journal of Research of the National Bureau of Standards, vol. 59, no. 6, pp. 379-382, December 1957.

АльникоАлюминийАлюминиевые сплавыАлюминиевая бронзаAluminium-lithium alloyArsenical bronzeArsenical copperBell metalБериллийBeryllium copperБиллонBirmabrightBismanolВисмутЛатуньБронзаCalamine brassChinese silverХромChromium hydrideКобальтКонстантанМедьГидрид меди(I)Copper–tungstenCorinthian bronzeДюралюминийDutch metalFlorentine bronzeГаллийGilding metalСтеклоGlucydurЗолотоGuanín (bronze)GunmetalHiduminiumHydronaliumИндийЖелезоItalmaСвинецMagnaliumМагнийMegalliumMercuryMuntz metalНихромНикельOrmoluPhosphor bronzePinchbeck (alloy)ПластмассыPlexiglasПлутонийКалийРодийСплав РозеСамарийСкандийСереброНатрийSpeculum metalНержавеющая стальСтальСтеллитКонструкционная стальОловоТитан (элемент)ТомпакУран (элемент)VitalliumСплав ВудаY alloyЦинкЦирконийМедно-никелевый сплавСплавы для тарелокСплав ДевардаЭлектрумHepatizonМанганинМельхиор (сплав)НейзильберMolybdochalkosСеверное золотоСякудоТумбагаAlGaGalfenolГалинстанЦветное золотоRhoditeCrown goldЭлинварField's metalПлатинитФерросплавыФерроцерийФеррохромФерромарганецФерромолибденФерросилицийФерротитанFerrouraniumИнварЧугунIron–hydrogen alloyПередельный чугунФехральКоварStaballoySpiegeleisenБулат (металл)Crucible steel41xx steelДамасская стальСталь ГадфильдаБыстрорежущая стальMushet steelMaraging steelHigh-strength low-alloy steelReynolds 531Электротехническая стальПружинная стальAL-6XNCelestriumAlloy 20Нержавеющая сталь AISI 316Martensitic stainless steelSanicro 28Surgical stainless steelZeron 100Серебрянка (сталь)Инструментальная стальСталь кортеновскаяWootz steelПрипойTerneType metalЭлектрон (сплав)АмальгамаMagnox (alloy)АлюмельBrightrayХромельHaynes InternationalИнконельМонель-металлNicrosilNisilНитинолМю-металлПермаллойСупермаллойNickel hydridePlutonium–gallium alloyНатрий-калиевый сплавМишметаллЛитийTerfenol-DPseudo palladiumScandium hydrideSamarium–cobalt magnetArgentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichiСтерлинг (сплав)Tibetan silverTitanium Beta CTitanium alloyГидрид титана(II)Gum metalTitanium goldНитрид титанаБаббитБританийПьютерQueen's metalWhite metalUranium hydrideZAMAKZirconium hydrideВодородГелийБор (элемент)АзотКислородФторМетанАнтресольАтом

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification