powered by CADENAS

Social Share

Amazon

Outdoor gym (3253 views - Sports List)

The outdoor gym is a gym built outside in a public park, with the all-weather construction of its exercise machines somewhat modeled on playground equipment. It is similar to the 1960s–1970s proliferation of fitness trails, which continue to be created particularly in the USA and Europe. In some instances, trails used for fitness are referred to as outdoor gyms.
Go to Article

Explanation by Hotspot Model

Youtube


    

Outdoor gym

Outdoor gym

The outdoor gym is a gym built outside in a public park, with the all-weather construction of its exercise machines somewhat modeled on playground equipment. It is similar to the 1960s–1970s proliferation of fitness trails, which continue to be created particularly in the USA and Europe. In some instances, trails used for fitness are referred to as outdoor gyms.[1]

Types of outdoor gym equipment

Types of outdoor gym equipment may vary according to the nature of parks, locality and the visitors. There is no fixed list as which can include all of the machines or fixtures used in different parts of the world for outdoor recreation. These fixtures or machines can also be categorized into strength training and simple fitness or resistance training. Some basic outdoor exercising installations used commonly all over the world are pullup bars, balancing beams, parallel dip bars, etc.[2]

By country

China

Outdoor gyms have been used in China as a national fitness campaign prior to the 2008 Summer Olympics.[3] The government has rolled out over 20,000,000 square metres (220,000,000 sq ft) of outdoor gymnasiums across China[3] Currently a third of the sports lottery is dedicated to funding this concept.[citation needed] In China they have a similar survey to the Active People Survey. The participation levels in physical activity have been steadily on the increase since the outdoor gym concept has been introduced to China.[citation needed].

India

Outdoor gyms are starting to trend in New Delhi, India, where traditional gyms have had low popularity. In 2012 the New Delhi Municipal Council (NDMC) installed 40 sets around the area, surrounding municipalities have followed suit.

United Kingdom

Since 2007, outdoor gyms have become increasingly common in the United Kingdom, where they are usually installed in public parks and school playgrounds.[4][5]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia