powered by CADENAS

Social Share

Amazon

Circuit design (12700 views - Electrical Engineering)

The process of circuit design can cover systems ranging from complex electronic systems all the way down to the individual transistors within an integrated circuit. For simple circuits the design process can often be done by one person without needing a planned or structured design process, but for more complex designs, teams of designers following a systematic approach with intelligently guided computer simulation are becoming increasingly common. In integrated circuit design automation, the term "circuit design" often refers to the step of the design cycle which outputs the schematics of the integrated circuit. Typically this is the step between logic design and physical design.
Go to Article

Explanation by Hotspot Model

Youtube


    

Circuit design

Circuit design

The process of circuit design can cover systems ranging from complex electronic systems all the way down to the individual transistors within an integrated circuit. For simple circuits the design process can often be done by one person without needing a planned or structured design process, but for more complex designs, teams of designers following a systematic approach with intelligently guided computer simulation are becoming increasingly common. In integrated circuit design automation, the term "circuit design" often refers to the step of the design cycle which outputs the schematics of the integrated circuit. Typically this is the step between logic design and physical design.[1]

Process

Formal circuit design usually involves a number of stages. Sometimes, a design specification is written after liaising with the customer. A technical proposal may be written to meet the requirements of the customer specification. The next stage involves synthesising on paper a schematic circuit diagram, an abstract electrical or electronic circuit that will meet the specifications. A calculation of the component values to meet the operating specifications under specified conditions should be made. Simulations may be performed to verify the correctness of the design.

A breadboard or other prototype version of the design for testing against specification may be built. It may involve the making of any alterations to the circuit to achieve compliance. A choice as to a method of construction as well as all the parts and materials to be used must be made. There is a presentation of component and layout information to draughtspersons, and layout and mechanical engineers, for prototype production. This is followed by the testing or type-testing a number of prototypes to ensure compliance with customer requirements. Usually there is a signing and approval of the final manufacturing drawings and there may be post-design services (obsolescence of components etc.).

Specification

The process of circuit design begins with the specification, which states the functionality that the finished design must provide, but does not indicate how it is to be achieved .[2] The initial specification is basically a technically detailed description of what the customer wants the finished circuit to achieve and can include a variety of electrical requirements, such as what signals the circuit will receive, what signals it must output, what power supplies are available and how much power it is permitted to consume. The specification can (and normally does) also set some of the physical parameters that the design must meet, such as size, weight, moisture resistance, temperature range, thermal output, vibration tolerance and acceleration tolerance.[3]

As the design process progresses the designer(s) will frequently return to the specification and alter it to take account of the progress of the design. This can involve tightening specifications that the customer has supplied, and adding tests that the circuit must pass in order to be accepted. These additional specifications will often be used in the verification of a design. Changes that conflict with or modify the customer's original specifications will almost always have to be approved by the customer before they can be acted upon.

Correctly identifying the customer needs can avoid a condition known as 'design creep' which occurs in the absence of realistic initial expectations, and later by failing to communicate fully with the client during the design process. It can be defined in terms of its results; "at one extreme is a circuit with more functionality than necessary, and at the other is a circuit having an incorrect functionality".[4][who?] Nevertheless, some changes can be expected and it is good practice to keep options open for as long as possible because it's easier to remove spare elements from the circuit later on than it is to put them in.

Design

The design process involves moving from the specification at the start, to a plan that contains all the information needed to be physically constructed at the end, this normally happens by passing through a number of stages, although in very simple circuit it may be done in a single step.[5] The process normally begins with the conversion of the specification into a block diagram of the various functions that the circuit must perform, at this stage the contents of each block are not considered, only what each block must do, this is sometimes referred to as a "black box" design. This approach allows the possibly very complicated task to be broken into smaller tasks which may either by tackled in sequence or divided amongst members of a design team.

Each block is then considered in more detail, still at an abstract stage, but with a lot more focus on the details of the electrical functions to be provided. At this or later stages it is common to require a large amount of research or mathematical modeling into what is and is not feasible to achieve.[6] The results of this research may be fed back into earlier stages of the design process, for example if it turns out one of the blocks cannot be designed within the parameters set for it, it may be necessary to alter other blocks instead. At this point it is also common to start considering both how to demonstrate that the design does meet the specifications, and how it is to be tested ( which can include self diagnostic tools ).[7]

Finally the individual circuit components are chosen to carry out each function in the overall design, at this stage the physical layout and electrical connections of each component are also decided, this layout commonly taking the form of artwork for the production of a printed circuit board or Integrated circuit. This stage is typically extremely time consuming because of the vast array of choices available. A practical constraint on the design at this stage is that of standardization, while a certain value of component may be calculated for use in some location in a circuit, if that value cannot be purchased from a supplier, then the problem has still not been solved. To avoid this a certain amount of 'catalog engineering' can be applied to solve the more mundane tasks within an overall design.

One area of rapid technology development is in the field of nanoelectronic circuit design.[8]

Costs

Proper design philosophy and structure incorporates economic and technical considerations and keeps them in balance at all times, and right from the start. Balance is the key concept here; just as many delays and pitfalls can come from ill-considered cost cutting as with cost overruns. Good accounting tools (and a design culture that fosters their use) is imperative for a successful project. "Manufacturing costs shrink as design costs soar," is often quoted as a truism in circuit design, particularly for ICs.

Verification and testing

Once a circuit has been designed, it must be both verified and tested. Verification is the process of going through each stage of a design and ensuring that it will do what the specification requires it to do. This is frequently a highly mathematical process and can involve large-scale computer simulations of the design. In any complicated design it is very likely that problems will be found at this stage and may involve a large amount of the design work be redone in order to fix them.

Testing is the real-world counterpart to verification, testing involves physically building at least a prototype of the design and then (in combination with the test procedures in the specification or added to it) checking the circuit really does do what it was designed to.

Prototyping

Prototyping is a means of exploring ideas before an investment is made in them. Depending on the scope of the prototype and the level of detail required, prototypes can be built at any time during the project. Sometimes they are created early in the project, during the planning and specification phase, commonly using a process known as breadboarding; that's when the need for exploration is greatest, and when the time investment needed is most viable. Later in the cycle packaging mock-ups are used to explore appearance and usability, and occasionally a circuit will need to be modified to take these factors into account.

Results

As circuit design is the process of working out the physical form that an electronic circuit will take, the result of the circuit design process is the instructions on how to construct the physical electronic circuit. This will normally take the form of blueprints describing the size, shape, connectors, etc., in use, and artwork or CAM file for manufacturing a printed circuit board or integrated circuit.

Documentation

Any commercial design will normally also include an element of documentation, the precise nature of this documentation will vary according to the size and complexity of the circuit as well as the country in which it is to be used. As a bare minimum the documentation will normally include at least the specification and testing procedures for the design and a statement of compliance with current regulations. In the EU this last item will normally take the form of a CE Declaration listing the European directives complied with and naming an individual responsible for compliance.[9]

Software

See also


Element wykonawczyAdjustable-speed driveAlternatorAlternator (automotive)Klasa ochronnościAutomotive batteryBateria ogniwSzynoprzewódCable reelCamlock (electrical)Controller Area NetworkCapacitive displacement sensorWyłącznik instalacyjnyCompact controllerPamięć komputerowaStycznikUkład regulacji (automatyka)ControlNetCorn PopperCurrent sensorTurbina DarrieusaSilnik prądu stałegoDigital sensorsElectric boilerŁadunek elektrycznyPrąd elektrycznyPrądnicaLampa elektrycznaSieć elektroenergetyczna rozdzielczaPojazd elektrycznyKabel elektrycznyZłącze (elektronika)Energia elektrycznaObwód elektrycznyLicznik energii elektrycznejElektrodaPole elektromagnetyczneElectronic symbolEnclosure (electrical)End terminalEthernet PowerlinkEtherNet/IPFerrite beadFischer ConnectorsBezpiecznik elektrycznyKontrolowana synteza termojądrowaGround lift plugRadiatorHipotHuawei AscendiMacImpellerInduction forgingPiec indukcyjnyInduction heaterInduction heatingInductive chargingIndustrial EthernetINTERBUSiOSiPhone 5SiPhone 6iPhone XIroningPuszka elektroinstalacyjnaKinetic inductance detectorSkaning laserowySilnik liniowyMegatronMEMS magnetic field sensorMikrofonMobile phone accessoriesPłyta głównaMotor controllerKamera filmowaMTConnectMultiprocessingNanomotorNanosensorLampa neonowaNeon lightingJack (wtyczka)FotodetektorCzujnik fotoelektrycznyFalownikProfibusPush-buttonU (jednostka długości)RadiostacjaRazer PhoneAkumulator elektrycznyKontaktronPrzekaźnikInżynieria odwrotnaRing main unitRobotykaRotary actuatorRotary switchWirnikSamsung Galaxy Core PrimeSCARAScrew terminalCzujnikSeparator (electricity)Servo driveServomotorSiemensTelewizja hybrydowaSmartfonLutownicaSpark-ignition engineSilnik krokowyStereo displayRozdzielnica elektrycznaSystem busTablet (komputer)Telecommunications engineeringTelegrafiaZłączka elektrycznaTransformator TesliTransformatorTurbine bladeUHF connectorVariable reluctance sensorVariable-frequency driveVirtual reality headsetWater heatingWi-FiWind turbine designZTE BladeZX-81Telecommunication circuitElement grzejnyDesignAmperomierzAmper

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electrical Engineering

EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced