powered by CADENAS

Social Share

Amazon

Fishing bait (3782 views - Sports List)

Fishing bait is any substance used to attract and catch fish, e.g. on the end of a fishing hook, or inside a fish trap. Traditionally, nightcrawlers, insects, and smaller bait fish have been used for this purpose. Fishermen have also begun using plastic bait and more recently, electronic lures, to attract fish. Studies show that natural baits like croaker and shrimp are more recognized by the fish and are more readily accepted. Which of the various techniques a fisher may choose is dictated mainly by the target species and by its habitat. Bait can be separated into two main categories: artificial baits and natural baits.
Go to Article

Explanation by Hotspot Model

Fishing bait

Fishing bait

Fishing bait

Fishing bait is any substance used to attract and catch fish, e.g. on the end of a fishing hook, or inside a fish trap. Traditionally, nightcrawlers, insects, and smaller bait fish have been used for this purpose. Fishermen have also begun using plastic bait and more recently, electronic lures, to attract fish.

Studies show that natural baits like croaker and shrimp are more recognized by the fish and are more readily accepted.[1] Which of the various techniques a fisher may choose is dictated mainly by the target species and by its habitat. Bait can be separated into two main categories: artificial baits and natural baits.

Artificial baits

Using lures is a popular method for catching predatory fish. Lures are artificial baits designed to resemble the appearance and movement of prey, usually small fish. The lure may require a specialised presentation to impart an enticing action as, for example, in fly fishing. A common way to fish a soft plastic worm is the Texas rig.

Natural baits

The rat-tailed maggot is a popular fish bait.

The natural bait angler, with few exceptions, will use a common prey species of the fish as an attractant. The natural bait used may be alive or dead. Common natural baits include worms, leeches (notably bait-leech Nephelopsis obscura), minnows, frogs, salamanders, and insects. Natural baits are effective due to the lifelike texture, odour and colour of the bait presented. Cheese has been known to be a very successful bait due to its strong smell and light colours.

Worms

The common earthworm is a universal bait for fresh water angling. Grubs and maggots are also excellent bait when trout fishing. Grasshoppers, bees and even ants are also used as bait for trout in their season, although many anglers believe that trout or salmon and many other fresh water fish roe is superior to any other bait. In lakes in southern climates such as Florida, United States, fish such as bream will take bread bait. Bread bait is a small amount of bread, often moistened by saliva, balled up to a small size that is bite size to a small fish.

Most common earthworm species, such as Lumbricus terrestris, which can often be dug up in the garden, are eminently suitable for freshwater fishing. However, on a commercial scale they are not really candidates for worm farming for providing fishing bait. The greyish brown common earthworms are deep burrowing (anecic) and do not readily breed in the shallow worm farm bins. The red compost worms, such as the well known red wiggler or the European nightcrawler, are better candidates, as they are epigeic, or surface dwellers. This is the reason that red worms are more usually available commercially for bait worms. Their natural home is just below the surface in rotting leaves, dung heaps and other plant litter. They are called detritivourous because they eat detritus (waste material).

The larger species, the European nightcrawler is much sought after for fishing bait as it tolerates near freezing water and is one of the few earthworms suitable for salt-water fishing. These worms can grow up to 7 inches (18 cm) in length, but usually are between 3 and 4 inches (7–10 cm) long. Worm farmers also offer other worm species for bait, depending on availability, which usually depends on the prevalent climatic conditions.[2]

Spreading disease

The capture, transportation and culture of bait fish can spread damaging organisms between ecosystems, endangering them. In 2007, several American states enacted regulations designed to slow the spread of fish diseases, including viral hemorrhagic septicemia, by bait fish.[3] Because of the risk of transmitting Myxobolus cerebralis (whirling disease), trout and salmon should not be used as bait.

Anglers may increase the possibility of contamination by emptying bait buckets into fishing venues and collecting or using bait improperly. The transportation of fish from one location to another can break the law and cause the introduction of fish alien to the ecosystem.

Gallery

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia