powered by CADENAS

Social Share

Amazon

Bench (weight training) (4602 views - Sports List)

A weight training bench is a piece of equipment that has a resemblance to a normal (e.g. park) bench, but is designed for use in weight training. Weight training benches may be of various designs: fixed horizontal, fixed inclined, fixed in a folded position, with one adjustable portion, with two or more adjustable portions, with racks to hold bars, etc. In the limit, the definition of a bench blurs into that of combinations that mix a bench and associated equipment. Benches are manufactured by many different vendors, in an array of qualities, features, and prices.
Go to Article

Explanation by Hotspot Model

Bench (weight training)

Bench (weight training)

Bench (weight training)

Licensed under Creative Commons Attribution-Share Alike 3.0 (No machine-readable author provided. Amcbride~commonswiki assumed (based on copyright claims).).

A weight training bench is a piece of equipment that has a resemblance to a normal (e.g. park) bench, but is designed for use in weight training.

Weight training benches may be of various designs: fixed horizontal, fixed inclined, fixed in a folded position, with one adjustable portion, with two or more adjustable portions, with racks to hold bars, etc. In the limit, the definition of a bench blurs into that of combinations that mix a bench and associated equipment.

Benches are manufactured by many different vendors, in an array of qualities, features, and prices.

Alternatives

Though the weight bench seems to define weight training for modern audiences, benches are not strictly necessary for many, if not most, exercises that typically use them. For example, seated presses may be done while standing. In recent years, many home fitness enthusiasts have begun incorporating a swiss ball into their workouts in place of a traditional bench, since it is both more space-efficient and requires engagement of the core abdominal muscles. This substitution is not without criticism, since it can be difficult to maintain form and balance when lifting more than one's own body weight.

Before the invention of the weight bench the common way to work the chest was to lie on the floor and do what was known as the floor or supine press.[citation needed]

Types of Weight Bench

There are 6 different types of weight benches available.

Flat Bench

These are the most common and most popular types of benches. These are the flat benches that don’t have any attachments. The main muscle being worked is the chest, and the secondary muscles being used are the triceps and the shoulders.

Adjustable Weight Bench

An adjustable bench is flexible and allows you to do a whole lot of exercises by adjusting the bench as per need. It can lie flat, can be inclined or declined

Olympic Weight Bench

Olympic benches are professional advance level benches that are wider and longer.

Olympic benches are not simple benches rather they have several additional equipment added to them such as squat rack, weight plates, rod, dumbbells and more. It is a complete workout machine that allows you to do some advance exercises such as squats, quad exercises, bench press and more.

Folding Weight Bench

Not all the benches can be folded. If you are in need of a weight bench that can be folded and carried easily anywhere, you should go for a folding one. These benches are not feature-rich as they have to fold so these are either flat or adjustable benches.

Abdominal Bench

It is a bench that is specifically made for performing ab exercises. The position of these benches can be either flat, incline or decline. These benches have foot rollers that are used to lock the feet thus protecting the exerciser.

Preacher Curl Bench[edit]

It is a bench that’s made for doing preacher curls specifically. Which are mainly used to work the peak of your biceps.



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia