Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Tystephens).
Developer(s) | WestDev Ltd. |
---|---|
Initial release | 2001 (2001) |
Stable release |
9.0
|
Operating system | Windows |
Type | Electronic design automation |
Licence | Proprietary |
Website |
www |
Pulsonix is an electronic design automation (EDA) software suite for schematic capture and PCB design. It is produced by WestDev, which is headquartered in Gloucestershire, England, with additional sales and distribution offices overseas. It was first released in 2001, and runs on Windows.
British software house WestDev created electronic design automation (EDA) software Pulsonix in 2001. Development team members had formerly worked at Racal–Redac on computer-aided design tools. A key aim of the developers was that the software be easy to use, without the need for extensive training that they believed existing EDA products at that time required.[1][2]
The software formed part of the €14 million euros EU-funded project "HERMES". The three-year project (2008–11) sought to embed components within a circuit board's inner layers, to minimize use of design space.[3][4]
Traditionally, wire leads of components were inserted through holes in a circuit board then soldered in place; more recently, components and chips are surface-mounted flush with the board and heat-set. Although the concept of embedding components directly within layers of a circuit board itself had existed for some time, technical difficulties meant it was experimental, unsuited for use in mass production.
An increased demand for miniaturization, for products such as smartphones or medical devices that have to be swallowed to explore inside the body, led the EU to create the three-year project to develop embedding for "industrialization" (mass production use).[4] No EDA software was suitable for embedding. The taskforce working on HERMES approached the "most important EDA tool suppliers and convinced them to support [the project]". Pulsonix was one of those contacted, the others being Cadence, Mentor Graphics, and Zuken.[3][5]
Pulsonix is a Windows application for schematic capture and PCB layout design. It is produced in three variants, from 1000 pins up to an unlimited component pins version suited to larger designs.[6] All three have autorouter capability.[7] Within a dual monitor setup, schematic and layout design processes can each be assigned to a single screen, with changes synchronized as needed.[8]
Schematic capture layout functionality, including:
Chris Anderson, then Wired editor-in-chief, gave it a generally positive review, at DIY Drones – an online portal for unmanned aerial vehicle ("drones") enthusiasts, in which he praised its user interface plus range of features such as 3D views, and, while noting it is an expensive product, deemed it "the best competitor to the aging Cadsoft Eagle" software.[12]
Neil Gruending, columnist at long-running electronics magazine Elektor, on board design among the maker subculture, reviewed around seven EDA products on his blog in late 2012. Gruending found Pulsonix's user interface straightforward, singling out how "copper pours work properly" for praise. He considered for range of features and cost, its closest relation was Altium. Contrasting the two products Gruending wrote Pulsonix had comparatively low market share in North America, though he found support from vendors significantly better for Pulsonix there.
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Electronics, Electro, EDA, PCB, Circuit, Schematics