powered by CADENAS

Social Share

Soccer-specific stadium (7602 views - Sports List)

Soccer-specific stadium is a term used mainly in the United States and Canada, to refer to a sports stadium either purpose-built or fundamentally redesigned for soccer and whose primary function is to host soccer matches, as opposed to a multipurpose stadium which is for a variety of sports. A soccer-specific stadium may host other sporting events (such as lacrosse, American football and rugby) and concerts, but the design and purpose of a soccer-specific stadium is primarily for soccer. Some facilities (for example Toyota Park, Toyota Stadium and Mapfre Stadium) have a permanent stage at one end of the stadium used for staging concerts. A soccer-specific stadium typically has amenities, dimensions and scale suitable for soccer in North America, including a scoreboard, video screen, luxury suites and possibly a roof. The field dimensions are within the range found optimal by FIFA: 110–120 yards (100–110 m) long by 70–80 yards (64–73 m) wide. These soccer field dimensions are wider than the regulation American football field width of 53 1⁄3 yards (48.8 m), or the 65-yard (59 m) width of a Canadian football field. The playing surface typically consists of grass as opposed to artificial turf, since the latter is generally disfavored for soccer matches since players are more susceptible to injuries. However, some soccer specific stadiums, such as Portland's Providence Park and Creighton University's Morrison Stadium, do have artificial turf. Lastly, the seating capacity is generally small enough to provide an intimate setting, between 18,000 and 30,000 for a Major League Soccer franchise, or smaller for minor league soccer teams. This is in comparison to the much larger American football stadiums that mostly range between 60,000 and 80,000 in which the original North American Soccer League teams played at and most MLS teams participated in during the league's inception. As opposed to gridiron-style football stadiums, where the front row of seats is elevated several feet above the field of play to allow spectators to see over the heads of substitute players and coaches on the sidelines, soccer-specific venues typically have the front row closer to the level of the pitch, providing a more intimate experience.
Go to Article

Explanation by Hotspot Model

Youtube

10 Football Stadiums | Now & In The Future | Ft. Camp Nou, Türk Telekom Arena, Stamford Bridge...etc | By ZANOMG


Ft:
10. White Hart Lane - Tottenham Hotspur
9. Mestalla Stadium - Valencia CF
8. Türk Telekom Arena - Galatasaray S.K
7. Stadio Olimpico - AS Roma
6. Etihad Stadium - Manchester City
5. Vicente Calderón - Atlético Madrid
4. San Siro Stadium - AC Milan
3. Stamford Bridge - Chelsea FC
2. Camp Nou - FC Barcelona
1. Santiago Bernabéu Stadium - Real Madrid

Soccer-specific stadium

Soccer-specific stadium

Soccer-specific stadium is a term used mainly in the United States and Canada,[1] to refer to a sports stadium either purpose-built or fundamentally redesigned for soccer and whose primary function is to host soccer matches, as opposed to a multipurpose stadium which is for a variety of sports. A soccer-specific stadium may host other sporting events (such as lacrosse, American football and rugby) and concerts, but the design and purpose of a soccer-specific stadium is primarily for soccer. Some facilities (for example Toyota Park, Toyota Stadium and Mapfre Stadium) have a permanent stage at one end of the stadium used for staging concerts.

A soccer-specific stadium typically has amenities, dimensions and scale suitable for soccer in North America, including a scoreboard, video screen, luxury suites and possibly a roof. The field dimensions are within the range found optimal by FIFA: 110–120 yards (100–110 m) long by 70–80 yards (64–73 m) wide.[2] These soccer field dimensions are wider than the regulation American football field width of 53 13 yards (48.8 m), or the 65-yard (59 m) width of a Canadian football field. The playing surface typically consists of grass as opposed to artificial turf, since the latter is generally disfavored for soccer matches since players are more susceptible to injuries.[3] However, some soccer specific stadiums, such as Portland's Providence Park and Creighton University's Morrison Stadium, do have artificial turf.

Lastly, the seating capacity is generally small enough to provide an intimate setting, between 18,000 and 30,000 for a Major League Soccer franchise,[4] or smaller for minor league soccer teams. This is in comparison to the much larger American football stadiums that mostly range between 60,000 and 80,000 in which the original North American Soccer League teams played at and most MLS teams participated in during the league's inception.[5] As opposed to gridiron-style football stadiums, where the front row of seats is elevated several feet above the field of play to allow spectators to see over the heads of substitute players and coaches on the sidelines, soccer-specific venues typically have the front row closer to the level of the pitch, providing a more intimate experience.[6]

History

In the 1980s and 1990s, Division I professional soccer leagues in the United States, such as the North American Soccer League and Major League Soccer, primarily used American football fields, many of which were oversized in terms of seating capacity, undersized in terms of width of the soccer field, and often used artificial turf (none of which, at the time, were approved for international soccer under FIFA rules).[citation needed] Although many of the baseball parks had smaller capacities, natural grass and a wider field in which to place the field, these parks were generally in-use during the summer season, when North American–based soccer leagues, such as Major League Soccer, also hold their seasons, and the irregular field dimensions and sightlines were often considered undesirable.

Soccer-specific stadiums first came into use in the 1990s, after the multi-purpose stadium era.[7][8]

The term "soccer-specific stadium" was coined by Lamar Hunt, who financed the construction of the Columbus Crew Stadium, the first soccer specific stadium used in Major League Soccer.[7] In the 2000s, other Major League Soccer teams in the United States began constructing their own stadiums. Canada's first soccer-specific stadium was BMO Field in Toronto, home to Toronto FC. This stadium was renovated to accommodate Canadian football for the 2016 and subsequent seasons.[9] The distinction is less prominent in Canada, where MLS's attendance figures are comparable to those of the domestic Canadian Football League, and the CFL's wider field means fewer compromises must be made to accommodate both; Tim Hortons Field was built purposely to both soccer specifications and CFL regulations. Of the three Canadian cities that host both MLS and CFL teams, only one (Montreal) has separate stadiums for each.

Major League Soccer (MLS)

Current MLS soccer-specific stadiums

Stadium Club(s) City Capacity Opened
Avaya Stadium San Jose Earthquakes San Jose, California 18,000 2015
BBVA Compass Stadium Houston Dynamo[n 1] Houston, Texas 22,039 2012
Children's Mercy Park Sporting Kansas City Kansas City, Kansas 18,467 2011
Dick's Sporting Goods Park Colorado Rapids Commerce City, Colorado 19,680 2007
Mapfre Stadium Columbus Crew SC Columbus, Ohio 20,145 1999
Orlando City Stadium Orlando City SC[n 2] Orlando, Florida 25,500 2017
Providence Park Portland Timbers Portland, Oregon 21,144 1926
Red Bull Arena New York Red Bulls Harrison, New Jersey 25,189 2010
Rio Tinto Stadium Real Salt Lake[n 3] Sandy, Utah 20,008 2008
Saputo Stadium Montreal Impact Montreal, Quebec 20,801 2008
StubHub Center LA Galaxy[n 4] Carson, California 27,000 2003
Talen Energy Stadium Philadelphia Union Chester, Pennsylvania 18,500 2010
Toyota Park Chicago Fire[n 5] Bridgeview, Illinois 20,000 2006
Toyota Stadium FC Dallas Frisco, Texas 20,500 2005

Future MLS soccer-specific stadiums

Stadium Club(s) City Capacity Construction
began
Planned
opening
Audi Field D.C. United Washington, D.C. 20,000 2017 2018
Banc of California Stadium Los Angeles FC Los Angeles, California 22,000 2016 2018
Allianz Field Minnesota United FC Saint Paul, Minnesota 21,500 2016 2019

Proposed MLS soccer-specific stadiums

Stadium Club(s) Metro area Proposed capacity
Miami MLS stadium Miami MLS team Miami, Florida 25,000

In 2011 Bob Lenarduzzi confirmed that the Vancouver Whitecaps are now committed to BC Place, and that plans for the waterfront stadium have been put on hold.[10]

North American Soccer League (NASL)

Current NASL soccer-specific stadiums

Stadium Club(s) City Capacity Opened
Clarke Stadium FC Edmonton Edmonton, Alberta 5,000 1938
WakeMed Soccer Park North Carolina FC Cary, North Carolina 10,000 2002
Juan Ramón Loubriel Stadium Puerto Rico FC Bayamón, Puerto Rico 22,000 1974 (2012 renovation)

United Soccer League (USL)

Current USL soccer-specific stadiums

All USL teams will be required to play in self-owned, soccer-specific stadiums by the 2020 season. The following is a list of current USL stadiums that are soccer-specific stadiums:

Stadium Club(s) City Capacity Opened
MUSC Health Stadium Charleston Battery Charleston, South Carolina 5,100 1999
Mecklenburg County Sportsplex Charlotte Independence Matthews, North Carolina 2,300 2017
Weidner Field Colorado Springs Switchbacks Colorado Springs, Colorado 5,000 2002 (Renovated 2015)
StubHub Center Track and Field Stadium LA Galaxy II Carson, California 2,000 2003
MSU Soccer Park at Pittser Field New York Red Bulls II Montclair, New Jersey 3,000 1998 (Renovated 2016)
Orlando City Stadium Orlando City B Orlando, Florida 25,500 2017
Phoenix Rising FC Soccer Complex Phoenix Rising FC Scottsdale, Arizona 6,200 2017
Highmark Stadium Pittsburgh Riverhounds Pittsburgh, Pennsylvania 3,500 2013
Providence Park Portland Timbers 2 Portland, Oregon 21,144 1990
Rio Tinto Stadium Real Monarchs Sandy, Utah 20,213 2008
H-E-B Park Rio Grande Valley FC Toros Edinburg, Texas 9,400 2017
Capelli Sport Stadium Rochester Rhinos Rochester, New York 13,768 2006
Toyota Stadium Saint Louis FC Fenton, Missouri 6,200 1982
Papa Murphy's Park Sacramento Republic FC Sacramento, California 11,242 2014
Toyota Field San Antonio FC San Antonio, Texas 8,296 2013
Starfire Sports Complex Seattle Sounders 2 Tukwila, Washington 4,500 2005
Swope Soccer Village Swope Park Rangers Kansas City, Missouri 3,500 2007
Al Lang Stadium Tampa Bay Rowdies St. Petersburg, Florida 7,227 1947 (2015 renovation)
Ontario Soccer Centre Toronto FC II Vaughan, Ontario 3,500 2015

Premier Development League (PDL)

Current PDL soccer-specific stadiums

Stadium Club(s) Division City Capacity Opened
City Park Stadium Westchester Flames PDL New Rochelle, New York 1,845 1970s
Lusitano Stadium Western Mass Pioneers PDL Ludlow, Massachusetts 3,000 1918
Macpherson Stadium Carolina Dynamo PDL Browns Summit, North Carolina 1,600 2002

NCAA (Division I)

Stadium Team(s) City Capacity Opened
Albert-Daly Field William & Mary Tribe Williamsburg, Virginia 1,000 2004
Ambrose Urbanic Field Pittsburgh Panthers Pittsburgh, Pennsylvania 735 2011
Belson Stadium St. John's Red Storm Queens, New York 2,600 2001
Bill Armstrong Stadium Indiana Hoosiers Bloomington, Indiana 6,500 1981
Columbia Soccer Stadium Columbia Lions New York City, New York 3,500 1985
Dick Dlesk Soccer Stadium West Virginia Mountaineers Morgantown, West Virginia 1,600 2004
Dr. Mark & Cindy Lynn Stadium Louisville Cardinals Louisville, Kentucky 5,300 2014
Elizabeth Lyle Robbie Stadium Minnesota Golden Gophers Falcon Heights, Minnesota 1,000 1999
Ellis Field Texas A&M Aggies College Station, Texas 3,500 1994
Eugene E. Stone III Stadium South Carolina Gamecocks Columbia, South Carolina 5,000 1981
Harder Stadium UC Santa Barbara Gauchos Santa Barbara, California 17,000 1966
Hermann Stadium Saint Louis Billikens St. Louis, Missouri 6,050 1999
Hofstra University Soccer Stadium Hofstra Pride Hempstead, New York 1,600 2003
Mazzella Field Iona Gaels New Rochelle, New York 2,400 1989
Mean Green Village North Texas Mean Green Denton, Texas 1,000 2006
Mike Rose Soccer Complex Memphis Tigers Memphis, Tennessee 2,500 2001
Morrison Stadium Creighton Bluejays Omaha, Nebraska 6,000 2003
Morrone Stadium UConn Huskies Storrs, Connecticut 5,100 1969
Old Dominion Soccer Complex Old Dominion Monarchs and Lady Monarchs Norfolk, Virginia 4,000 1990
Riggs Field Clemson Tigers Clemson, South Carolina 6,500 1915
Roberts Stadium Princeton Tigers Princeton, New Jersey 2,356 2008
SU Soccer Stadium Syracuse Orange Syracuse, New York 1,500 1996
University of Denver Soccer Stadium Denver Pioneers Denver, Colorado 2,000 2009
UNCG Soccer Stadium University of North Carolina at Greensboro Greensboro, North Carolina 3,540 1990
Veterans Memorial Soccer Complex Marshall Thundering Herd Huntington, West Virginia 1,006 2013
Waipio Peninsula Soccer Stadium Hawaiʻi Rainbow Wahine Waipiʻo, Hawaii 4,500 2000
Yurcak Field Rutgers Scarlet Knights Piscataway, New Jersey 5,000 1994

Other soccer-specific stadiums

Stadium Team(s) Division City Capacity Opened
Atlanta Silverbacks Park Atlanta Silverbacks NPSL Atlanta, Georgia 5,000 2006
Fifth Third Bank Stadium Kennesaw State Owls NCAA Kennesaw, Georgia 8,300 2010
King George V Park National Stadium
Memorial Sea-Hawks
CONCACAF
CIS
St. John's, Newfoundland and Labrador 10,000 1925
Kiwanis Municipal Park Stadium Williamsburg, Virginia
Maryland SoccerPlex Washington Spirit NWSL Germantown, Maryland[n 6] 5,128 2000
Metropolitan Oval Queens, New York 1,500 1925 (2001 renovation)
Orange Beach Sportsplex Local teams Local Orange Beach, Alabama 1,500 2001
Starfire Sports Seattle Sounders FC 2
Seattle Sounders Women
USL
W-League
Tukwila, Washington 4,500 2002
Uihlein Soccer Park MSOE Raiders NCAA Milwaukee, Wisconsin 7,000 1994
Virginia Beach Sportsplex Virginia Beach, Virginia 10,500 1999
WRAL Soccer Center CASL teams CASL Raleigh, North Carolina 3,200 1990

Past soccer-specific stadiums

Stadium Club(s) City Capacity Opened Years used Status
Mark's Stadium Fall River F.C. North Tiverton, Rhode Island 15,000 1922
BMO Field Toronto FC Toronto, Ontario 30,991 2007 2007–present Changed into a multi-purpose stadium in 2016 after becoming the home of the CFL's Toronto Argonauts.

Other countries

The term "football-specific stadium" is sometimes used in countries where the sport is known as football rather than soccer,[citation needed] although the term is not common in countries where football is the dominant sport and thus football-specific stadiums are quite common. The term tends to have a slightly different meaning in these countries, usually referring to a stadium without an athletics track surrounding the field.[citation needed] Some soccer stadiums in Europe are also used for other sports, including Rugby, American Football, and Field Hockey. The problem with oversized stadiums designed for another sport is particularly visible in European American Football leagues and conflicts between teams sharing the stadium (a notable example are Eintracht Braunschweig and the Braunschweig Lions which share a stadium) and (often municipal) owners of the stadiums sometimes arise, leading to attempts at single sport-specific venues.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia