Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (No machine-readable author provided. Kim H Yusuke~commonswiki assumed (based on copyright claims).).
A retractable hardtop — also known as "coupé convertible" or "coupé cabriolet" — is a car with an automatically operated, self-storing hardtop, as opposed to the folding textile-based roof used by traditional convertible cars.
The benefits of improved climate control and security are traded off against increased mechanical complexity, cost, weight and often reduced luggage capacity.
A 2006 New York Times article suggested the retractable hardtop may herald the demise of the textile-roofed convertible,[1] and a 2007 Wall Street Journal article suggested "more and more convertibles are eschewing soft cloth tops in favor of sophisticated folding metal roofs, making them practical in all climates, year-round."[2]
1919 Ben P. Ellerbeck conceived a retractable hardtop – a manually operated system on a Hudson coupe that allowed unimpeded use of the rumble seat even with the top down[3] – but never saw production.[4]
1934 Lancia introduced the first production, power-operated retractable hardtop in 1934, the Belna Eclipse,[5][6][7] designed and patented by Georges Paulin.[1] The Belna was a French-built Lancia Augusta. The French coachbuilder, Marcel Pourtout, custom-built examples of Paulin's designs on other makes like Panhard and Peugeot 402, 401 or 601.[1]
1941 Chrysler introduced a retractable hardtop concept car, the Chrysler Thunderbolt.[3]
1953 Ford Motor Company spent an estimated US$2 million (US$18,728,856 in 2018 dollars[8]) to engineer a Continental Mark II with a servo-operated retractable roof. The project was headed by Ben Smith, a 30-year-old draftsman.[9] The concept was rejected for cost and marketing reasons.[3] Engineering work was recycled to the Ford Division which used the retractable mechanism in their 1957-1959 flagship Ford Fairlane 500 Skyliner after an estimated US$18 million (US$160,571,090 in 2018 dollars[8]) more was spent.[10]
1955 Brothers Ed and Jim Gaylord showed their first prototype at the 1955 Paris motor show,[11] but the car failed to reach production.
1957 Ford introduced the Fairlane 500 Skyliner in the United States. A total of 48,394 were built from 1957 to 1959.[3] The retractable top was noted for its complexity and usually decent reliability[12][13] in the pre-transistor era. Its mechanism contained 10 power relays, 10 limit switches, four lock motors, three drive motors, eight circuit breakers, as well as 610 feet (190 m) of electrical wire,[3] and could raise or lower the top in about 40 seconds. The Skyliner was a halo car with little luggage space (i.e., practicality), and cost twice that of a baseline Ford sedan.
1989 Toyota introduced a modern retractable hardtop, the MZ20 Soarer Aerocabin. The car featured an electric folding hardtop and was marketed as a 2-seater with a cargo area behind the front seats. Production was 500 units.
1995 The Mitsubishi GTO Spyder by ASC was marketed in the U.S.[4] The design was further popularized by such cars as the 1996 Mercedes-Benz SLK.[1] and 2001 Peugeot 206 CC.
2006 Peugeot presented a concept four-door retractable hardtop convertible, the Peugeot 407 Macarena.[14] Produced by French coachbuilding specialist Heuliez, the Macarena's top can be folded in about 30 seconds.[14] It has a reinforcing beam behind the front seats which incorporates LCD screens into the crossmember for the rear passengers.[14]
Retractable hardtops are commonly made from between two and five sections of metal or plastic and often rely on complex dual-hinged trunk/boot lids that enable the trunk lid to both receive the retracting top from the front and also receive parcels or luggage from the rear. The trunk also often includes a divider mechanism to prevent loading of luggage that would conflict with the operation of the hardtop.
The retractable hardtop's advantages include:
The retractable hardtop's disadvantages include:
Mazda Miata Power Retractable Hard Top (PRHT) c. 2007, with 77 lb (35 kg) polycarbonate hardtop and identical cargo capacity to the soft top version[15]
Cadillac XLR c. 2007, with fully retracted aluminum (i.e., lightweight) hardtop concealed by self-storing tonneau cover, the hardtop manufactured by a supplier joint venture of Mercedes-Benz and Porsche[23]
Daihatsu Copen c. 2001 with retracted hardtop, qualifying for the ultra-compact Japanese Kei class
Ford Focus CC c. 2006 with its roof retracted, its final assembly performed by Pininfarina
Chevrolet SSR c. 2004, a retractable hardtop convertible pickup truck, its top engineered by ASC
Volkswagen Eos c. 2007, the five-segment top features an independently sliding sunroof, made by OASys
Opel Astra Twintop with a three-part folding metal roof which sits in the upper half of the boot space, leaving considerable luggage space below it. Sold from 2005-2012.
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer, Bus