Studio glass is the modern use of glass as an artistic medium to produce sculptures or three-dimensional artworks. The glass objects created are intended to make a sculptural or decorative statement. Their prices may range from a few hundred to hundreds of thousands of dollars (US)[1]. For the largest installations, the prices are in the millions.[2]
During the early 20th-century (before the early 1960s), contemporary glass art was generally made by teams of factory workers, taking glass from furnaces containing a thousand or more pounds. This form of glass art, of which Tiffany and Steuben in the U.S., Gallé in France and Hoya Crystal in Japan, Royal Leerdam Crystal in the Netherlands and Orrefors and Kosta Boda in Sweden are perhaps the best known, grew out of the factory system in which all glass objects were hand or mold blown by teams.
Modern glass studios use a great variety of techniques in creating glass artworks, including:
From the 19th century, various types of fancy glass started to become significant branches of the decorative arts. Cameo glass was revived for the first time since the Romans, initially mostly used for pieces in a neo-classical style. The Art Nouveau movement in particular made great use of glass, with René Lalique, Émile Gallé, and Daum of Nancy important names in the first French wave of the movement, producing colored vases and similar pieces, often in cameo glass, and also using lustre techniques. Louis Comfort Tiffany in America specialized in secular stained glass, mostly of plant subjects, both in panels and his famous lamps. From the 20th century, some glass artists began to class themselves as sculptors working in glass and as part of the fine arts.
In the early 20th century, most glass production happened in factories. Even individual glassblowers making their own personalized designs would do their work in those large shared buildings. The idea of "art glass" grew – small decorative works in small production runs, often with designs or objects inside.
By the 1970s, there were good designs for smaller furnaces, and in the United States this gave rise to the "studio glass" movement of glassblowers, who worked outside of factories, often in their own buildings or studios. This coincided with a move towards smaller production runs of particular styles. This movement spread to other parts of the world as well.
Modern glass studios use a great variety of techniques in creating their pieces. The ancient technique of blown glass, where a glassblower works at a furnace full of molten glass using metal rods and hand tools to blow and shape almost any form of glass, is one of the more popular ways to work. Most large hollow pieces are made this way, and it allows the artist to be improvisational as they create their work.
Another type is flame-worked glass, which uses torches and kilns in its production. The artist generally works at a bench using rods and tubes of glass, shaping with hand tools to create their work. Many forms can be achieved this way with little investment into money and space. Though the artist is somewhat limited in the size of the work that can be created, a great level of detail can be achieved with this technique. The paperweights by Paul Stankard are good examples of what can be achieved with flame-working techniques. In the 21st century, flame-worked glass became commonly used as adornments on functional items. The glass conductor's baton, commissioned by Chandler Bridges for Dr. Andre Thomas, is a clear example of flame-working being used to transform a traditional item into an artistic statement.
Cast glass can be done at the furnace, at the torch or in a kiln. Generally the artist makes a mold out of refractory, sand, or plaster and silica which can be filled with either clear glass or colored or patterned glass, depending on the techniques and effects desired. Large scale sculpture is usually created this way. Slumped glass and fused glass is similar to cast glass, but it is not done at as high of a temperature. Usually the glass is only heated enough to impress a shape or a texture onto the piece, or to stick several pieces of glass together without a glue.
The traditional technique of stained glass is still employed for the creation of studio glass. The artist cuts the glass into shapes and sets the pieces into lead cames which are soldered together. They artist can also use hot techniques in a kiln to create texture, patterns, or change the overall shape of the glass.
Etched glass is created by dipping glass that has an acid resistant pattern applied to its surface into an acid solution. Also an artist can engrave it by hand using wheels. Sandblasting can create a similar effect.
Cold glass is any glass worked without the use of heat. Glass may be cut, chiseled, sandblasted, and glued or bonded to form art objects ranging from small pieces to monumental sculpture.
The international studio glass movement originated in America, spreading to Europe, the United Kingdom, Australia and Asia. The emphasis of this movement was on the artist as the designer and maker of one-of-a-kind objects, in a small studio environment. This movement enabled the sharing of technical knowledge and ideas among artists and designers that, in industry, would not be possible.[3]
With the dominance of Modernism in the arts, there was a broadening of artistic media throughout the 20th century. Indeed, glass was part of the curriculum at art schools such as the Bauhaus. Frank Lloyd Wright's produced glass windows considered by some as masterpieces not only of design, but of painterly composition as well. During the 1950s, studio ceramics and other craft media in the U.S. began to gain in popularity and importance, and American artists interested in glass looked for new paths outside industry.[3] Harvey Littleton, often referred to as the "Father of the Studio Glass Movement",[4] was inspired to develop studio glassblowing in America by the great glass being designed and made in Italy, Sweden and many other places, and by the pioneering work in ceramics of the California potter Peter Voulkos. Harvey Littleton and Dominick Labino held the now-famous glass workshop at the Toledo Museum of Art in 1962. The goal was to melt glass in a small furnace so individual artists could use glass as an art medium in a non-industrial setting. This was the workshop that would stimulate the studio glass movement that spread around the world. Instead of the large, industrial settings of the past, a glass artist could now work with a small glass furnace in an individual setting and produce art from glass.
The early glass movement (studio glass) in Australia was spurred on by a visit to Australia by American artist Bill Boysen, who toured the country in the early seventies with a mobile studio. Boysen traveled to Australia in 1974, where he promoted glass artistry by presenting a "revolutionary demonstration of glass blowing"[5] to a gathering of around 250 attendees. Boysen's mobile studio "successfully toured eight eastern states’ venues in ’74, thus greatly enhancing the credibility of hand crafted glass."[6] Boysen's visit is credited with helping "inspire a generation of [Australian] artists to work with glass and eventually led to the creation of the national glass art collection"[5] in Wagga Wagga, Australia. This important collection includes over 450 works of art and is "the most comprehensive public collection of Australian studio glass anywhere."[5] Since that time Australian glass has gained worldwide recognition with Adelaide in South Australia, hosting the International Glass Art Society Conference in 2005 on only its third occasion outside of the U.S. The Ranamok Glass Prize, presented every year from 1994 to 2014, promotes contemporary glass artists living in Australia and New Zealand.[7]
Daniël Theys en Chris Miseur from the glass factory Theys & Miseur in Kortrijk-Dutsel [nl], Belgium, which represent Belgian artistic glass work concerning the entire world.
In China, glass art first appeared in the Western Zhou period (1046–771 BC) and was called liuli. One of the oldest artifacts of Chinese liuli, a pair of burial ear cups, was retrieved from the archaeological site of Western Han Dynasty Prince Liu Sheng of Zhongshan in Hebei Province. Across thousands of years, the art gradually diminished until it was resurrected by artists Loretta H. Yang and Chang Yi in 1987 through the first contemporary Chinese liuli art studio Liuligongfang. In 1997, Yang and Chang released their technique and procedure to the public with the purpose of creating a diplomatic platform for education and advancement. The Liuligongfang technique has since become a key cornerstone upon which contemporary Chinese liuli is built with Yang and Chang widely recognized as the pioneers and founders of contemporary Chinese liuli.[citation needed]
Glass blowing began in the Roman Empire, and Italy has refined the techniques of glass blowing ever since. Until the very recent explosion of glass shops in Seattle (US), there were more on the Island of Murano (Italy) than anywhere else in world. The majority of the refined artistic techniques of glassblowing (e.g., incalmo, reticello, zanfirico, latticino) were developed there. Moreover, generations of blowers passed on their techniques to family members. Boys would begin working at the fornace (actually "furnace"—called "the factory" in English).
Japanese glass art has a short history. The first independent glass studios were built by Saburo Funakoshi and Makoto Ito, and Shinzo Kotani in separate places. Yoshihiko Takahashi and Hiroshi Yamano show their works at galleries throughout the world and are arguably Japan's glass artists of note. Yoichi Ohira has worked with great success in Murano with Italian gaffers. The small Pacific island Niijima, administered by Tokyo. has a renowned glass art center, built and run by Osamu and Yumiko Noda, graduates of Illinois State University, where they studied with Joel Philip Myers. Every autumn, the Niijima International Glass Art Festival takes place inviting top international glass artists for demonstrations and seminars. Emerging glass artists, such as Yukako Kojima and Tomoe Shizumu, were featured at the 2007 Glass Art Society exhibition space at the Pittsburgh Glass Center. Kyohei Fujita was another noteworthy Japanese studio glass artist.
Mexico was the first country in Latin America to have a glass factory in the early sixteenth century brought by the Spanish conquerors. Although traditional glass in Mexico has prevailed over modern glass art, since the 1970s there have been a List of glass artists#Mexico that have given a place to that country in international glass art.
Glass art in the Netherlands is mainly stimulated by the glass designing and glass blowing factory Royal Leerdam Crystal. Such notable designers as H.P. Berlage, Andries Copier and Sybren Valkema, Willem Heesen (Master Glassblower as well) had a major influence on Dutch glass art. Later the studio glass movement, inspired by the American Harvey Littleton and the new Workgroup Glass founded by Sybren Valkema at the Gerrit Rietveld Academy in Amsterdam led to a new generation of glass artists.
Notable centres of glass production in the UK have been St. Helens in Merseyside (the home of Pilkington Glass and the site on which lead crystal glass was first produced by George Ravenscroft), Stourbridge in the Midlands and Sunderland in the North East. Sunderland is now home to the National Glass Centre which houses a specialist glass art course. St. Helens boasts a similar establishment but without the educational body attached. Perthshire in Scotland was known internationally for its glass paperweights. It has always hosted the best glass artists working on small scales, but closed its factory in Crieff, Scotland in January 2002.
Glass artists in the UK have a variety of exhibitions. The Scottish Glass Society hosts a yearly exhibition for members, the Guild of Glass Engravers exhibit every two years and the British Glass Biennale, begun in 2004 is now opening its third show.
British Glass Art owes much to the long history of craft. The majority of its glass blowers who operate small studio furnaces produce aesthetically beautiful though primarily functional objects. Technical skill as a blower is given as much importance as the artistic intent. Other notable Glasshouse artists are Steven Newell, Catherine Hough, Annette Meech and of course Simon Moore. There are a growing number of glass studios in the UK. Many specialize in production glassware while others concentrate on one off or limited edition pieces. An Arts Council funded, non-profit making organisation, the Contemporary Glass Society, founded in 1976 as British Artists in Glass, exists to promote and support the work of glass artists in the UK.[8]
Other glass organisations in the UK are The Guild of Glass Engravers, the Scottish Glass Society and Cohesion. Cohesion is a different sort of entity to the other organisations in that it was specifically founded to promote and develop glass art as a commercial concern. It organises trade events in and around the UK and at the international level. Originally it focused only on artists based the north east of England but has since expanded its remit to cover the whole of the UK.
The Northlands Glass School was established in late 1990s in the far north of Scotland and offers residencies and masterclasses to arts students and established glass artists.
In November 2007 the glass sculpture Model for a Hotel was unveiled as an exhibit on the fourth plinth of Trafalgar Square, London.
The United States has had two phases of development in glass. The first, in the early and mid-1900s, started in the cities of Toledo, Ohio, and Corning, New York, where factories such as Fenton and Steuben were making both functional and artistic glass pieces. Toledo’s rich history in glass goes back to the turn of the century when Libbey Glass, Owens-Illinois and Johns Manville led the world in the manufacturing of glass products. Their reputations earned Toledo the title of the "Glass Capital of the World." These industry leaders, along with the Toledo Museum of Art, sponsored the first glass workshop in 1961. This workshop would lead to a new movement in American studio glass.
The American Studio Glass Movement
The second, and most prominent, phase in American glass began in 1962, when then-ceramics professor Harvey Littleton and chemist Dominick Labino began the contemporary glassblowing movement. The impetus for the movement consisted of their two workshops at the Toledo Museum of Art, during which they began experimenting with melting glass in a small furnace and creating blown glass art. Littleton and Labino were the first to make molten glass feasible for artists in private studios. Harvey Littleton extended his influence through his own important artistic contributions and through his teaching and training, including many of the most important contemporary glass artists, including Marvin Lipofsky, Sam Herman (Britain), Fritz Dreisbach and Dale Chihuly.
In 1964, Tom McGlauchlin started one of the first accredited glass programs at the University of Iowa, and Marvin Lipofsky founded the university-level glass program at the University of California at Berkeley. In 1964, Dr. Robert C. Fritz founded a university-level glass program at San Jose State University in San Jose, California. As a graduate student at the University of Wisconsin-Madison under Harvey Littleton, Bill H. Boysen built the first glass studio at Penland School of Crafts, in Penland, North Carolina, in 1965. After graduating in 1966, he started the graduate glass program at Southern Illinois University at Carbondale, Illinois. Dale Chihuly initiated the glass program at the Rhode Island School of Design in 1969. Tom McGlauchlin joined the Toledo Museum of Art as Professor and Director of Glass in conjunction with the University of Toledo's Art program in 1971.
The growth of studio glass led to the formation of glass schools and art studios located across the country. The largest concentrations of glass artists are located in Seattle, Ohio, New York, Pennsylvania and New Jersey. San Francisco, Los Angeles/Orange County and Corning, New York also have sizable concentrations of artists working in glass.
The Pilchuck Glass School near Seattle has become a mecca for glass artists from all over the world. Those who attend Pilchuck, either college students or established artists, have the opportunity to attend master classes and exchange skills and information in an environment dedicated solely to glass based arts.
Pittsburgh Glass Center in Pittsburgh has residency programs for artists working in glass, as well as a facility for artists to make use of for their works. Pittsburgh Glass Center offers classes to the public on glassblowing and many other forms of glass art. Philadelphia hosts a small array of glass studios for artists that use glass. Home to the National Liberty Museum (featuring all exhibits by international glass artists), Philadelphia hosts the non-profit P.I.P.E. program, with residencies for artists that use glass as well as metal, electroforming on glass, and bronze casting. The state of Pennsylvania has a long tradition of the production of industrial glass and its influence has quickly been absorbed by artists working in glass.
The Studio of The Corning Museum of Glass,[9] established in 1996, is an internationally renowned teaching facility in Corning, NY. Classes and workshops are held for new and experienced glassworkers and artists. The Studio’s residency program brings artists from around the world to Corning for a month to work in The Studio facilities, where they can explore and develop new glassblowing techniques or expand on their current bodies of work. Artists working in The Studio have access to the collections of The Corning Museum of Glass, and benefit from the resources of the Rakow Research Library,[10] whose holdings cover the art and history of glass and glassmaking.
Wheaton Arts and Cultural Center,[11] located in the historic glass industry capital of Millville, New Jersey, is a nonprofit art and history education center that is home to the Museum of American Glass, which houses the largest collection of American glass objects in the world. The collection includes historical glass as well as contemporary work from some of the glass world's biggest names. In addition to the museum, WheatonArts operates a world-class glass studio under the creative direction of Hank Murta Adams.[12] The Creative Glass Center of America,[13] which is funded by WheatonArts and crucial to its mission of continuing Millville's legacy in the glass world, hosts a fellowship program exclusively for up-and-coming and mid-career artists working in glass. Well-known alumnae of the CGCA fellowship include Steve Tobin (1983) Kait Rhoads (1997 and 2008), Lino Tagliapietra (1989), Beth Lipman (2001), Gregory Nangle (2006), Deborah Czeresko (2006 and 2010), Angus Powers (2003), and Stephen Paul Day (1992, 1997, 2004, and 2009).[14]
Macro detail from a glass bowl blown at The World of Glass Museum (incorporating the Pilkington Glass Museum), St. Helens, UK
Glass ball made by Tyler Hopkins at the Verrerie of Brehat in Brittany
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art