powered by CADENAS

Social Share

Amazon

Danish design (4849 views - Interior Design)

Danish Design is a style of functionalistic design and architecture that was developed in mid-20th century. Influenced by the German Bauhaus school, many Danish designers used the new industrial technologies, combined with ideas of simplicity and functionalism to design buildings, furniture and household objects, many of which have become iconic and are still in use and production. Prominent examples are the Egg chair, the PH lamps and the Sydney Opera House (Australia).
Go to Article

Explanation by Hotspot Model

Youtube


    

Danish design

Danish design

Danish Design is a style of functionalistic design and architecture that was developed in mid-20th century. Influenced by the German Bauhaus school, many Danish designers used the new industrial technologies, combined with ideas of simplicity and functionalism to design buildings, furniture and household objects, many of which have become iconic and are still in use and production. Prominent examples are the Egg chair, the PH lamps and the Sydney Opera House (Australia).

Designers

Among the most successful designers associated with the concept are Børge Mogensen (1914–72), Finn Juhl (1912–89), Hans Wegner (1914–2007), Arne Jacobsen (1902–71), Poul Kjærholm (1929–80), Poul Henningsen (1894–1967) and Verner Panton (1926–98).[1]

Other designers of note include Kristian Solmer Vedel (1923–2003) in the area of industrial design, Jens Harald Quistgaard (1919–2008) for kitchen furniture and implements, Gertrud Vasegaard (1913–2007) for ceramics, and Ole Wanscher (1903–85), who had a classical approach to furniture design.

History

Arne Jacobsen's Ant Chair, 1951

The Danish Culture Canon credits Thorvald Bindesbøll (1846–1908) with early contributions to design in the areas of ceramics, jewellery, bookbinding, silver and furniture although he is known in the rest of the world for creating the Carlsberg logo (1904), still in use today.[2] The Canon also includes Knud V. Engelhardt (1882–1931) for a more industrial approach, especially in the rounded contours of his electric tramcar designs which were widely copied.[3] In the area of textiles, Marie Gudme Leth (1895–1997) brought the screen printing process to Denmark, opening a factory in 1935 which allowed her colourful patterns to be manufactured on an industrial basis.[4] August Sandgren introduced functionalism in the design of his masterful bookbindings.

In the late 1940s, shortly after the end of the Second World War, conditions in Denmark were ideally suited to success in design. The emphasis was on furniture but architecture, silver, ceramics, glass and textiles also benefitted from the trend. Denmark's late industrialisation combined with a tradition of high-quality craftsmanship formed the basis of gradual progress towards industrial production. After the end of the war, Europeans were keen to find novel approaches such as the light wood furniture from Denmark. Last but not least, support in Denmark for freedom of individual expression assisted the cause.[5]

The newly established Furniture School at the Royal Danish Academy of Art played a considerable part in the development of furniture design. Kaare Klint taught functionalism based on the size and proportions of objects, wielding considerable influence. Hans J. Wegner, who had been trained as a cabinetmaker, contributed with a unique sense of form, especially in designing chairs.[6]

As head of the cooperative FDB furniture design studio, Børge Mogensen designed simple and robust objects of furniture for the average Danish family. Finn Juhl demonstrated an individualistic approach in designing chairs with an appealing but functional look.

In the early 1950s, American design also influenced Danish furniture. The American Charles Eames designed and manufactured chairs of moulded wood and steel pipes. These encouraged Arne Jacobsen to design his worldfamous Ant Chair, Denmark's first industrially manufactured chair. Furthermore, as Shaker furniture—and especially its reputation for stripped down chairs—began to be more and more known abroad, it also influenced Danish designers.[7]

Poul Kjærholm, Verner Panton and Nanna Ditzel followed a few years later, continuing the successful story of Danish design. Kjærholm worked mainly in steel and leather, Panton left Denmark during the 1960s to continue designing imaginative but highly unconventional plastic chairs while Nanna Ditzel, who also had a strongly individualistic approach, was successful in helping to renew Danish furniture design in the 1980s.

Modern trends

In the seventies Verner Panton made some of his most important designs. The Pantonova and the 1-2-3 System. They were a rave with the critics, but the consumers at the time found it too spacey. Today however it's true value to the design tradition is obvious. Danish furniture design failed to make any new important contributions in the 1980s. By contrast, industrial designers began to prosper, making use of the basic principles of focus on the user, respect for materials and attention to detail. For example, there are well known Danish designers, like Tobias Jacobsen (the grandson of Arne Jacobsen), who focused on the single elements of a violin when creating his chair "Vio" or on a boomerang when designing his eponymous sideboard.[8]

The Bernadotte & Bjørn studio, established in 1950, was the first to specialise in industrial design, with an emphasis on office machines, domestic appliances and functional articles such as the thermos jug. The electronics manufacturer Bang & Olufsen, in collaboration with Bernadotte & Bjørn and later with Jacob Jensen and David Lewis, went on to excel in modern design work. Around the same time, the Stelton company collaborated with Arne Jacobsen and Erik Magnussen to produce their iconic vacuum jug, a huge international success.

Another successful design field is medical technology. Danish design companies like 3PART, Designit and CBD have worked in this area with individual designers such as Steve McGugan and Anders Smith.

In 2002 the Danish Government and the City of Copenhagen launched an effort to establish a world event for design in Copenhagen. Originally understood as a tool for branding traditional Danish design, the non-profit organization INDEX: shifted focus after worldwide research and coined the concept of Design to Improve Life, which rapidly became celebrated in Denmark and around the world. The organization now hands out the biggest design award in the world biannual in Copenhagen, tours large scale outdoor exhibition around the world, run educational program as well as design labs and hosts a global network.[citation needed]

Today, there is strong focus on design in Denmark as industry increasingly appreciates the importance of design in the business environment. In addition, as part of its trade and industry policy, the Danish government has launched the DesignDenmark initiative which aims to restore Denmark to the international design elite.[9]

Architecture

Modern architecture has also contributed to the concept of Danish design.

Arne Jacobsen was not just a furniture designer but one of the leading architects of his times. Among his achievements are the Bellevue Theater and restaurant, Klampenborg (1936), the Århus City Hall (with Erik Møller; 1939–42) and the SAS Royal Hotel (1958–60).[10]

Jørn Utzon (1918–2008), Denmark's most widely recognized architect, is remembered for his expressionist Sydney Opera House (1966) and the later Bagsværd Church (1976) with its wavy concrete roof.[11]

Henning Larsen (b. 1925) is the architect who designed the boldly modern Copenhagen Opera House on the island of Holmen which was completed in 2005.[12]

Recent achievements

Today, the concept of Danish design is thriving in an ever-wider number of fields. Among recent highlights are:

Museums

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Interior Design

3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art