Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Herranderssvensson).
Touring car and tourer are both terms for open cars (i.e. cars without a fixed roof).
"Touring car" is a style of open car built in the United States which seats four or more people. The style was popular from the early 1900s to the 1920s. The cars used for touring car racing in various series since the 1960s are unrelated to these early touring cars, despite sharing the same name.
"Tourer" is used in British English for any open car. The term "all-weather tourer" was used to describe convertibles (vehicles that could be fully enclosed). A popular version of the tourer was the torpedo, with the hood/bonnet line at the car's waistline giving the car a straight line from front to back.
"Touring car" was applied in the U.S. to open cars (cars without a fixed roof, for example convertibles) that seat four or more people and has direct entrance to the tonneau (rear passenger area),[1] although it has also been described as seating five or more people.[2] Touring cars may have two or four doors, and the drivetrain layouts of early touring cars was either front engined or mid-engined.
When the top was folded down, it formed a bulky mass known as the "fan" behind the back seat: "fan covers" were made to protect the top and its wooden ribs while in the down position. Some touring cars were available with side curtains to protect occupants from wind and weather by snapping or zipping them into place; otherwise, the occupants had minimal weather protection.
The touring car body style was popular in the early 20th century, being a larger alternative to the two-seat runabout and the roadster. By the mid-1910s, the touring car body had evolved into several types, including the four-door touring car which was equipped with a convertible top.[3][4]
Most of Model T's produced by Ford between 1908 and 1927 were four and then three-door models (with drivers sliding behind the wheel from passenger seat) touring cars, accounting for 6,519,643 cars sold out of the 15,000,000 estimated Model T's built. This accounted for 44% of all Model T's sold over the model's eighteen-plus year life span, making it the most popular body style.[citation needed]
The popularity of the touring car began to wane in the 1920s when cars with enclosed passenger compartments (i.e. fixed steel roofs) became more affordable, and began to consistently out-sell the open cars.[5]
Tourer is used for open cars.[6]
The belt lines of 1930s tourers were often lowered at the front doors to suggest a more sporting character.[7]
All-weather tourer (just as in the U.S.) are cars with high quality tops and wind-up side-windows;[8] they were later called convertibles.[9]
1927 Austin 20 tourer- front (without side curtains)
1951 Ford Anglia tourer- note the lowered beltline at the front door
The torpedo was a style of 4-seat or 5-seat tourers built from 1908 until the mid-1930s.[10] The design consists of a hood/bonnet line raised to be level with the car's waistline, resulting in a straight beltline from front to back.[11]
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Car, Truck,MotorBike, Bicycle, Engine, Racer, Bus