powered by CADENAS

Social Share

Artillery wheel (5333 views - Cars & Motorbikes & Trucks & Buse)

The artillery wheel was developed for use on gun carriages when it was found that the lateral forces involved in horse artillery manoeuvres caused normally constructed cart wheels to collapse. Rather than having its spokes mortised into a wooden nave (hub), it has them fitted together (mitred) then bolted into a metal nave. Its tyre is shrunk onto the rim in the usual way but it is also bolted on for security. A normal wagon wheel is dished so that in its lowest part, the spokes are perpendicular to the ground thus supporting the weight (with the axle not truly horizontal but angled downward toward the outside about 5 degrees). This is not done with artillery wheels.
Go to Article

Explanation by Hotspot Model

Youtube


    

Artillery wheel

Artillery wheel

Artillery wheel

The artillery wheel was developed for use on gun carriages when it was found that the lateral forces involved in horse artillery manoeuvres caused normally constructed cart wheels to collapse. Rather than having its spokes mortised into a wooden nave (hub), it has them fitted together (mitred) then bolted into a metal nave. Its tyre is shrunk onto the rim in the usual way but it is also bolted on for security. A normal wagon wheel is dished so that in its lowest part, the spokes are perpendicular to the ground thus supporting the weight (with the axle not truly horizontal but angled downward toward the outside about 5 degrees). This is not done with artillery wheels.

Motor vehicles

When higher speeds and consequently higher lateral forces were attained with the introduction of motor vehicles, the artillery wheel was used in those too. By the 1920s, motor cars used wheels that looked at a glance like artillery wheels but which were of forged steel or welded from steel pressed sections. These too were usually called artillery wheels.

Joseph Sankey's pressed steel artillery wheels

After training as an engineer, Joseph Sankey founded a major tea tray producer. A pioneer motorist, Sankey became personal friends with Herbert Austin, becoming a supplier of sheet steel components to the industry as a result.[1] By 1914, Joseph Sankey and Sons Ltd. supplied sheet steel bodies to Austin, Daimler, Humber, Rover, Star and Argyll.[1]

As a result of complaints from motor manufacturers about the wooden wheels on these early cars disintegrating upon touching any roadside kerb,[1] In 1908 Sankey with his works manager, Wingfield Burton, developed and patented the first pressed-steel and welded detachable motor car wheel.[2][1] Production started in 1908, with customers including Herbert Austin and, later, William Morris.[1] In addition to his original factory at Bilston a new plant was established near Wellington, Shropshire, which was devoted to wheel production.[1]

In 1920, GKN purchased steel company John Lysaght and their subsidiary, Joseph Sankey and Sons Ltd.[1] By that time the plant was supplying wheels to many UK manufacturers.[1]

Wire wheels

By the late 1920s the inadequacies of artillery wheels had brought about their sweeping replacement by the more expensive wire wheels.

  1. ^ a b c d e f g h "Making the most of it Or – are you driving a GKN?". Motor. 10 May 1969. pp. 58–60.
  2. ^ Edgar Jones, A History of GKN: Volume 2: The Growth of a Business, 1918-1945, Macmillan, London, 1990 ISBN 9781349096664


This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks & Buse

Car, Truck,MotorBike, Bicycle, Engine, Racer, Bus