powered by CADENAS

Social Share

Spray bottle (3627 views - Food Drinks Beverages)

A spray bottle is a bottle that can squirt, spray or mist fluids. A common use for spray bottles is dispensing cool cleaners, cosmetics, and chemical specialties. Another wide use of spray bottles is mixing down concentrates such as pine oil with water.
Go to Article

Explanation by Hotspot Model

Spray bottle

Spray bottle

Spray bottle

Licensed under Creative Commons Attribution 2.0 (robin_24).

A spray bottle is a bottle that can squirt, spray or mist fluids. A common use for spray bottles is dispensing cool cleaners, cosmetics, and chemical specialties. Another wide use of spray bottles is mixing down concentrates such as pine oil with water.

History

While spray bottles existed long before the middle of the 20th century, they used a rubber bulb which was squeezed to produce the spray; the quickly-moving air siphoned fluid from the bottle. The rapid improvement in plastics after World War II increased the range of fluids that could be dispensed, and reduced the cost of the sprayers because assembly could be fully automated.

The Drackett company, manufacturers of Windex glass cleaner, was a leader in promoting spray bottles. Roger Drackett raised soybeans, converted the soybeans to plastic using technology purchased from Henry Ford, and was an investor in the Seaquist company, an early manufacturer of sprayers and closures. Initially, the brittle nature of early plastics required that sprayers be packaged in a cardboard box, and the sprayer inserted in the glass Windex bottle by the consumer. The cost in the manufacturing sprayers was also a factor; consumers would reuse the sprayers with bottle after bottle of glass cleaner. As plastics improved and the cost of sprayers dropped, manufacturers were able to ship products with the sprayer already in the bottle.

In the late 1960s, spray bottles with trigger-style actuators appeared and quickly became popular, as this design was less fatiguing to use. The original pump-style bottle remained more popular for applications like non-aerosol deodorants, where size was a factor and repeated pumps were not required.

Modern spray bottles

Unlike the rubber bulb dispenser which primarily moved air with a small amount of fluid, modern spray bottles use a positive displacement pump that acts directly on the fluid. The pump draws liquid up a siphon tube from the bottom of the bottle and forces it through a nozzle. Depending on the sprayer, the nozzle may or may not be adjustable, so as to select between squirting a stream, aerosolizing a mist, or dispensing a spray.

In a spray bottle, the dispensing is powered by the user's efforts, as opposed to the spray can, in which the user simply actuates a valve and product is dispensed under pressure.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Food Drinks Beverages

food,liquor,alcohol,drink,beverage,coke