powered by CADENAS

Social Share

Sodium chromate (19865 views - Material Database)

Sodium chromate is the inorganic compound with the formula Na2CrO4. It exists as a yellow hygroscopic solid, which can form tetra-, hexa-, and decahydrates. It is an intermediate in the extraction of chromium from its ores. Sodium chromate, like other hexavalent chromium compounds, is toxic and carcinogenic.
Go to Article

Sodium chromate

Sodium chromate

Sodium chromate
Sodium chromate
Names
IUPAC name
Sodium chromate
Other names
Chromic acid, (Na2CrO4), disodium salt
Chromium disodium oxide
Rachromate
Identifiers
3D model (JSmol)
ChEBI
ECHA InfoCard 100.028.990
EC Number 231-889-5
RTECS number GB2955000
UNII
UN number 3288
Properties
Na2CrO4
Molar mass 161.97 g/mol
Appearance yellow crystals
Odor odorless
Density 2.698 g/cm3
Melting point 792 °C (1,458 °F; 1,065 K) (anhydrous)
20 °C (decahydrate)
31.8 g/100 mL (0 °C)
84.5 g/100 mL (25 °C)
126.7 g/100 mL (100 °C)
Solubility slightly soluble in ethanol
Solubility in methanol 0.344 g/100 mL (25 °C)
+55.0·10−6 cm3/mol
Structure
orthorhombic (hexagonal above 413 °C)
Thermochemistry
142.1 J/mol K
174.5 J/mol K
−1329 kJ/mol
-1232 kJ/mol
Hazards
Safety data sheet ICSC 1370
Carc. Cat. 2
Muta. Cat. 2
Repr. Cat. 2
Very toxic (T+)
Harmful (Xn)
Corrosive (C)
Dangerous for the environment (N)
R-phrases (outdated) R45, R46, R60, R61, R21, R25, R26, R34, R42/43, R48/23, R50/53
S-phrases (outdated) S53, S45, S60, S61
NFPA 704
Flammability code 0: Will not burn. E.g., waterHealth code 3: Short exposure could cause serious temporary or residual injury. E.g., chlorine gasReactivity (yellow): no hazard codeSpecial hazard OX: Oxidizer. E.g., potassium perchlorate
0
3
Flash point Non-flammable
Related compounds
Other anions
Sodium dichromate
Sodium molybdate
Sodium tungstate
Other cations
Potassium chromate
Calcium chromate
Barium chromate
Except where otherwise noted, data are given for materials in their standard state (at 25 °C [77 °F], 100 kPa).
N verify (what is YN ?)
Infobox references

Sodium chromate is the inorganic compound with the formula Na2CrO4. It exists as a yellow hygroscopic solid, which can form tetra-, hexa-, and decahydrates. It is an intermediate in the extraction of chromium from its ores. Sodium chromate, like other hexavalent chromium compounds, is toxic and carcinogenic.[1]

Production and reactivity

It is obtained on a vast scale by roasting chromium ores in air in the presence of sodium carbonate:

2Cr2O3 + 4 Na2CO3 + 3 O2 → 4 Na2CrO4 + 4 CO2

This process converts the chromium into a water-extractable form, leaving behind iron oxides. Typically calcium carbonate is included in the mixture to improve oxygen access and to keep silicon and aluminium impurities in an insoluble form. The process temperature is typically around 1100 C.[2] For lab and small scale preparations a mixture of chromite ore, sodium hydroxide and sodium nitrate reacting at lower temperatures may be used (even 350 C in the corresponding potassium chromate system).[3] Subsequent to its formation, the chromate salt is converted to sodium dichromate, the precursor to most chromium compounds and materials.[1] The industrial route to chromium(III) oxide involves reduction of sodium chromate with sulfur.

Acid-base behavior

It converts to sodium dichromate when treated with acids:

2 Na2CrO4 + 2HCl → Na2Cr2O7 + 2NaCl + H2O

Further acidification affords chromium trioxide:

Na2CrO4 + H2SO4 → CrO3 + Na2SO4 + H2O

Uses

Aside from its central role in the production of chromium from its ores, sodium chromate is used as a corrosion inhibitor in the petroleum industry.[1] It is also a dyeing auxiliary in the textile industry[1] and a wood preservative.[4] It is a diagnostic pharmaceutical in determining red blood cell volume.[5]

In organic chemistry, sodium chromate is used as an oxidant, converting primary alcohols to carboxylic acids and secondary alcohols to ketones.[6]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification