powered by CADENAS

Social Share

Mischmetal (12697 views - Material Database)

Mischmetal (from German: Mischmetall – "mixed metal") is an alloy of rare earth elements. It is also called cerium mischmetal, rare earth mischmetal or misch metal. A typical composition includes approximately 50% cerium and 25% lanthanum, with small amounts of neodymium and praseodymium. Its most common use is in the ferrocerium "flint" ignition device of many lighters and torches, although an alloy of only rare-earth elements would be too soft to give good sparks. For this purpose, it is blended with iron oxide and magnesium oxide to form a harder material known as ferrocerium. In chemical formulae it is commonly abbreviated as Mm, e.g. MmNi5.
Go to Article

Mischmetal

Mischmetal

Mischmetal (from German: Mischmetall – "mixed metal") is an alloy of rare earth elements. It is also called cerium mischmetal, rare earth mischmetal or misch metal. A typical composition includes approximately 50% cerium and 25% lanthanum, with small amounts of neodymium and praseodymium. Its most common use is in the ferrocerium "flint" ignition device of many lighters and torches, although an alloy of only rare-earth elements would be too soft to give good sparks. For this purpose, it is blended with iron oxide and magnesium oxide to form a harder material known as ferrocerium. In chemical formulae it is commonly abbreviated as Mm, e.g. MmNi5.[1]

History

Carl Auer von Welsbach was not only the discoverer of neodymium and praseodymium, and co-discoverer of lutetium, but was also the inventor of the light-mantle (using thorium), and of the rare earth industry. After extracting necessary thorium content from monazite sand, a lot of lanthanides were left over, for which there was no commercial use. He began exploration for applications to which the rare earths might be put. Among his first discoveries/inventions to bear practical fruit was mischmetal.

Preparation

Historically, mischmetal was prepared from monazite, an anhydrous phosphate of the light lanthanides and thorium. The ore was cracked by reaction at high temperature either with concentrated sulfuric acid, or with sodium hydroxide. Thorium was removed by taking advantage of its weaker basicity relative to the trivalent lanthanides, its daughter radium was precipitated out using entrainment in barium sulfate, and the remaining lanthanides were converted to their chlorides. The resulting "rare earth chloride" (hexahydrate), sometimes known as "lanthanide chloride", was the major commodity chemical of the rare earth industry. By careful heating, preferably with ammonium chloride or in an atmosphere of hydrogen chloride, the hexahydrate could be dehydrated to provide the anhydrous chloride. Electrolysis of the molten anhydrous chloride (admixed with other anhydrous halide to improve the melt behavior) led to the formation of molten mischmetal, which would then be cast into ingots. Any samarium content of the ore tended not to be reduced to the metal, but accumulated in the molten halide, from which it could later be profitably isolated. Monazite-derived mischmetal typically was about 48% cerium, 25% lanthanum, 17% neodymium, and 5% praseodymium, with the balance being the other lanthanides. When bastnäsite started being processed for rare earth content in about 1965, it too was converted to a version of rare earth chloride, and on to mischmetal. This version was higher in lanthanum and lower in neodymium.

As of 2007, the high demand for neodymium has made it profitable to remove all of the heavier lanthanides and neodymium (and sometimes all of the praseodymium as well) from the natural-abundance lanthanide mixture for separate sale, and to include only La-Ce-Pr or La-Ce in the most economical forms of mischmetal. The light lanthanides are so similar in their metallurgical properties, that any application for which the original composition would have been suitable, would be equally well served by these truncated mixtures. The traditional "rare earth chloride", as a commodity chemical, was also used to extract the individual rare earths by companies that did not wish to process the ores directly. As of 2007 mischmetal is typically priced at less than US$10 per kilogram, and the underlying rare earth chloride mixtures are typically less than US$5 per kilogram.

Use

Mischmetal is used in the preparation of virtually all rare earth elements. This is because such elements are nearly identical in most chemical processes, meaning that ordinary extraction processes do not distinguish them. Highly specialized processes, such as those developed by Carl Auer von Welsbach, exploit subtle differences in solubility to separate mischmetal into its constituent elements, with each step producing only an incremental change in composition. Such processes later informed Marie Curie in her search for new elements.

  1. ^ Jurczyk, M; Rajewski, W; Majchrzycki, W; Wójcik, G (1999-08-30). "Mechanically alloyed MmNi5-type materials for metal hydride electrodes". Journal of Alloys and Compounds. 290 (1–2): 262–266. doi:10.1016/S0925-8388(99)00202-9. 
  • R.J. Callow, "The Industrial Chemistry of the Lanthanons, Yttrium, Thorium and Uranium", Pergamon Press, 1967
  • Gupta, C. K.; Krishnamurthy, N. (2005). Extractive metallurgy of rare earths. Boca Raton: CRC Press. ISBN 0-415-33340-7. 
  • F.H. Spedding and A.H. Daane, editors, "The Rare Earths", John Wiley & Sons, 1961.

41xx steelAL-6XNAlGaAlloy 20AlnicoAlumel알루미늄알루미늄 합금알루미늄 청동Aluminium-lithium alloy아말감Arsenical bronzeArsenical copperBell metal베릴륨베릴륨구리Billon (alloy)BirmabrightBismanol비스무트황동Brightray청동Bulat steelCalamine brass주철CelestriumChinese silverChromel크로뮴Chromium hydride코발트Colored goldConstantan구리Copper hydrideCopper–tungstenCorinthian bronzeCrown goldCrucible steelCunife백동Cymbal alloys다마스쿠스 강Devarda's alloy두랄루민Dutch metalElectrical steel호박금Elektron (alloy)ElinvarFernicoFerroalloy페로세륨FerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolGalinstan갈륨Gilding metal유리GlucydurGuanín (bronze)GunmetalHaynes InternationalHepatizonHiduminiumHigh-speed steelHigh-strength low-alloy steelHydronaliumInconel인듐InvarIron–hydrogen alloyItalmaKanthal (alloy)KovarMagnalium마그네슘Magnox (alloy)MangalloyManganinMaraging steelMarine grade stainlessMartensitic stainless steelMegalliumMelchior (alloy)머큐리MolybdochalkosMonelMu-metalMuntz metalMushet steel니크롬니켈Nickel hydride양은Nickel titaniumNicrosilNisil노르딕 골드Ormolu퍼멀로이Phosphor bronze선철Pinchbeck (alloy)플라스틱Plexiglas플루토늄Plutonium–gallium alloy칼륨Reynolds 531Rhodite로듐Rose's metal사마륨Sanicro 28스칸듐ShakudōSilver steel나트륨나크땜납Speculum metalSpiegeleisenSpring steelStaballoy스테인리스강강철StelliteStructural steelSupermalloySurgical stainless steelTerne주석 (원소)타이타늄TombacTool steelTumbagaType metal우라늄VitalliumWeathering steel우드 합금Wootz steelY alloyZeron 100아연지르코늄리튬Terfenol-DPseudo palladiumScandium hydrideSamarium–cobalt magnetArgentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichi스털링 실버Tibetan silverTitanium Beta CTitanium alloyTitanium hydrideGum metalTitanium goldTitanium nitride배빗메탈Britannia metal퓨터Queen's metalWhite metalUranium hydrideZamakZirconium hydride수소헬륨붕소질소산소플루오린메테인Mezzanine원자Honing (metalworking)Metalworking재료과학

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification