powered by CADENAS

Social Share

Constantan (17192 views - Material Database)

Constantan is a copper–nickel alloy also known as Eureka, Advance, and Ferry. It usually consists of 55% copper and 45% nickel. Its main feature is its resistivity, which is constant over a wide range of temperatures. Other alloys with similarly low temperature coefficients are known, such as manganin (Cu86Mn12Ni2).
Go to Article

Constantan

Constantan

Constantan
Type Copper-nickel alloy
Physical properties
Density (ρ) 8 885.24941 kg/m^3
Mechanical properties
Young's modulus (E) 24 x 106 PSI
Tensile strengtht) 60,000 PSI
Elongation (ε) at break 25%
Thermal properties
Melting temperature (Tm) 1210° C
Thermal conductivity (k) 21.2W/m· K
Specific heat capacity (c) .094 gram· cal./°C
Electrical properties
Surface resistivity 0.49 μΩ·m

Constantan is a coppernickel alloy also known as Eureka, Advance, and Ferry.[1] It usually consists of 55% copper and 45% nickel.[2] Its main feature is its resistivity, which is constant over a wide range of temperatures. Other alloys with similarly low temperature coefficients are known, such as manganin (Cu86Mn12Ni2).

History

In 1887, Edward Weston discovered that metals can have a negative temperature coefficient of resistance, inventing what he called his "Alloy No. 2." It was produced in Germany where it was renamed "constantan".[3][4]

Constantan alloy

Of all modern strain gauge alloys, constantan is the oldest, and still the most widely used. This situation reflects the fact that constantan has the best overall combination of properties needed for many strain gauge applications. This alloy has, for example, an adequately high strain sensitivity, or gauge factor, which is relatively insensitive to strain level and temperature. Its resistivity (49.0 x 10−8 Ω·m)[5] is high enough to achieve suitable resistance values in even very small grids, and its temperature coefficient of resistance is fairly low. In addition, constantan is characterized by good fatigue life and relatively high elongation capability. However, constantan tends to exhibit a continuous drift at temperatures above 65 °C (150 °F);[6] and this characteristic should be taken into account when zero stability of the strain gauge is critical over a period of hours or days. Constantan is also used for electrical resistance heating and thermocouples.[7]

A-Alloy

Very importantly, constantan can be processed for self-temperature compensation to match a wide range of test material coefficients of thermal expansion. A-alloy is supplied in self-temperature-compensation (S-T-C) numbers 00, 03, 05, 06, 09, 13, 15, 18, 30, 40 and 50, for use on test materials with corresponding thermal expansion coefficients, expressed in parts per million by length (or µm/m) per degrees Celsius or kelvins

P alloy

For the measurement of very large strains, 5% (50 000 microstrain) or above, annealed constantan (P alloy) is the grid material normally selected. Constantan in this form is very ductile; and, in gauge lengths of 0.125 in (3 mm) and longer, can be strained to >20%. It should be borne in mind, however, that under high cyclic strains the P alloy will exhibit some permanent resistivity change with each cycle, and cause a corresponding zero shift in the strain gauge. Because of this characteristic, and the tendency for premature grid failure with repeated straining, P alloy is not ordinarily recommended for cyclic strain applications. P alloy is available with S-T-C numbers of 08 and 40 for use on metals and plastics, respectively.

Physical properties

Electrical resistivity at room temperature[2] 4.9 x 10−7 Ω·m
Temperature coefficient at 20 °C[8] 8 ppmK−1
Temperature coefficient -55 to 105 °C[2] ±40 ppmK−1
Curie point[9] 35 K
Density[2] 8.9 × 103 kg/m³
Melting point 1221 to 1300 °C
Specific heat capacity 0.39 kJ/(kg·K)
Thermal conductivity at 23 °C 19.5 W/(m.K)
Linear coefficient of thermal expansion at 25-105 °C[2] 14.9 × 10−6 K−1
Tensile strength[2] 455-860 MPa
Elongation at fracture <45%
Elastic modulus 162 GPa

Temperature measurement

Constantan is also used to form thermocouples with wires made of iron, copper, or chromel.[7] It has an extraordinarily strong negative Seebeck coefficient above 0 Celsius,[10] leading to a good temperature sensitivity.

  1. ^ M. A. Laughton; D. F. Warne (2003). Electrical Engineers Reference Book (16th ed.). Elsevier. p. 10/43. ISBN 0-7506-4637-3. 
  2. ^ a b c d e f J. R. Davis (2001). Copper and Copper Alloys. ASM International. p. 158. ISBN 0-87170-726-8. 
  3. ^ A chronological history of electrical development from 600 B.C. National Electrical Manufacturers Association. 1946. p. 59. 
  4. ^ D. O. Woodbury (1949). A measure for greatness: a short biography of Edward Weston. McGraw-Hill. p. 168. 
  5. ^ "Table of Resistivity". hyperphysics.phy-astr.gsu.edu. Retrieved 2016-05-18. 
  6. ^ Hannah, R.L. (1992). Strain Gage Users' Handbook. New York: Springer. p. 50. ISBN 978-0412537202. 
  7. ^ a b "Working with Chromel, Alumel & Constantan". Keats Manufacturing Co. 2015-03-12. Retrieved 2016-05-18. 
  8. ^ J. O'Malley (1992). Schaum's outline of theory and problems of basic circuit analysis. McGraw-Hill Professional. p. 19. ISBN 0-07-047824-4. 
  9. ^ Varanasi, C. V.; Brunke, L.; Burke, J.; Maartense, I.; Padmaja, N.; Efstathiadis, H.; Chaney, A.; Barnes, P. N. (2006). "Biaxially textured constantan alloy (Cu 55 wt%, Ni 44 wt%, Mn 1 wt%) substrates for YBa2Cu3O7−x coated conductors". Superconductor Science and Technology. 19 (9): 896. doi:10.1088/0953-2048/19/9/002. 
  10. ^ Handbook of Temperature Measurement Vol. 3, edited by Robin E. Bentley

Bibliography

  • J. R. Davis (2001). Copper and Copper Alloys. ASM International. ISBN 0-87170-726-8. 

Alnico알루미늄알루미늄 합금알루미늄 청동Aluminium-lithium alloyArsenical bronzeArsenical copperBell metal베릴륨베릴륨구리Billon (alloy)BirmabrightBismanol비스무트황동청동Calamine brassChinese silver크로뮴Chromium hydride코발트구리두랄루민Dutch metalFlorentine bronze갈륨Gilding metal유리GlucydurGuanín (bronze)GunmetalHiduminiumHydronalium인듐ItalmaMagnalium마그네슘Megallium머큐리Muntz metal니크롬니켈OrmoluPhosphor bronzePinchbeck (alloy)플라스틱Plexiglas플루토늄칼륨로듐Rose's metal사마륨스칸듐나트륨Speculum metal스테인리스강강철StelliteStructural steel주석 (원소)타이타늄Tombac우라늄Vitallium우드 합금Y alloy아연지르코늄Copper hydrideCopper–tungstenCorinthian bronzeCunife백동Cymbal alloysDevarda's alloy호박금HepatizonManganinMelchior (alloy)양은Molybdochalkos노르딕 골드ShakudōTumbagaAlGaGalfenolGalinstanColored goldRhoditeCrown goldElinvarField's metalFernicoFerroalloy페로세륨FerrochromeFerromanganeseFerromolybdenumFerrosiliconFerrotitaniumFerrouraniumInvar주철Iron–hydrogen alloy선철Kanthal (alloy)KovarStaballoySpiegeleisenBulat steelCrucible steel41xx steel다마스쿠스 강MangalloyHigh-speed steelMushet steelMaraging steelHigh-strength low-alloy steelReynolds 531Electrical steelSpring steelAL-6XNCelestriumAlloy 20Marine grade stainlessMartensitic stainless steelSanicro 28Surgical stainless steelZeron 100Silver steelTool steelWeathering steelWootz steel땜납TerneType metalElektron (alloy)아말감Magnox (alloy)AlumelBrightrayChromelHaynes InternationalInconelMonelNicrosilNisilNickel titaniumMu-metal퍼멀로이SupermalloyNickel hydridePlutonium–gallium alloy나크Mischmetal리튬Terfenol-DPseudo palladiumScandium hydrideSamarium–cobalt magnetArgentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterlingShibuichi스털링 실버Tibetan silverTitanium Beta CTitanium alloyTitanium hydrideGum metalTitanium goldTitanium nitride배빗메탈Britannia metal퓨터Queen's metalWhite metalUranium hydrideZamakZirconium hydride수소헬륨붕소질소산소플루오린메테인Mezzanine원자

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification