powered by CADENAS

Social Share

Amazon

Automobile roof (4787 views - Cars & Motorbikes & Trucks & Buse)

An automobile roof or car top is the portion of an automobile that sits above the passenger compartment, protecting the vehicle occupants from sun, wind, rain, and other external elements. Because the earliest automobiles were designed in an era of horse-drawn carriages, early automobile roofs used similar materials and designs.
Go to Article

Explanation by Hotspot Model

Youtube


    

Automobile roof

Automobile roof

Automobile roof

Licensed under Creative Commons Attribution 3.0 (Unkown).

An automobile roof or car top is the portion of an automobile that sits above the passenger compartment, protecting the vehicle occupants from sun, wind, rain, and other external elements. Because the earliest automobiles were designed in an era of horse-drawn carriages, early automobile roofs used similar materials and designs.

Variations

In later years, many variations on the automobile roof developed. These include:

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks & Buse

Car, Truck,MotorBike, Bicycle, Engine, Racer, Bus