powered by CADENAS

Social Share

Amazon

Strike fighter (2678 views - Transportation - Air Water Earth)

In current military parlance, a strike fighter is a multirole combat aircraft designed to operate primarily as an attack aircraft, while also incorporating certain performance characteristics of a fighter for air-to-air combat. As a category, it is distinct from fighter-bombers. It is closely related to the concept of interdictor aircraft, but it puts more emphasis on air-to-air combat capabilities as a multirole combat aircraft. Examples of contemporary American strike fighters are the McDonnell Douglas F-15E Strike Eagle, Boeing F/A-18E/F Super Hornet, and Lockheed Martin F-35 Lightning II.
Go to Article

Explanation by Hotspot Model

Youtube


    

Strike fighter

Strike fighter

Strike fighter

In current military parlance, a strike fighter is a multirole combat aircraft designed to operate primarily as an attack aircraft, while also incorporating certain performance characteristics of a fighter for air-to-air combat. As a category, it is distinct from fighter-bombers.[citation needed] It is closely related to the concept of interdictor aircraft,[citation needed] but it puts more emphasis on air-to-air combat capabilities as a multirole combat aircraft. Examples of contemporary American strike fighters are the McDonnell Douglas F-15E Strike Eagle, Boeing F/A-18E/F Super Hornet, and Lockheed Martin F-35 Lightning II.

History

Beginning in the 1940s, the term "strike fighter" was occasionally used in navies to refer to fighter aircraft capable of performing air-to-surface strikes, such as the Westland Wyvern,[1] Blackburn Firebrand[2] and Blackburn Firecrest.

The term "light weight tactical strike fighter (LWTSF)" was used to describe the aircraft to meet the December 1953 NATO specification NBMR-1.[3] Amongst the designs submitted to the competition were the Aerfer Sagittario 2, Breguet Br.1001 Taon, Dassault Étendard VI, Fiat G.91 and Sud-Est Baroudeur.

The term entered normal use in the United States Navy[4] by the end of the 1970s, becoming the official[5] description of the new McDonnell Douglas F/A-18 Hornet. In 1983, the U.S. Navy even renamed each existing Fighter Attack Squadron to Strike Fighter Squadron to emphasize[6] the air-to-surface mission (as the "Fighter Attack" designation was confused with the "Fighter" designation, which flew pure air-to-air missions).

This name quickly spread to non-maritime use. When the F-15E Strike Eagle came into service, it was originally called a "dual role fighter",[7] but it instead quickly became known as a "strike fighter".

Joint Strike Fighter

In 1995, the U.S. military's Joint Advanced Strike Technology program changed its name to the Joint Strike Fighter program.[8] The project consequently resulted in the development of the F-35 Lightning II family of fifth generation multirole fighters to perform ground attack, reconnaissance, and air defense missions with stealth capability.

Modern strike fighters

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht