Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
A display device is an output device for presentation of information in visual[1] or tactile form (the latter used for example in tactile electronic displays for blind people).[2] When the input information that is supplied has an electrical signal, the display is called an electronic display.
Common applications for electronic visual displays are televisions or computer monitors.
In the history of display technology, a variety of display devices and technologies have been used.
There are various designs for display devices, using various technologies. Several components are common to most display devices.
These are the technologies used to create the various displays in use today.
Some displays can show only digits or alphanumeric characters. They are called segment displays, because they are composed of several segments that switch on and off to give appearance of desired glyph. The segments are usually single LEDs or liquid crystals. They are mostly used in digital watches and pocket calculators. There are several types:
2-dimensional displays that cover a full area (usually a rectangle) are also called video displays, since it is the main modality of presenting video.
Full-area 2-dimensional displays are used in, for example:
Underlying technologies for full-area 2-dimensional displays include:
The multiplexed display technique is used to drive most display devices.
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Computer, Hardware, Software