powered by CADENAS

Social Share

Amazon

Moustache cup (6196 views - Food Drinks Beverages)

The moustache cup (or mustache cup) is a drinking cup with a semicircular ledge inside. The ledge has a half moon-shaped opening to allow the passage of liquids and serves as a guard to keep moustaches dry. It is generally acknowledged to have been invented in the 1860s by British potter Harvey Adams (born 1835).
Go to Article

Explanation by Hotspot Model

Youtube


    

Moustache cup

Moustache cup

Moustache cup

Licensed under Creative Commons Attribution-Share Alike 4.0 (Foto: Anne-Lise Reinsfelt, Norsk Folkemuseum).

The moustache cup (or mustache cup) is a drinking cup with a semicircular ledge inside. The ledge has a half moon-shaped opening to allow the passage of liquids and serves as a guard to keep moustaches dry. It is generally acknowledged to have been invented in the 1860s by British potter Harvey Adams (born 1835).[1]

Historic context

Moustaches flourished throughout the Victorian era. In fact, from 1860 to 1916, the British military actually required all of its soldiers to sport a moustache for the authority it imparted to the moustachioed man.[2] Often, moustache wax was applied to the moustache to keep it stiff, with every hair in place. When drinking hot liquids, steam from the drink would melt the wax, which would drip into the cup. Sipping hot tea or coffee would also often stain moustaches.[3]

Invention

In 1860, Englishman Harvey Adams came up with an unusual invention, "the moustache cup". This had a ledge or shelf, called a moustache guard, across the cup. The ledge had one semicircular opening against the side of the cup. The pampered moustache then rested safe and dry on the guard while sipping a hot beverage through the opening.[1]

Production

The new invention spread all over the European continent and soon, every famous potter was making the new cups. A multiplicity of moustache cups were made by famous manufactories such as Meissen, Royal Crown Derby, Imari, Royal Bayreuth, Limoges and others. Each potter created his own version of this masculine tableware and the news of that invention soon spread to America.

Although many moustache cups were made in America, the earliest were marked with names which led buyers to believe they were actually manufactured in England. This was due to the popularity of English-made ceramics. Therefore, with the exception of the quadruple silver moustache cups made in the U.S., it is nowadays extremely difficult to find an authentic Victorian moustache cup bearing an American pottery mark.

Decline and resurge

Between 1920 and 1930, moustaches progressively began to go out of fashion and hence moustache cup production trickled down. Today though, these examples of Victorian male elegance are coveted and collected by a growing number of enthusiasts.[1]

Moustache cups are becoming highly collectible as their popularity has increased in recent years due to a resurgence of men's facial hair styles.[4]

In popular culture

In James Joyce's Ulysses, Leopold Bloom drinks his tea from a moustache cup he received from his daughter Milly for his twenty-seventh birthday.[5]

On Episode 15 of Season 4 on the Andy Griffith Show Aunt Bea receives one as a gift from a local Farmer, MR. Frisby.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Food Drinks Beverages

food,liquor,alcohol,drink,beverage,coke