powered by CADENAS

Social Share

Amazon

Hurricane glass (7952 views - Food Drinks Beverages)

A Hurricane glass is a form of drinking glass which typically will contain 20 US fluid ounces (590 ml; 21 imp fl oz). It is used to serve mixed drinks, particularly the Hurricane from which it is named originating at Pat O'Brien's Bar in New Orleans. Other drinks served in this glass include the Singapore Sling, June bug, Piña colada and Blue Hawaii. It is shaped similarly to a vase or a hurricane lamp and is typically taller and wider than a highball glass. In New Orleans, a Hurricane is sometimes served in a disposable plastic cup, as New Orleans laws permit drinking in public and leaving a bar with a drink, but prohibit public drinking from glass or metal containers.The Poco Grande glass has a similar fluted bowl shape, but is shallower and has a longer stem. It is used for similar drinks as the hurricane glass, but its smaller portion size (about 12 fluid ounces) allows the bartender flexibility in determining the size of the drinks offered and/or the amount of alcohol in the glass.
Go to Article

Explanation by Hotspot Model

Youtube


    

Hurricane glass

Hurricane glass

A Hurricane glass is a form of drinking glass which typically will contain 20 US fluid ounces (590 ml; 21 imp fl oz). It is used to serve mixed drinks, particularly the Hurricane from which it is named originating at Pat O'Brien's Bar in New Orleans.[1] Other drinks served in this glass include the Singapore Sling, June bug, Piña colada and Blue Hawaii. It is shaped similarly to a vase or a hurricane lamp and is typically taller and wider than a highball glass.

In New Orleans, a Hurricane is sometimes served in a disposable plastic cup, as New Orleans laws permit drinking in public and leaving a bar with a drink, but prohibit public drinking from glass or metal containers.[2][3]

The Poco Grande glass has a similar fluted bowl shape, but is shallower and has a longer stem. It is used for similar drinks as the hurricane glass, but its smaller portion size (about 12 fluid ounces) allows the bartender flexibility in determining the size of the drinks offered and/or the amount of alcohol in the glass.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Food Drinks Beverages

food,liquor,alcohol,drink,beverage,coke