powered by CADENAS

Social Share

Amazon

Spacers and standoffs (5785 views - Tooling)

A standoff is a threaded separator of defined length used to raise one assembly above another. They are usually round or hex (for wrench tightening), often made of aluminum, brass, or nylon, and come in male-female or female-female forms. In electronics they are frequently used to raise a printed-circuit board above a surface. Insulating standoffs keep two parts from touching each other, thereby preventing electrical shorts. When used to fasten cable connectors (i.e. "D" connectors) together, they are called "jack screws". In contrast, a spacer is an unthreaded piece of tubing which lets the entire bolt pass through. Since they cannot be tightened, they are usually round.
Go to Article

Explanation by Hotspot Model

Spacers and standoffs

Spacers and standoffs

Spacers and standoffs

A standoff is a threaded separator of defined length used to raise one assembly above another. They are usually round or hex (for wrench tightening), often made of aluminum, brass, or nylon, and come in male-female or female-female forms. In electronics they are frequently used to raise a printed-circuit board above a surface. Insulating standoffs keep two parts from touching each other, thereby preventing electrical shorts. When used to fasten cable connectors (i.e. "D" connectors) together, they are called "jack screws".

In contrast, a spacer is an unthreaded piece of tubing which lets the entire bolt pass through. Since they cannot be tightened, they are usually round.[1]

Usage in home computers

Size 4-40 is used to secure cables to external computer ports, and size 6-32 is used for motherboard mounts.

Dell, Inc. refers to standoffs that receive thumbscrews as "hex nut screws" and measures them with the Metric system.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing