powered by CADENAS

Social Share

Amazon

Guna people (6528 views - Countries & Continents)

The Guna, known as Kuna prior to an orthographic reform in 2010, and historically as Cuna, are an indigenous people of Panama and Colombia. The Congreso General de la Nación Gunadule since 2010 promotes the spelling Guna. In the Kuna language, they call themselves Dule or Tule, meaning "people", and the name of the language in Kuna is Dulegaya, literally "people-mouth".
Go to Article

Explanation by Hotspot Model

Guna people

Guna people

Guna
A Guna woman wearing a mola[1] stands next to a clothes line in Kuna Yala, Panama
Total population
about 50,000
Regions with significant populations
Panama, Colombia
Languages
Kuna, Spanish
Religion
traditional Kuna religion, Christianity
Related ethnic groups
other Chibchan-speaking people, Miskito
The Guna, known as Kuna prior to an orthographic reform in 2010[2], and historically as Cuna, are an indigenous people of Panama and Colombia. The Congreso General de la Nación Gunadule since 2010 promotes the spelling Guna. In the Kuna language, they call themselves Dule or Tule, meaning "people", and the name of the language in Kuna is Dulegaya, literally "people-mouth".[3]

Location

The Guna live in three politically autonomous comarcas or reservations in Panama, and in a few small villages in Colombia. There are also communities of Kuna people in Panama City, Colón, and other cities. The most Gunas live on small islands off the coast of the comarca of Kuna Yala known as the San Blas Islands. The other two Guna comarcas in Panama are Kuna de Madugandí and Kuna de Wargandí. They are Guna speaking people who once occupied the central region of what is now Panama and the neighboring San Blas Islands and still survive in marginal areas.

Political and social organization

In Guna Yala, each community has its own political organization, led by a saila (pronounced "sigh-lah"). The saila is traditionally both the political and spiritual leader of the community; he memorizes songs which relate the sacred history of the people, and in turn transmits them to the people. Decisions are made in meetings held in the Onmaked Nega, or Ibeorgun Nega (Congress House or Casa de Congreso), a structure which likewise serves both political and spiritual purposes. It is in the Onmaked Nega that the saila sings the history, legends and laws of the Guna, as well as administering the day-to-day political and social affairs. The saila is usually accompanied by one or more voceros who function as interpreters and counselors for the saila. Because the songs and oral history of the Guna are in a higher linguistic register with specialized vocabulary, the saila's recitation will frequently be followed by an explanation and interpretation from one of the voceros in everyday Guna language.

Traditionally, Guna families are matrilinear, with the groom moving to become part of the bride's family. The groom takes the last name of the bride as well.

Today there are 49 communities in Kuna Yala. The region as a whole is governed by the Guna General Congress, which is led by three Saila Dummagan ("Great Sailas").[4]

Flag

The flag of the Kuna Yala community.

The Guna Swastika flag was adopted after 1925 rebellion against Panamanian suppression. Horizontal stripes have a proportion of 1:2:1 and the central swastika is an ancestral symbol called Naa Ukuryaa. According to one explanation, it symbolizes the four sides of the world or the origin from which peoples of the world emerged.[5] Also known as the flag of Guna Yala island today, the flag is used for the province of San Blas and also as Kuna ethnic flag. The central stripe, meaning peace and purity, is white on the official flag of the reservation, officially adopted by Guna National Congress, while yellow stripe is used on ethnic flag (it was introduced on the flag at about 1940). In 1942 the flag was modified with a red ring encompassing the center of the swastika because of Nazi associations; the ring was later abandoned.[6]

Culture

The Guna are famous for their bright molas, a colorful textile art form made with the techniques of appliqué and reverse appliqué. Mola panels are used to make the blouses of the Kuna women's national dress, which is worn daily by many Guna women. Mola means "clothing" in the Kuna language. The Guna word for a mola blouse is Tulemola, (or "dulemola") "Kuna people's clothing."

Economy

A Guna woman selling molas in Panama City.

The economy of Kuna Yala is based on agriculture, fishing and the manufacture of clothing with a long tradition of international trade. Plantains, coconuts, and fish form the core of the Guna diet, supplemented with imported foods, a few domestic animals, and wild game. Coconuts, called ogob [IPA: okˑɔβ] in the Kuna language, and lobsters skungit (skuŋkˑit) are the most important export products. Migrant labor and the sale of molas provide other sources of income.

The Guna have a long deep rooted history of mercantilism and a longstanding tradition of selling goods through family owned venues. Most imported goods originate from Colombian, Mexican or Chinese ships and are sold in small retail stores owned by Guna people. The Guna traditionally excise no tax when trading goods and place strong emphasis on economic success. This tradition of trade and self-determination has been credited by many as a chief reason why the Guna have been able to successfully function independently compared to other indigenous groups.

Guna communities in Panama City are typically made up of migrant laborers and small business owners, although many Kuna also migrate to Panama City to sell fish and agricultural products produced by their respective communities. The sale of Mola and other forms of Guna art has become a large part of the Guna peoples economy in recent years and mola vendors can be found in most cities in Panama where they are marketed to both foreigners and Hispano Panamanians. Tourism is now an important part of the economy in the Carti region, and abandoned goods from the drug trade provide occasional windfalls.

History

Contemporary traditional Guna houses in the Guna Yala built on stilts over shallow coastal marshes

The Gunas were living in what is now Northern Colombia and the Darién Province of Panama at the time of the Spanish invasion, and only later began to move westward towards what is now Guna Yala due to a conflict with the Spanish and other indigenous groups. Centuries before the conquest, the Gunas arrived in South America as part of a Chibchan migration moving east from Central America. At the time of the Spanish invasion, they were living in the region of Uraba and near the borders of what are now Antioquia and Caldas. Alonso de Ojeda and Vasco Núñez de Balboa explored the coast of Colombia in 1500 and 1501. They spent the most time in the Gulf of Urabá, where they made contact with the Gunas.

In far Eastern Guna Yala, the community of New Caledonia is near the site where Scottish explorers tried, unsuccessfully, to establish a colony in the "New World". The bankruptcy of the expedition has been cited as one of the motivations of the 1707 Acts of Union.

There is a wide consensus regarding the migrations of Gunas from Colombia and the Darien towards what is now Guna Yala. These migrations were caused partly by wars with the Catio people, but some sources contend that they were mostly due to bad treatment by the Spanish invaders. The Guna themselves attribute their migration to Guna Yala to conflicts with the native peoples, and their migration to the islands to the excessive mosquito populations on the mainland.

During the first decades of the twentieth century, the Panamanian government attempted to suppress many of the traditional customs. This was bitterly resisted, culminating in a short-lived yet successful revolt in 1925 known as the Dule Revolution (or "people revolution") – led by Iguaibilikinya Nele Kantule of Ustupu and supported by American adventurer and part-time diplomat Richard Marsh[7] – and a treaty in which the Panamanians agreed to give the Guna some degree of cultural autonomy.[7]

The San Blas Islands could be rendered uninhabitable by sea level rise in the late 21st century.[8]

Language

The Kuna language is a Native American language of the Chibchan family spoken by 50,000 to 70,000 people. Dulegaya is the primary language of daily life in the comarcas, and the majority of Guna children speak the language. Although it is relatively viable, Guna is considered an endangered language.

Spanish is also widely used, especially in education and written documents.

Health

The Guna have been shown to have a low average blood pressure (BP, 110/70 mm Hg), and, do not experience the age-related increase in blood pressure that is common in Western society.[9] Death rates from cardiovascular disease (CVD) and cancer – the #1 and #2 causes of death in the US – are low in the Guna. Between 2000 and 2004 on the mainland of Panama, for every 100,000 residents, 119 died from CVD and 74 died from cancer; in contrast, per 100,000 Guna, these death rates were 8 for CVD and 4 for cancer.[10]

Albinism

The Guna have a high incidence rate of albinism,[11] which led to their nickname of "White Indians" in the early 1900s.[12][13] In Guna mythology, albinos (or "sipu") were given a special place and are considered a special race of people.[11] They have the specific duty of defending the Moon against a dragon which tries to eat it on occasion during a lunar eclipse, and only they are allowed to go outside on the night of a lunar eclipse and to use specially-made bows and arrows to shoot down the dragon.[14]

  1. ^ Wetter, Renate (2009). "Mola History". PANAMA MOLA. Archived from the original on 16 September 2010. Retrieved 17 October 2010. 
  2. ^ "Lenguaje – ¿Guna, kuna o cuna?: James Howe" [Language – Guna, kuna or cuna?: James Howe]. La Prensa (in Spanish). 22 February 2014. 
  3. ^ Erice, Jesus (1985), Diccionario de la Lengua Kuna, Impresora La Nacion (INAC) 
  4. ^ "Nuestras Autoridades de Kuna Yala" [Our Authorities of Kuna Yala]. Comarca Kuna Yala / Congreso Generales Kunas. 12 October 2006. Archived from the original on 18 February 2007. 
  5. ^ "Segunda parte de mi Viaje a Panamá:El Mundo de los Gunas; Capítulo I , Historia y Organización Política – El Mundo de los Gunas – Historia y Organización Política, Parte 1" [Second part of my Trip to Panama: The World of the Gunas; Chapter I, History and Political Organization – The World of the Gunas – History and Political Organization, Part 1]. paseandote por el peru...y el mundo (in Spanish). May 10, 2013. Retrieved 15 October 2017. 
  6. ^ "Panama - Native Peoples". Flags Of The World. CRW Flags Inc. 22 May 2014. Retrieved 15 October 2017. 
  7. ^ a b Howe, James (1998). A people who would not kneel: Panama, the United States, and the San Blas Kuna. Smithsonian Series in Ethnographic Inquiry. Smithsonian Institution Press. ISBN 978-1-56098-890-8. 
  8. ^ McCleland, Jacob (12 November 2015). "Rising Sea Levels Threaten Tiny Islands Home To Indigenous Panamanians". NPR. All Things Considered. National Public Radio. Retrieved 15 October 2017. 
  9. ^ Hollenberg, Norman K.; Martinez, Gregorio; McCullough, Marji; Meinking, Terri; Passan, Diane; Preston, Mack; Rivera, Alicio; Taplin, David; Vicaria-Clement, Maureen (1997). "Aging, Acculturation, Salt Intake, and Hypertension in the Kuna of Panama" (PDF). Hypertension. 29: 171–176. doi:10.1161/01.HYP.29.1.171. PMID 9039098. 
  10. ^ Bayard, V; Chamorro, F; Motta, J; Hollenberg, NK (27 January 2007). "Does flavanol intake influence mortality from nitric oxide-dependent processes? Ischemic heart disease, stroke, diabetes mellitus, and cancer in Panama". Int J Med Sci. 4 (1): 53–58. 
  11. ^ a b Jeambrun, P. (August 1998). "L'albinisme oculocutané: mises au point clinique, historique et anthropologique" [Oculocutaneous albinism: clinical, historical and anthropological aspects]. Archives de Pédiatrie (in French). Société française de pédiatrie. 5 (8): 896–907. doi:10.1016/S0929-693X(98)80136-X. PMID 9759297. 
  12. ^ PROCEEDINGS OF THE BOARD OF REGENTS OF THE SMITHSONIAN INSTITUTION AT THE ANNUAL MEETING HELD DECEMBER 9, 1926, Smithsonian Institution, December 9, 1926, A paper by Miss Frances Densmore discusses the music and songs of the Tule Indians of Panama - the so-called "white Indians". 
  13. ^ Marsh, Richard Oglesby (1934). White Indians of Darien. New York, New York: G. P. Putnam's Sons. 
  14. ^ Jeambrun, Pascale; Sergent, Bernard (1991). Les enfants de la lune: L'albinisme chez les Amérindiens [Children of the Moon: Albinism among the Amerindians] (PDF) (in French). Paris: Éditions INSERM. pp. 238–239. ISBN 2-85598-488-2. 

Further reading



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Countries & Continents

3D,cad,europe,americas,apac,emea,asia,australia,africa,