powered by CADENAS

Social Share

Amazon

solidThinking (1986 views - Animation & Rendering & Toon)

solidThinking is a software company developing Evolve, a 3D modeling and rendering software and Inspire, a concept generation tool.
Go to Article

Explanation by Hotspot Model

solidThinking

solidThinking

solidThinking Inc.
Private
Website www.solidthinking.com

solidThinking is a software company developing Evolve, a 3D modeling and rendering software and Inspire, a concept generation tool.

History

The design software was originally developed for NEXTSTEP, the operating system developed by NeXT, and it was soon awarded as the best new application in the "CAD and 3D" category at NeXTWORLD EXPO held in San Francisco in June 1993.

A complete re-write of the application for the Windows platform started in 1997 and was completed in 1998 with the release of solidThinking 3.0 for Windows. The Construction History and an extensive NURBS modeling toolset were the main additions. One year later solidThinking for Mac OS X was also released. Today all releases of solidThinking are simultaneously developed for both Windows and Mac OS X.[1]

solidThinking version 8.0 and solidThinking Inspired 8.0, introducing the morphogenesis[2] form-generation technology, were released in September 2009.

With the 9.0 release, solidThinking became Evolve and solidThinking Inspired became Inspire, both sold under the solidThinking brand.



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Animation & Rendering & Toon

Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, toon, cartoon