Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 2.5 (Haragayato).
This article needs additional citations for verification. Please help improve this article by adding citations to reliable sources. Unsourced material may be challenged and removed. (April 2017) (Learn how and when to remove this template message) |
A self-tapping screw is a screw that can tap its own hole as it is driven into the material. For hard substrates such as metal or hard plastics, the self-tapping ability is often created by cutting a gap in the continuity of the thread on the screw, generating a flute and cutting edge similar to those on a tap. Thus, whereas a regular machine screw cannot tap its own hole in a metal substrate, a self-tapping one can (within reasonable limits of substrate hardness and depth). For softer substrates such as wood or soft plastics, the self-tapping ability can come simply from a tip that tapers to a gimlet point (in which no flute is needed). Like the tip of a nail or gimlet, such a point forms the hole by displacement of the surrounding material rather than any chip-forming drilling/cutting/evacuating action.
Some self-tapping screws are also self-drilling, which means that, in addition to the tap-like flute in the leading threads, there is also a preliminary drill-like fluted tip that looks much like the tip of a center drill. These screws combine a thrilling-like action and the fastener installation itself into only one driving motion (instead of separate drilling, tapping, and installing motions); they are thus very efficient in a variety of hard-substrate applications, from assembly lines to roofing.
Sheet metal screws (sometimes called "sheet-metal self-tappers", or P-K screws from the brand name Parker Kalon - who pioneered[1] the manufacture of, but did not invent, these screws) are a type of self-tapping screw despite the thread created in the sheet of metal being small. Pan-head PK Self-tapping screws are common in electrical equipment,[2] while flatter-headed truss or flat countersunk headed self-tapping screws[3] are more common in aviation applications.
Winged self-drilling have thin wings wider than the thread formed just behind the self drilling head. These cut a clearance hole in soft materials (such as wood or plastic), but are destroyed by more robust materials (such as metal). Thus, to clamp some material to metal, the clearance drilling, tap drilling, thread tapping, and fixing itself can happen in a single operation from one side, with the materials in their final position.
Self-tapping screws are used in a variety of applications ranging from DIY carpentry to surgery. Many dental implants and orthopedic bone screws are examples of self-tapping screws used in surgery.[4]
Self-tapping screws can be divided into two classes;[5] those that displace material (especially plastic and thin metal sheets) without removing it are termed thread-forming self-tapping screws; self-tappers with sharp cutting surfaces that remove the material as they are inserted are termed self-cutting.
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD