powered by CADENAS

Social Share

Light table (9548 views - Electronics & PCB Engineering)

A light table is a viewing device that is used to review photographic film or artwork placed on top of it. A horizontal form of a self-standing lightbox, it provides even illumination of the subject from below through a translucent cover and fluorescent lights that emit little heat. Some light tables may be like big light boxes horizontally standing on some type of support (legs) allowing to lay sheets of paper or films on their work surface to easily view or trace them while being comfortably seated on an office chair, but others are big complicated affairs with stereoscopes integrated as an autosupported unit. That kind is used by Tomcat TARPS squadrons for interpreting aerial photographs. They are mainly used in the trades of graphics to trace designs, especially in the world of cartoon or comics. Another use is for example to review film negatives, photoliths or any kind artwork that can be placed on top of a table for working with it. In general: professional tracing, animation, cartoons, design and drawing creation, education, architecture, interior design, fashion, in hospitals for viewing radiographs (X-rays, MRI, etc. ..)
Go to Article

Explanation by Hotspot Model

Light table

Light table

Light table

A light table[1] is a viewing device that is used to review photographic film or artwork placed on top of it. A horizontal form of a self-standing lightbox, it provides even illumination of the subject from below through a translucent cover and fluorescent lights that emit little heat.

Some light tables may be like big light boxes horizontally standing on some type of support (legs) allowing to lay sheets of paper or films on their work surface to easily view or trace them while being comfortably seated on an office chair, but others are big complicated affairs with stereoscopes integrated as an autosupported unit. That kind is used by Tomcat TARPS squadrons for interpreting aerial photographs.

They are mainly used in the trades of graphics to trace designs, especially in the world of cartoon or comics. Another use is for example to review film negatives, photoliths or any kind artwork that can be placed on top of a table for working with it.

In general: professional tracing, animation, cartoons, design and drawing creation, education, architecture, interior design, fashion, in hospitals for viewing radiographs (X-rays, MRI, etc. ..)

TARPS

Tactical Airborne Reconnaissance Pod System squadrons were staffed with Navy photographer's mates that maintained the cameras and worked with the carrier to process the imagery. TARPS squadrons also included an extra Intelligence officer and Intelligence Specialists to help plan TARPS missions and exploit the imagery afterwards.

The TARPS shop maintained the cameras and removed or loaded the pod when and if needed. Wet film processing was conducted in a processing room connected to the ship's Intelligence Center (CVIC) where the Intelligence Specialists has a dedicated space with a light table for analyzing the hundreds of feet of film and exploiting the data.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electronics & PCB Engineering

Cadence, Mentor Graphics, Eagle CAD, Altium Designer, AUTODESK EAGLE, Cadence Allegro, DesignSpark PCB , Mentor PADS, Mentor Xpedition, Novarm DipTrace, Pulsonix, TARGET 3001!, Xpedition xDX Designer, Zuken CADSTAR, Altium P-CAD, Agnisys, Altera Quartus, OrCAD, kiCAD, Solido Design Automation, ELectronics, PCB, Curcuit Board, 3D drawings, 3D library, 3D content, PCB Design, 2D symbols, 2D drawings, 2D icons, 2D schematics