powered by CADENAS

Social Share

Titanium hydride (24772 views - Material Database)

Titanium hydride normally refers to the inorganic compound TiH2 and related nonstoichiometric materials. It is commercially available as a stable grey/black powder, which is used as an additive in the production of Alnico sintered magnets, in the sintering of powdered metals, the production of metal foam, the production of powdered titanium metal and in pyrotechnics.
Go to Article

Titanium hydride

Titanium hydride

Titanium hydride

Titanium hydride powder
Names
IUPAC name
titanium dihydride (hydrogen deficient)
Identifiers
ECHA InfoCard 100.028.843
Properties
TiH2−x
Molar mass 49.88 g/mol (TiH2)
Appearance black powder (commercial form)
Density 3.76 g/cm3 (typical commercial form)
Melting point 350 °C (662 °F; 623 K) approximately
Except where otherwise noted, data are given for materials in their standard state (at 25 °C [77 °F], 100 kPa).
Y verify (what is YN ?)
Infobox references

Titanium hydride normally refers to the inorganic compound TiH2 and related nonstoichiometric materials.[1][2] It is commercially available as a stable grey/black powder, which is used as an additive in the production of Alnico sintered magnets, in the sintering of powdered metals, the production of metal foam, the production of powdered titanium metal and in pyrotechnics.[3]

Production and reactions of TiH(2-x)

In the commercial process for producing non-stoichiometric TiH(2-x), titanium metal sponge is treated with hydrogen gas at atmospheric pressure at between 300-500 °C. Absorption of hydrogen is exothermic and rapid, changing the color of the sponge grey/black. The brittle product is ground to a powder, which has a composition around TiH1.95.[3] In the laboratory, titanium hydride is produced by heating titanium powder under flowing hydrogen at 700 °C, the idealized equation being:[4]

Ti + H2 → TiH2

Other methods of producing titanium hydride include electrochemical and ball milling methods.[5][6]

Reactions

TiH1.95 is unaffected by water and air. It is slowly attacked by strong acids and is degraded by hydrofluoric and hot sulfuric acids. It reacts rapidly with oxidising agents, this reactivity leading to the use of titanium hydride in pyrotechnics.[3]

The material has been used to produce highly pure hydrogen, which is released upon heating the solid starting at 300 °C.[4] Only at the melting point of titanium is dissociation complete.[3] Titanium tritiide has been proposed for the long-term storage of tritium gas.[7]

Structure

As TiHx approaches stoichiometry, it adopts a distorted body-centered tetragonal structure, termed the ε-form with an axial ratio of less than 1. This composition is very unstable with respect to partial thermal decomposition, unless maintained under a pure hydrogen atmosphere. Otherwise, the composition rapidly decomposes at room temperature until an approximate composition of TiH1.74 is reached. This composition adopts the fluorite structure, and is termed the δ-form, and only very slowly thermally decomposing at room temperature until an approximate composition of TiH1.47 is reached, at which point, inclusions of the hexagonal close packed α-form, which is the same form as pure titanium, begin to appear.

The evolution of the dihydride from titanium metal and hydrogen has been examined in some detail. α-Titanium has an hexagonal close packed (hcp) structure at room temperature. Hydrogen initially occupies tetrahedral interstitial sites in the titanium. As the H/Ti ratio approaches 2, the material adopts the β-form to a face centred cubic (fcc), δ- form, the H atoms eventually filling all the tetrahedral sites to give the limiting stoichiometry of TiH2. The various phases are described in the table below.

Temperature approx. 500 °C,taken from illustration[8]
Phase Weight % H Atomic % H TiHx Metal lattice
α- 0 - 0.2 0 - 8 hcp
α- & β- 0.2 - 1.1 8 - 34 TiH0.1 - TiH0.5
β- 1.1 - 1.8 34 - 47 TiH0.5 - TiH0.9 bcc
β- & δ 1.8 - 2.5 47 - 57 TiH0.9 - TiH1.32
δ- 2.7 - 4.1 57- 67 TiH1.32 - TiH2 fcc

If titanium hydride contains 4.0% hydrogen at less than around 40 °C then it transforms into a body-centred tetragonal (bct) structure called ε-titanium.[8]

When titanium hydrides with less than 1.3% hydrogen, known as hypoeutectoid titanium hydride are cooled, the β-titanium phase of the mixture attempts to revert to the α-titanium phase, resulting in an excess of hydrogen. One way for hydrogen to leave the β-titanium phase is for the titanium to partially transform into δ-titanium, leaving behind titanium that is low enough in hydrogen to take the form of α-titanium, resulting in an α-titanium matrix with δ-titanium inclusions.

A metastable γ-titanium hydride phase has been reported.[9] When α-titanium hydride with a hydrogen content of 0.02-0.06% is quenched rapidly, it forms into γ-titanium hydride, as the atoms "freeze" in place when the cell structure changes from hcp to fcc. γ-Titanium takes a body centred tetragonal (bct) structure. Moreover, there is no compositional change so the atoms generally retain their same neighbours.

Hydrogen embrittlement titanium and titanium alloys

The absorption of hydrogen and the formation of titanium hydride are a source of damage to titanium and titanium alloys (Ti /Ti alloys). This hydrogen embrittlement process is of particular concern when titanium and alloys are used as structural materials, as in nuclear reactors.

Hydrogen embrittlement manifests as a reduction in ductility and eventually spalling of titanium surfaces. The effect of hydrogen is to a large extent determined by the composition, metallurgical history and handling of the Ti /Ti alloy.[10] CP-titanium (commercially pure: ≤99.55% Ti content) is more susceptible to hydrogen attack than pure α-titanium. Embrittlement, observed as a reduction in ductility and caused by the formation of a solid solution of hydrogen, can occur in CP-titanium at concentrations as low as 30-40 ppm. Hydride formation has been linked to the presence of iron in the surface of a Ti alloy. Hydride particles are observed in specimens of Ti /Ti alloys that have been welded, and because of this welding is often carried out under an inert gas shield to reduce the possibility of hydride formation.[10]

Ti /Ti alloys form a surface oxide layer, composed of a mixture of Ti(II), Ti(III) and Ti(IV) oxides,[11] which offers a degree of protection to hydrogen entering the bulk.[10] The thickness of this can be increased by anodizing, a process which also results in a distinctive colouration of the material. Ti /Ti alloys are often used in hydrogen containing environments and in conditions where hydrogen is reduced electrolytically on the surface. Pickling, an acid bath treatment which is used to clean the surface can be a source of hydrogen.

Uses

Common applications include ceramics, pyrotechnics, sports equipment, as a laboratory reagent, as a blowing agent, and as a precursor to porous titanium. When heated as a mixture with other metals in powder metallurgy, titanium hydride releases hydrogen which serves to remove carbon and oxygen, producing a strong alloy.[3]


  1. ^ Greenwood, Norman N.; Earnshaw, Alan (1997). Chemistry of the Elements (2nd ed.). Butterworth-Heinemann. ISBN 0-08-037941-9. 
  2. ^ Holleman, A. F.; Wiberg, E. "Inorganic Chemistry" Academic Press: San Diego, 2001. ISBN 0-12-352651-5.
  3. ^ a b c d e Rittmeyer, Peter; Weitelmann, Ulrich (2005). "Hydrides". Ullmann's Encyclopedia of Industrial Chemistry. Wiley-VCH. doi:10.1002/14356007.a13_199. 
  4. ^ a b M. Baudler "Hydrogen, Deuterium, Water" in Handbook of Preparative Inorganic Chemistry, 2nd Ed. Edited by G. Brauer, Academic Press, 1963, NY. Vol. 1. p. 114-115.
  5. ^ Millenbach, Pauline; Givon, Meir (1 October 1982). "The electrochemical formation of titanium hydride". Journal of the Less Common Metals. 87 (2): 179–184. doi:10.1016/0022-5088(82)90086-8. Retrieved 10 March 2013. 
  6. ^ Zhang, Heng; Kisi, Erich H (1997). "Formation of titanium hydride at room temperature by ball milling". Journal of Physics: Condensed Matter. 9 (11): L185–L190. ISSN 0953-8984. doi:10.1088/0953-8984/9/11/005. 
  7. ^ Brown, Charles C.; Buxbaum, Robert E. (June 1988). "Kinetics of hydrogen absorption in alpha titanium". Metallurgical Transactions A. 19 (6): 1425–1427. doi:10.1007/bf02674016. Retrieved 16 February 2013. 
  8. ^ a b Fukai, Y (2005). The Metal-Hydrogen System, Basic Bulk Properties, 2d edition. Springer. ISBN 978-3-540-00494-3. 
  9. ^ Numakura, H; Koiwa, M; Asano, H; Izumi, F (1988). "Neutron diffraction study of the metastable γ titanium deuteride". Acta Metallurgica. 36 (8): 2267–2273. ISSN 0001-6160. doi:10.1016/0001-6160(88)90326-4. 
  10. ^ a b c Donachie, Matthew J. (2000). Titanium: A Technical Guide. ASM International. ISBN 0-87170-686-5. 
  11. ^ Lu, Gang; Bernasek, Steven L.; Schwartz, Jeffrey (2000). "Oxidation of a polycrystalline titanium surface by oxygen and water". Surface Science. 458 (1-3): 80–90. Bibcode:2000SurSc.458...80L. ISSN 0039-6028. doi:10.1016/S0039-6028(00)00420-9. 

クロムモリブデン鋼AL-6XNAlGaAlloy 20アルニコ磁石Alumelアルミニウムアルミニウム合金アルミニウム青銅Aluminium-lithium alloyアマルガムArgentium sterling silverArsenical bronzeArsenical copperBell metalベリリウムベリリウム銅ビロンBirmabrightBismanolビスマス黄銅BrightrayBritannia silver青銅Bulat steelCalamine brass鋳鉄CelestriumChinese silverChromelクロムChromium hydrideコバルトホワイトゴールドコンスタンタン水素化銅Copper–tungstenCorinthian bronzeCrown goldCrucible steelクニフェ白銅Cymbal alloysダマスカス鋼デバルダ合金Doré bullionジュラルミンDutch metalケイ素鋼エレクトロン貨Elektron (alloy)エリンバーFernicoフェロアロイフェロセリウムフェロクロムフェロマンガンフェロモリブデンFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolガリンスタンガリウムGilding metalガラスGlucydurGoloidGuanín (bronze)Gum metal砲金Haynes InternationalHepatizonHiduminium高速度鋼高張力鋼HydronaliumインコネルインジウムインバーIron–hydrogen alloyItalmaKanthal (alloy)コバールリチウムMagnaliumマグネシウムマグノックス高マンガン鋼マンガニンマルエージング鋼Marine grade stainlessMartensitic stainless steelMegalliumMelchior (alloy)マーキュリーミッシュメタルMolybdochalkosモネルMu-metalMuntz metalMushet steelニクロムニッケルNickel hydride洋白Nickel titaniumNicrosilNisilノルディック・ゴールドOrmoluパーマロイリン青銅銑鉄Pinchbeck (alloy)合成樹脂Platinum sterlingPlexiglasプルトニウムプルトニウムガリウム合金カリウムPseudo palladiumReynolds 531RhoditeロジウムRose's metalサマリウムサマリウムコバルト磁石Sanicro 28スカンジウムScandium hydride赤銅 (合金)四分一 (合金)Silver steelナトリウムナトリウムカリウム合金はんだスペキュラム合金スピーゲルばね鋼Staballoyステンレス鋼ステライトスターリングシルバー鉄骨構造SupermalloySurgical stainless steelTerfenol-DTerneTibetan silverスズチタンチタン合金Titanium Beta Cトムバック工具鋼Tumbaga活字合金ウランVitallium耐候性鋼ウッドメタルWootz steelY alloyZeron 100亜鉛ジルコニウムTitanium gold窒化チタンバビットメタルBritannia metalピューターQueen's metalWhite metal水素化ウラン(III)ZamakZirconium hydride水素ヘリウムホウ素窒素酸素フッ素メタン中二階原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification