powered by CADENAS

Social Share

Gum metal (9631 views - Material Database)

Gum metal, also called TNTZ, is a unique titanium alloy with high elasticity, ductility, and yield strength. While originally developed with a composition of 23% niobium, 0.7% tantalum, 2% zirconium, and 1% oxygen, it can exist over a range of compositions and also include vanadium and hafnium. Applying cold work to gum metal actually decreases its elastic modulus, with reported shear moduli as low as 20 gigapascals (2,900,000 psi). At the same time, cold work increases gum metal's yield strength. By using a heat treatment after this cold work, some elasticity can be sacrificed for even greater strength, with yield strengths ranging as high as 2 gigapascals (290,000 psi), on par with some of the strongest steels. "Gum metal" is a registered trademark of Toyota Central R&D Labs and was initially developed there. The results of that research were first published in April 2003.
Go to Article

Gum metal

Gum metal

Gum metal, also called TNTZ, is a unique titanium alloy with high elasticity, ductility, and yield strength. While originally developed with a composition of 23% niobium, 0.7% tantalum, 2% zirconium, and 1% oxygen, it can exist over a range of compositions and also include vanadium and hafnium.[1][2]

Applying cold work to gum metal actually decreases its elastic modulus,[1] with reported shear moduli as low as 20 gigapascals (2,900,000 psi).[3] At the same time, cold work increases gum metal's yield strength.[1] By using a heat treatment after this cold work, some elasticity can be sacrificed for even greater strength, with yield strengths ranging as high as 2 gigapascals (290,000 psi), on par with some of the strongest steels.[3]

"Gum metal" is a registered trademark of Toyota Central R&D Labs and was initially developed there. The results of that research were first published in April 2003.[3]

  1. ^ a b c Saito, Takashi; Furuta, Tadahiko; Hwang, Jung-Hwan; Kuramoto, Shigeru; Nishino, Kazuaki; Suzuki, Nobuaki; Chen, Rong; Yamada, Akira; Ito, Kazuhiko; Seno, Yoshiki; Nonaka, Takamasa; Ikehata, Hideaki; Nagasako, Naoyuki; Iwamoto, Chihiro; Ikuhara, Yuuichi; Sakuma, Taketo (18 April 2003). "Multifunctional Alloys Obtained via a Dislocation-Free Plastic Deformation Mechanism". Science. American Association for the Advancement of Science. 300 (5618): 464–7. PMID 12702870. doi:10.1126/science.1081957. 
  2. ^ Talling, RJ; Dashwood, RJ; Jackson, M; Dye, D (June 2009). "Compositional variability in gum metal". Scripta Materialia. Elsevier. 60 (11): 1000–3. doi:10.1016/j.scriptamat.2009.02.044. 
  3. ^ a b c Nishino, Kazuaki (September 2003). "Super Multifunctional Alloy "GUM METAL"" (PDF). R&D Review of Toyota CRDL. Nagakute, Japan: Toyota Central R&D Labs. 38 (3): 50. ISSN 1347-9652. Retrieved 29 July 2011. 

クロムモリブデン鋼AL-6XNAlGaAlloy 20アルニコ磁石Alumelアルミニウムアルミニウム合金アルミニウム青銅Aluminium-lithium alloyアマルガムArgentium sterling silverArsenical bronzeArsenical copperBell metalベリリウムベリリウム銅ビロンBirmabrightBismanolビスマス黄銅BrightrayBritannia silver青銅Bulat steelCalamine brass鋳鉄CelestriumChinese silverChromelクロムChromium hydrideコバルトホワイトゴールドコンスタンタン水素化銅Copper–tungstenCorinthian bronzeCrown goldCrucible steelクニフェ白銅Cymbal alloysダマスカス鋼デバルダ合金Doré bullionジュラルミンDutch metalケイ素鋼エレクトロン貨Elektron (alloy)エリンバーFernicoフェロアロイフェロセリウムフェロクロムフェロマンガンフェロモリブデンFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolガリンスタンガリウムGilding metalガラスGlucydurGoloidGuanín (bronze)砲金Haynes InternationalHepatizonHiduminium高速度鋼高張力鋼HydronaliumインコネルインジウムインバーIron–hydrogen alloyItalmaKanthal (alloy)コバールリチウムMagnaliumマグネシウムマグノックス高マンガン鋼マンガニンマルエージング鋼Marine grade stainlessMartensitic stainless steelMegalliumMelchior (alloy)マーキュリーミッシュメタルMolybdochalkosモネルMu-metalMuntz metalMushet steelニクロムニッケルNickel hydride洋白Nickel titaniumNicrosilNisilノルディック・ゴールドOrmoluパーマロイリン青銅銑鉄Pinchbeck (alloy)合成樹脂Platinum sterlingPlexiglasプルトニウムプルトニウムガリウム合金カリウムPseudo palladiumReynolds 531RhoditeロジウムRose's metalサマリウムサマリウムコバルト磁石Sanicro 28スカンジウムScandium hydride赤銅 (合金)四分一 (合金)Silver steelナトリウムナトリウムカリウム合金はんだスペキュラム合金スピーゲルばね鋼Staballoyステンレス鋼ステライトスターリングシルバー鉄骨構造SupermalloySurgical stainless steelTerfenol-DTerneTibetan silverスズチタンチタン合金Titanium Beta Cトムバック工具鋼Tumbaga活字合金ウランVitallium耐候性鋼ウッドメタルWootz steelY alloyZeron 100亜鉛ジルコニウムTitanium hydrideTitanium gold窒化チタンバビットメタルBritannia metalピューターQueen's metalWhite metal水素化ウラン(III)ZamakZirconium hydride水素ヘリウムホウ素窒素酸素フッ素メタン中二階原子ゴムHoning (metalworking)金属加工材料工学

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification