powered by CADENAS

Social Share

Platinum sterling (8954 views - Material Database)

Platinum Sterling is a registered trademark name of ABI Precious Metals, Inc. The trademark covers a range of alloys whose primary constituents are platinum and silver, primarily used in jewellery. The range of Platinum Sterling alloys was developed in 2003 by Marc Robinson, and its solder was created by Chuck Bennett.
Go to Article

Platinum sterling

Platinum sterling

Platinum Sterling is a registered trademark name of ABI Precious Metals, Inc. The trademark covers a range of alloys whose primary constituents are platinum and silver, primarily used in jewellery.[1] The range of Platinum Sterling alloys was developed in 2003 by Marc Robinson, and its solder was created by Chuck Bennett.

Properties

The platinum is used to replace at least some of the copper present in a typical sterling silver alloy, which provides a greater light reflectivity (by refining the grain structure) and resistance to tarnish (thought to be caused by oxidation of copper) than standard sterling silver.

Platinum Sterling is a cheaper alternative to white gold.[citation needed] It is also allegedly hard wearing and very white and so does not require rhodium plating like white gold.[2]

Composition

The composition of Platinum Sterling is published; three alloys are commercially available, all containing standard 92.5% sterling silver and 1%, 3.5% or 5% platinum.[3] A small amount of gallium can also be added to the alloy to ease manufacturing.

The patent application for Platinum Sterling claims:

A metal alloy having a composition consisting essentially of 90.5–95.5% silver by weight, about 0.5–6% platinum by weight, about 0.7–4% copper by weight, about 0.1–2% gallium by weight, about 1–3% tin by weight, about 1–2.5% germanium by weight, about 0.5–4% zinc by weight, and about 0.1–0.2% silicon by weight.
— [4]

The claim also states:

...the preferred embodiments of the present invention provide a metal alloy comprising about 90.5–95.5% silver, about 0.5–6% platinum, about 0.7–4% copper, and about 0.1–2% gallium. In some embodiments, the alloy further comprises about 0.5–4% zinc, about 0–0.2% silicon, about 0–0.3% boron and about 0–1.5% indium. In other embodiments, the alloy further comprises about 0–3% tin and about 0–2.5% germanium.

See also


クロムモリブデン鋼AL-6XNAlGaAlloy 20アルニコ磁石Alumelアルミニウムアルミニウム合金アルミニウム青銅Aluminium-lithium alloyアマルガムArgentium sterling silverArsenical bronzeArsenical copperBell metalベリリウムベリリウム銅ビロンBirmabrightBismanolビスマス黄銅BrightrayBritannia silver青銅Bulat steelCalamine brass鋳鉄CelestriumChinese silverChromelクロムChromium hydrideコバルトホワイトゴールドコンスタンタン水素化銅Copper–tungstenCorinthian bronzeCrown goldCrucible steelクニフェ白銅Cymbal alloysダマスカス鋼デバルダ合金Doré bullionジュラルミンDutch metalケイ素鋼エレクトロン貨Elektron (alloy)エリンバーFernicoフェロアロイフェロセリウムフェロクロムフェロマンガンフェロモリブデンFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolガリンスタンガリウムGilding metalガラスGlucydurGoloidGuanín (bronze)砲金Haynes InternationalHepatizonHiduminium高速度鋼高張力鋼HydronaliumインコネルインジウムインバーIron–hydrogen alloyItalmaKanthal (alloy)コバールリチウムMagnaliumマグネシウムマグノックス高マンガン鋼マンガニンマルエージング鋼Marine grade stainlessMartensitic stainless steelMegalliumMelchior (alloy)マーキュリーミッシュメタルMolybdochalkosモネルMu-metalMuntz metalMushet steelニクロムニッケルNickel hydride洋白Nickel titaniumNicrosilNisilノルディック・ゴールドOrmoluパーマロイリン青銅銑鉄Pinchbeck (alloy)合成樹脂Plexiglasプルトニウムプルトニウムガリウム合金カリウムPseudo palladiumReynolds 531RhoditeロジウムRose's metalサマリウムサマリウムコバルト磁石Sanicro 28スカンジウムScandium hydride赤銅 (合金)Silver steelナトリウムナトリウムカリウム合金はんだスペキュラム合金スピーゲルばね鋼Staballoyステンレス鋼ステライト鉄骨構造SupermalloySurgical stainless steelTerfenol-DTerneスズチタントムバック工具鋼Tumbaga活字合金ウランVitallium耐候性鋼ウッドメタルWootz steelY alloyZeron 100亜鉛ジルコニウム四分一 (合金)スターリングシルバーTibetan silverTitanium Beta Cチタン合金Titanium hydrideGum metalTitanium gold窒化チタンバビットメタルBritannia metalピューターQueen's metalWhite metal水素化ウラン(III)ZamakZirconium hydride水素ヘリウムホウ素窒素酸素フッ素メタン中二階原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification