powered by CADENAS

Social Share

Scandium hydride (7832 views - Material Database)

Scandium hydride, also known as scandium–hydrogen alloy, is an alloy made by combining scandium and hydrogen. Hydrogen acts as a hardening agent, preventing dislocations in the scandium atom crystal lattice from sliding past one another. Varying the amount of hydrogen controls qualities such as the hardness of the resulting scandium hydride. Scandium hydride with increased hydrogen content can be made harder than scandium. It can be formed by progressive hydrogenation of scandium foil with hydrogen. In the narrow range of concentrations which make up scandium hydride, mixtures of hydrogen and scandium can form two different structures. At room temperature, the most stable form of scandium is the hexagonal close-packed (HCP) structure α-scandium. It is a fairly soft metallic material that can dissolve a moderate concentration of hydrogen, no more than 0.89 wt% at 22 °C. If scandium hydride contains more than 0.89% hydrogen at room temperature then it transforms into a face-centred cubic (FCC) structure, the δ-phase. It can dissolve considerably more hydrogen, as much as 4.29%, which reflects the upper hydrogen content of scandium hydride. Research indicates the existence of a third phase created under extreme conditions termed the η-phase. This phase can dissolve as much as 6.30% hydrogen. Concentration dependent activation-energies are observed for hydrogen diffusion in scandium metal.
Go to Article

Scandium hydride

Scandium hydride

Scandium hydride, also known as scandium–hydrogen alloy, is an alloy made by combining scandium and hydrogen. Hydrogen acts as a hardening agent, preventing dislocations in the scandium atom crystal lattice from sliding past one another. Varying the amount of hydrogen controls qualities such as the hardness of the resulting scandium hydride. Scandium hydride with increased hydrogen content can be made harder than scandium.

It can be formed by progressive hydrogenation of scandium foil with hydrogen.[1]

In the narrow range of concentrations which make up scandium hydride, mixtures of hydrogen and scandium can form two different structures. At room temperature, the most stable form of scandium is the hexagonal close-packed (HCP) structure α-scandium.[2] It is a fairly soft metallic material that can dissolve a moderate concentration of hydrogen, no more than 0.89 wt% at 22 °C. If scandium hydride contains more than 0.89% hydrogen at room temperature then it transforms into a face-centred cubic (FCC) structure, the δ-phase. It can dissolve considerably more hydrogen, as much as 4.29%, which reflects the upper hydrogen content of scandium hydride.

Research indicates the existence of a third phase created under extreme conditions termed the η-phase. This phase can dissolve as much as 6.30% hydrogen.

Concentration dependent activation-energies are observed for hydrogen diffusion in scandium metal.[3]

  1. ^ Chemistry of d-block elements G. Singh (2007)
  2. ^ Manchester, F. D.; Pitre, J. M. (1997). "The H- SC (Hydrogen- Scandium) system". Journal of Phase Equilibria. 18 (2): 194–205. ISSN 1054-9714. doi:10.1007/BF02665706. 
  3. ^ Weaver, H. (1972). "Nuclear-Magnetic-Resonance Investigation of Proton Motion in Scandium Hydride". Physical Review B. 5 (5): 1663–1667. ISSN 0556-2805. doi:10.1103/PhysRevB.5.1663. 

クロムモリブデン鋼AL-6XNAlGaAlloy 20アルニコ磁石Alumelアルミニウムアルミニウム合金アルミニウム青銅Aluminium-lithium alloyアマルガムArsenical bronzeArsenical copperBell metalベリリウムベリリウム銅ビロンBirmabrightBismanolビスマス黄銅Brightray青銅Bulat steelCalamine brass鋳鉄CelestriumChinese silverChromelクロムChromium hydrideコバルトホワイトゴールドコンスタンタン水素化銅Copper–tungstenCorinthian bronzeCrown goldCrucible steelクニフェ白銅Cymbal alloysダマスカス鋼デバルダ合金ジュラルミンDutch metalケイ素鋼エレクトロン貨Elektron (alloy)エリンバーFernicoフェロアロイフェロセリウムフェロクロムフェロマンガンフェロモリブデンFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolガリンスタンガリウムGilding metalガラスGlucydurGuanín (bronze)砲金Haynes InternationalHepatizonHiduminium高速度鋼高張力鋼HydronaliumインコネルインジウムインバーIron–hydrogen alloyItalmaKanthal (alloy)コバールリチウムMagnaliumマグネシウムマグノックス高マンガン鋼マンガニンマルエージング鋼Marine grade stainlessMartensitic stainless steelMegalliumMelchior (alloy)マーキュリーミッシュメタルMolybdochalkosモネルMu-metalMuntz metalMushet steelニクロムニッケルNickel hydride洋白Nickel titaniumNicrosilNisilノルディック・ゴールドOrmoluパーマロイリン青銅銑鉄Pinchbeck (alloy)合成樹脂Plexiglasプルトニウムプルトニウムガリウム合金カリウムPseudo palladiumReynolds 531RhoditeロジウムRose's metalサマリウムSanicro 28スカンジウム赤銅 (合金)Silver steelナトリウムナトリウムカリウム合金はんだスペキュラム合金スピーゲルばね鋼Staballoyステンレス鋼ステライト鉄骨構造SupermalloySurgical stainless steelTerfenol-DTerneスズチタントムバック工具鋼Tumbaga活字合金ウランVitallium耐候性鋼ウッドメタルWootz steelY alloyZeron 100亜鉛ジルコニウムサマリウムコバルト磁石Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterling四分一 (合金)スターリングシルバーTibetan silverTitanium Beta Cチタン合金Titanium hydrideGum metalTitanium gold窒化チタンバビットメタルBritannia metalピューターQueen's metalWhite metal水素化ウラン(III)ZamakZirconium hydride水素ヘリウムホウ素窒素酸素フッ素メタン中二階原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification