powered by CADENAS

Social Share

Pseudo palladium (9217 views - Material Database)

Pseudo palladium (RhAg) is a binary alloy consisting of equal parts of rhodium (atomic number 45) and silver (atomic number 47) created using nanotechnology to create a far more homogenous mixture than might be possible using more conventional methods. This alloy exhibits properties of the intervening element palladium (atomic number 46).
Go to Article

Pseudo palladium

Pseudo palladium

Pseudo palladium

Pseudo palladium (RhAg) is a binary alloy consisting of equal parts of rhodium (atomic number 45) and silver (atomic number 47) created using nanotechnology to create a far more homogenous mixture than might be possible using more conventional methods. This alloy exhibits properties of the intervening element palladium (atomic number 46).

History

The production of this alloy was first reported by Kyoto University Professor Hiroshi Kitagawa and his research team, October 27, 2010.[1] To make the new alloy, the Kyoto team used nanotechnology to "nebulise" the rhodium and silver and gradually mixed them with heated alcohol, with the two metals mixed stably at the atomic level. The same team also produced alternatives to other kinds of rare metals.[2]

Characteristics

The new alloy has similar properties to palladium, which is used as a catalyst to cleanse exhaust gas and absorbs large quantities of hydrogen.

Rhodium, palladium and silver have 45, 46 and 47 electrons, respectively, numbers that determine their chemical characterizations.

"The orbits of the electrons in the rhodium and silver atoms probably got jumbled up and formed the same orbits as those of palladium," Kitagawa said.[3]

Applications

The alloy has similar properties to palladium, which is used in cars' emission-reducing catalytic converters as well as in computers, mobile phones, flatscreen TVs and dentistry instruments.

Hydrogen storage is cited as one potential use, however, according to researchers, the pseudo palladium alloy has only one half of palladium's hydrogen storage capacity.[4]

See also


クロムモリブデン鋼AL-6XNAlGaAlloy 20アルニコ磁石Alumelアルミニウムアルミニウム合金アルミニウム青銅Aluminium-lithium alloyアマルガムArsenical bronzeArsenical copperBell metalベリリウムベリリウム銅ビロンBirmabrightBismanolビスマス黄銅Brightray青銅Bulat steelCalamine brass鋳鉄CelestriumChinese silverChromelクロムChromium hydrideコバルトホワイトゴールドコンスタンタン水素化銅Copper–tungstenCorinthian bronzeCrown goldCrucible steelクニフェ白銅Cymbal alloysダマスカス鋼デバルダ合金ジュラルミンDutch metalケイ素鋼エレクトロン貨Elektron (alloy)エリンバーFernicoフェロアロイフェロセリウムフェロクロムフェロマンガンフェロモリブデンFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolガリンスタンガリウムGilding metalガラスGlucydurGuanín (bronze)砲金Haynes InternationalHepatizonHiduminium高速度鋼高張力鋼HydronaliumインコネルインジウムインバーIron–hydrogen alloyItalmaKanthal (alloy)コバールリチウムMagnaliumマグネシウムマグノックス高マンガン鋼マンガニンマルエージング鋼Marine grade stainlessMartensitic stainless steelMegalliumMelchior (alloy)マーキュリーミッシュメタルMolybdochalkosモネルMu-metalMuntz metalMushet steelニクロムニッケルNickel hydride洋白Nickel titaniumNicrosilNisilノルディック・ゴールドOrmoluパーマロイリン青銅銑鉄Pinchbeck (alloy)合成樹脂Plexiglasプルトニウムプルトニウムガリウム合金カリウムReynolds 531RhoditeロジウムRose's metalサマリウムSanicro 28スカンジウム赤銅 (合金)Silver steelナトリウムナトリウムカリウム合金はんだスペキュラム合金スピーゲルばね鋼Staballoyステンレス鋼ステライト鉄骨構造SupermalloySurgical stainless steelTerneスズチタントムバック工具鋼Tumbaga活字合金ウランVitallium耐候性鋼ウッドメタルWootz steelY alloyZeron 100亜鉛ジルコニウムTerfenol-DScandium hydrideサマリウムコバルト磁石Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterling四分一 (合金)スターリングシルバーTibetan silverTitanium Beta Cチタン合金Titanium hydrideGum metalTitanium gold窒化チタンバビットメタルBritannia metalピューターQueen's metalWhite metal水素化ウラン(III)ZamakZirconium hydride水素ヘリウムホウ素窒素酸素フッ素メタン中二階原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification