powered by CADENAS

Social Share

Martensitic stainless steel (13584 views - Material Database)

Martensitic stainless steel is a specific type of stainless steel alloy. Stainless steels may be classified by their crystalline structure into three main types: austenitic, ferritic and martensitic. Martensitic stainless steels can be high- or low-carbon steels built around the Type 410 composition of iron, 12% chromium, and up to 1.2% carbon. They are usually tempered and hardened. Tempered martensite gives steel good hardness and high toughness; used largely for medical tools (scalpels, razors and internal clamps). Untempered martensite is low in toughness and therefore brittle. The characteristic body-centered tetragonal martensite microstructure was first observed by German microscopist Adolf Martens around 1890. In 1912, Elwood Haynes applied for a U.S. patent on a martensitic stainless steel alloy. This patent was not granted until 1919. Martensitic stainless steel can be nondestructively tested using the magnetic particle inspection method, unlike austenitic stainless steel. Also in 1912, Harry Brearley of the Brown-Firth research laboratory in Sheffield, England, while seeking a corrosion-resistant alloy for gun barrels, discovered and subsequently industrialized a martensitic stainless steel alloy. The discovery was announced two years later in a January 1915 newspaper article in The New York Times. Brearly applied for a U.S. patent during 1915. This was later marketed under the "Staybrite" brand by Firth Vickers in England and was used for the new entrance canopy for the Savoy Hotel in 1929 in London.
Go to Article

Martensitic stainless steel

Martensitic stainless steel

Martensitic stainless steel is a specific type of stainless steel alloy.[1]

Stainless steels may be classified by their crystalline structure into three main types: austenitic, ferritic and martensitic. Martensitic stainless steels can be high-[1] or low-carbon steels built around the Type 410 composition of iron, 12% chromium, and up to 1.2% carbon.[2] They are usually tempered and hardened. Tempered martensite gives steel good hardness and high toughness; used largely for medical tools (scalpels, razors and internal clamps).[3] Untempered martensite is low in toughness and therefore brittle.

The characteristic body-centered tetragonal martensite microstructure was first observed by German microscopist Adolf Martens around 1890. In 1912, Elwood Haynes applied for a U.S. patent on a martensitic stainless steel alloy. This patent was not granted until 1919.[4]

Martensitic stainless steel can be nondestructively tested using the magnetic particle inspection method, unlike austenitic stainless steel.

Also in 1912, Harry Brearley of the Brown-Firth research laboratory in Sheffield, England, while seeking a corrosion-resistant alloy for gun barrels, discovered and subsequently industrialized a martensitic stainless steel alloy. The discovery was announced two years later in a January 1915 newspaper article in The New York Times.[5] Brearly applied for a U.S. patent during 1915. This was later marketed under the "Staybrite" brand by Firth Vickers in England and was used for the new entrance canopy for the Savoy Hotel in 1929 in London.[6]

See also


クロムモリブデン鋼AL-6XNAlGaAlloy 20アルニコ磁石アルミニウムアルミニウム合金アルミニウム青銅Aluminium-lithium alloyArsenical bronzeArsenical copperBell metalベリリウムベリリウム銅ビロンBirmabrightBismanolビスマス黄銅青銅Bulat steelCalamine brass鋳鉄CelestriumChinese silverクロムChromium hydrideコバルトホワイトゴールドコンスタンタン水素化銅Copper–tungstenCorinthian bronzeCrown goldCrucible steelクニフェ白銅Cymbal alloysダマスカス鋼デバルダ合金ジュラルミンDutch metalケイ素鋼エレクトロン貨エリンバーFernicoフェロアロイフェロセリウムフェロクロムフェロマンガンフェロモリブデンFerrosiliconFerrotitaniumFerrouraniumField's metalFlorentine bronzeGalfenolガリンスタンガリウムGilding metalガラスGlucydurGuanín (bronze)砲金HepatizonHiduminium高速度鋼高張力鋼HydronaliumインジウムインバーIron–hydrogen alloyItalmaKanthal (alloy)コバールMagnaliumマグネシウム高マンガン鋼マンガニンマルエージング鋼Marine grade stainlessMegalliumMelchior (alloy)マーキュリーMolybdochalkosMuntz metalMushet steelニクロムニッケル洋白ノルディック・ゴールドOrmoluリン青銅銑鉄Pinchbeck (alloy)合成樹脂PlexiglasプルトニウムカリウムReynolds 531RhoditeロジウムRose's metalサマリウムスカンジウム赤銅 (合金)ナトリウムスペキュラム合金スピーゲルばね鋼Staballoyステンレス鋼ステライト鉄骨構造スズチタントムバックTumbagaウランVitalliumウッドメタルY alloy亜鉛ジルコニウムSanicro 28Surgical stainless steelZeron 100Silver steel工具鋼耐候性鋼Wootz steelはんだTerne活字合金Elektron (alloy)アマルガムマグノックスAlumelBrightrayChromelHaynes InternationalインコネルモネルNicrosilNisilNickel titaniumMu-metalパーマロイSupermalloyNickel hydrideプルトニウムガリウム合金ナトリウムカリウム合金ミッシュメタルリチウムTerfenol-DPseudo palladiumScandium hydrideサマリウムコバルト磁石Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterling四分一 (合金)スターリングシルバーTibetan silverTitanium Beta Cチタン合金Titanium hydrideGum metalTitanium gold窒化チタンバビットメタルBritannia metalピューターQueen's metalWhite metal水素化ウラン(III)ZamakZirconium hydride水素ヘリウムホウ素窒素酸素フッ素メタン中二階原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification