Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
高マンガン鋼(こうまんがんこう)とは、炭素鋼にマンガンを12%前後加えた組成を持つ合金鋼である。発明者のロバート・ハッドフィールド(en:Robert Hadfield)に因み、ハッドフィールド鋼とも呼ぶ。[1]。
炭素鋼は、常温でフェライト(体心立方格子)相が、高温でオーステナイト(面心立方格子)相が安定している。これに対しオーステナイト形成元素のマンガンを添加し、常温でオーステナイト相を安定にしたのが高マンガン鋼である[2]。鋼の焼入れはフェライト・オーステナイト相間の変態を利用するが、高マンガン鋼はオーステナイト相から変態しないため、焼入れしても効果はない[2]。
高マンガン鋼はオーステナイト組織を持つため、じん性が高く磁性を持たない[2]。また加工硬化性が大きく、荷重を受けるほどに表面が硬くなり、耐摩耗性も向上する[2]。このため靱性と耐摩耗性が求められる用途に向く。
加工硬化が著しいという特徴のため切削性が悪いので、高マンガン鋼は主に鋳造品に利用される[3]。鋳造直後は結晶粒界に炭化物が析出して脆い状態にあるので、炭化物を解消し、製品にじん性を持たせるには1000℃まで加熱し急冷する処理を行う[2]。これは液体化処理や水靱処理と呼ばれている[2]。加熱後急冷する点は焼入れに似ているが、目的も原理も異なる処理である。
ほかに比較的少量(1~数%)のマンガンを添加したマンガン鋼(低マンガン鋼)があるが、これは強靭化や焼入れ性の向上を狙ったものであり、オーステナイト相を利用する高マンガン鋼とは性質が異なる[4]。
This article uses material from the Wikipedia article "高マンガン鋼", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification