powered by CADENAS

Social Share

AlGa (9940 views - Material Database)

AlGa is a degenerate alloy that results from liquid gallium infiltrating the crystal structure of aluminium metal. The resulting alloy is very weak and brittle, being broken under the most minute pressure. The alloy is also chemically weaker, as the gallium inhibits the aluminium from forming a protective oxide layer.
Go to Article

AlGa

AlGa

AlGa is a degenerate alloy that results from liquid gallium infiltrating the crystal structure of aluminium metal. The resulting alloy is very weak and brittle, being broken under the most minute pressure. The alloy is also chemically weaker, as the gallium inhibits the aluminium from forming a protective oxide layer.

Uses

The alloy can be reacted with water to form hydrogen gas, aluminium oxide and gallium metal. This however is not practical for generating hydrogen as electrolysis is a far cheaper and more efficient method.

Safety concerns

Due to AlGa extreme lack of structural integrity and ability to form a protective oxide layer, Gallium metal is considered to be corrosive. If AlGa were to form on an aluminum structure, the aforementioned structure could weaken or collapse. Gallium is illegal to transport on aircraft as it could compromise the integrity of the aluminium hull.


アルニコ磁石アルミニウムアルミニウム合金アルミニウム青銅Aluminium-lithium alloyArsenical bronzeArsenical copperBell metalベリリウムベリリウム銅ビロンBirmabrightBismanolビスマス黄銅青銅Calamine brassChinese silverクロムChromium hydrideコバルトコンスタンタン水素化銅Copper–tungstenCorinthian bronzeクニフェ白銅Cymbal alloysデバルダ合金ジュラルミンDutch metalエレクトロン貨Florentine bronzeガリウムGilding metalガラスGlucydurGuanín (bronze)砲金HepatizonHiduminiumHydronaliumインジウムItalmaMagnaliumマグネシウムマンガニンMegalliumMelchior (alloy)マーキュリーMolybdochalkosMuntz metalニクロムニッケル洋白ノルディック・ゴールドOrmoluリン青銅Pinchbeck (alloy)合成樹脂PlexiglasプルトニウムカリウムロジウムRose's metalサマリウムスカンジウム赤銅 (合金)ナトリウムスペキュラム合金ステンレス鋼ステライト鉄骨構造スズチタントムバックTumbagaウランVitalliumウッドメタルY alloy亜鉛ジルコニウムGalfenolガリンスタンホワイトゴールドRhoditeCrown goldエリンバーField's metalFernicoフェロアロイフェロセリウムフェロクロムフェロマンガンフェロモリブデンFerrosiliconFerrotitaniumFerrouraniumインバー鋳鉄Iron–hydrogen alloy銑鉄Kanthal (alloy)コバールStaballoyスピーゲルBulat steelCrucible steelクロムモリブデン鋼ダマスカス鋼高マンガン鋼高速度鋼Mushet steelマルエージング鋼高張力鋼Reynolds 531ケイ素鋼ばね鋼AL-6XNCelestriumAlloy 20Marine grade stainlessMartensitic stainless steelSanicro 28Surgical stainless steelZeron 100Silver steel工具鋼耐候性鋼Wootz steelはんだTerne活字合金Elektron (alloy)アマルガムマグノックスAlumelBrightrayChromelHaynes InternationalインコネルモネルNicrosilNisilNickel titaniumMu-metalパーマロイSupermalloyNickel hydrideプルトニウムガリウム合金ナトリウムカリウム合金ミッシュメタルリチウムTerfenol-DPseudo palladiumScandium hydrideサマリウムコバルト磁石Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterling四分一 (合金)スターリングシルバーTibetan silverTitanium Beta Cチタン合金Titanium hydrideGum metalTitanium gold窒化チタンバビットメタルBritannia metalピューターQueen's metalWhite metal水素化ウラン(III)ZamakZirconium hydride水素ヘリウムホウ素窒素酸素フッ素メタン中二階原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification