powered by CADENAS

Social Share

Vitallium (15959 views - Material Database)

Vitallium is a trademark for an alloy of 65% cobalt, 30% chromium, 5% molybdenum, and other substances. The alloy is used in dentistry and artificial joints, because of its resistance to corrosion. It is also used for components of turbochargers because of its thermal resistance. Vitallium was developed by Albert W. Merrick for the Austenal Laboratories in 1932. In 2016 Norman Sharp, a 91 year old British man, was recognised as having the world's oldest hip replacement implants. The two vitallium implants were implanted in November 1948 at the Royal National Orthopaedic Hospital, under the newly formed NHS. The 67 year old implants had such an unusually long life, partly because they had not required the typical replacement of such implants, but also because of Mr Sharp's young age of 23 when they were implanted, owing to a childhood case of septic arthritis. For high-temperature use in engines, particularly turbochargers, the first alloy used was Haynes Stellite Nº 21, similar to Vitallium. This was suggested by the British engineer, and denture wearer, Sam Heron during WWII. Although the characteristics of the material obviously suggested itself for making turbocharger blades, it was thought impossible to cast it to the precision needed. Heron demonstrated that it could be, by showing his Vitallium dentures.
Go to Article

Vitallium

Vitallium

Vitallium is a trademark for an alloy of 65% cobalt, 30% chromium, 5% molybdenum, and other substances. The alloy is used in dentistry and artificial joints, because of its resistance to corrosion. It is also used for components of turbochargers because of its thermal resistance. Vitallium was developed by Albert W. Merrick for the Austenal Laboratories in 1932.

In 2016 Norman Sharp, a 91 year old British man, was recognised as having the world's oldest hip replacement implants. The two vitallium implants were implanted in November 1948 at the Royal National Orthopaedic Hospital, under the newly formed NHS. The 67 year old implants had such an unusually long life, partly because they had not required the typical replacement of such implants, but also because of Mr Sharp's young age of 23 when they were implanted, owing to a childhood case of septic arthritis.[1]

For high-temperature use in engines, particularly turbochargers, the first alloy used was Haynes Stellite Nº 21, similar to Vitallium. This was suggested by the British engineer, and denture wearer, Sam Heron during WWII. Although the characteristics of the material obviously suggested itself for making turbocharger blades, it was thought impossible to cast it to the precision needed. Heron demonstrated that it could be, by showing his Vitallium dentures.[2]

  1. ^ "Former RNOH patient has world's oldest hip replacements". Royal National Orthopaedic Hospital. 21 March 2016. 
  2. ^ Setright, L.J.K. "Supercharging". Power To Fly. George Allen & Unwin. p. 195. ISBN 0-04-338041-7. 
  • Wojnar, L (2001). "Porosity structure and mechanical properties of vitalium-type alloy for implants". Materials Characterization. 46 (2–3): 221–225. doi:10.1016/S1044-5803(01)00127-9. 
  • Kaminski, M; Baszkiewicz, J; Kozubowski, J; Bednarska, A; Barcz, A; Gawlik, G; Jagielski, J (1997). "Effect of silicon ion implantation on the properties of a cast Co–Cr–Mo alloy". Journal of Materials Science. 32 (14): 3727–3732. doi:10.1023/A:1018607219482. 

アルニコ磁石アルミニウムアルミニウム合金Aluminium-lithium alloyArsenical copperベリリウムBirmabrightBismanolビスマスクロムChromium hydrideコバルトジュラルミンガリウムガラスHiduminiumHydronaliumインジウムItalmaMagnaliumマグネシウムMegalliumマーキュリーニクロムニッケル合成樹脂PlexiglasプルトニウムカリウムロジウムRose's metalサマリウムスカンジウムナトリウムステンレス鋼ステライト鉄骨構造スズチタンウランウッドメタルY alloy亜鉛ジルコニウムベリリウム銅ビロン黄銅Calamine brassChinese silverDutch metalGilding metalMuntz metalPinchbeck (alloy)トムバック青銅アルミニウム青銅Arsenical bronzeBell metalFlorentine bronzeGlucydurGuanín (bronze)砲金リン青銅Ormoluスペキュラム合金コンスタンタン水素化銅Copper–tungstenCorinthian bronzeクニフェ白銅Cymbal alloysデバルダ合金エレクトロン貨HepatizonマンガニンMelchior (alloy)洋白Molybdochalkosノルディック・ゴールド赤銅 (合金)TumbagaAlGaGalfenolガリンスタンホワイトゴールドRhoditeCrown goldエリンバーField's metalFernicoフェロアロイフェロセリウムフェロクロムフェロマンガンフェロモリブデンFerrosiliconFerrotitaniumFerrouraniumインバー鋳鉄Iron–hydrogen alloy銑鉄Kanthal (alloy)コバールStaballoyBulat steelCrucible steelクロムモリブデン鋼ダマスカス鋼高マンガン鋼高速度鋼Mushet steelマルエージング鋼高張力鋼Reynolds 531ケイ素鋼ばね鋼AL-6XNCelestriumAlloy 20Marine grade stainlessMartensitic stainless steelSanicro 28Surgical stainless steelZeron 100Silver steel工具鋼耐候性鋼Wootz steelはんだTerne活字合金Elektron (alloy)アマルガムマグノックスAlumelBrightrayChromelHaynes InternationalインコネルモネルNicrosilNisilNickel titaniumMu-metalパーマロイSupermalloyNickel hydrideプルトニウムガリウム合金ナトリウムカリウム合金ミッシュメタルリチウムTerfenol-DPseudo palladiumScandium hydrideサマリウムコバルト磁石Argentium sterling silverBritannia silverDoré bullionGoloidPlatinum sterling四分一 (合金)スターリングシルバーTibetan silverTitanium Beta Cチタン合金Titanium hydrideGum metalTitanium gold窒化チタンバビットメタルBritannia metalピューターQueen's metalWhite metal水素化ウラン(III)ZamakZirconium hydride水素ヘリウムホウ素窒素酸素フッ素メタン中二階原子

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Material Database

database,rohs,reach,compliancy,directory,listing,information,substance,material,restrictions,data sheet,specification