powered by CADENAS

Social Share

Champagne glass (13997 views - Basics)

A Champagne glass is a form of stemware designed specifically to enhance the pleasure of drinking champagne. The two most common forms are the flute and coupe. In each the stem allows the drinker to hold the glass without affecting the temperature of the drink, making them readily adaptable to consuming other sparkling wines and certain beers.
Go to Article

Explanation by Hotspot Model

Champagne glass

Champagne glass

Champagne glass

Licensed under Creative Commons Attribution 2.0 (Taken on September 22, 2005).

A Champagne glass is a form of stemware designed specifically to enhance the pleasure of drinking champagne. The two most common forms are the flute and coupe. In each the stem allows the drinker to hold the glass without affecting the temperature of the drink,[1] making them readily adaptable to consuming other sparkling wines and certain beers.

Flute

The champagne flute (French: flûte à Champagne) is a stem glass with either a tall tapered conical shape or elongated slender bowl, generally holding about 6 to 10 US fl oz (180 to 300 ml) of liquid.[2]

The champagne flute was developed along with other wine stemware in the early 1700s as the preferred shape for sparkling wine as materials for drinking vessels shifted from metal and ceramic to glassware.[3] Initially, the flute was tall, conical, and slender; [4] by the 20th century preferences changed from a straight-sided glass to one which curved inward slightly near the lip.[5]

This inward taper is designed to retain champagne's signature carbonation by reducing the surface area for it to escape.[6] Nucleation in a champagne glass helps form the wine's bubbles; too much surface area allows carbonation to fizzle out quickly. More bubbles create greater texture in the taster's mouth, and a flute's deep bowl allows for greater visual effect of bubbles rising to the top.[6] The flute's narrow cross-section also minimizes the oxygen-to-wine ratio, which enhances both the wine's aroma and taste.[3][a]

While most commonly used for sparkling wines, flutes are also used for certain beers, especially fruit beers and Belgian lambics and gueuzes.[8][9] The flute shows off the beer's color, and helps gather the aroma for the nose.[9] The champagne flute is distinguished from the pilsner glass, which lacks a stem.[10]

Coupe

The champagne coupe is a shallow, broad-bowled, saucer shaped stemmed glass generally capable of containing 4 to 8 US fl oz (120 to 240 ml) of liquid.[2] Legend has it the shape of the coupe was modelled on the breast of French queen Marie Antoinette, but the glass was designed in England over a century earlier especially for sparkling wine and champagne in 1663.[11][12][13] The coupe was fashionable in France from its introduction in the 1700s until the 1970s,[14] and in the United States from the 1930s[15] to the 1980s.[12]

Tulip

Champagne is also served in a tulip glass. The white wine tulip is distinguishable from the champagne flute by its wider flared body and mouth.[16] Some oenophiles prefer the tulip glass, as it permits the drinker to get more of the aroma than a traditional flute while the mouth is still narrow enough to avoid quick loss of carbonation.[7][17] The glass maker Riedel particularly criticizes flutes as one-dimensional, impairing drinkers’ ability to appreciate a wine's full range of aromas and taste profiles.[18]

Double-wall stemware

In the 1960s, double-wall stemware was developed to slow the transfer of heat from a drinker's hand to champagne and other beverages.[19] Inner and outer walls are separated by a small gap filled with air, a poor thermal conductor.

Notes
  1. ^ Sources disagree as to whether the narrow mouth of the flute created to capture a wine's aroma allows sufficient access to appreciate it. Wine writer Victoria Moore argues that the "Flutes are no good for champagne because they are too narrow to allow the odour molecules to gather in a place you can get your nose into."[7]
Citations
  1. ^ Cech & Schact 2005, p. 32.
  2. ^ a b Giblin 2011, p. 15.
  3. ^ a b Sezgin 2010, pp. 72-74.
  4. ^ Bray 2001, p. 120.
  5. ^ Walden 2001, p. 9.
  6. ^ a b Andrews 2014, pp. 138, 140.
  7. ^ a b Moore, Victoria (21 October 2014). "Why settle for a flute when you can savour the whole symphony?". The Daily Telegraph. Retrieved 31 December 2015. 
  8. ^ Jackson 1908, p. 114.
  9. ^ a b Villa 2012, p. 373.
  10. ^ Kohn 2013, p. 175.
  11. ^ Lamprey 2010, p. 35.
  12. ^ a b Boehmer 2009, p. 55.
  13. ^ Ray 1967, p. 59.
  14. ^ Liger-Belair 2004, p. 31.
  15. ^ Andrews 2014, p. 138.
  16. ^ Robards 1984, pp. 55-56.
  17. ^ Krebiehl, Anne (January 5, 2016). "Farewell to Champagne flutes in 2016?". Decanter.com. Retrieved November 20, 2016 ; "The Trouble with Champagne Flutes". Milk Street. Fall 2016. p. 29. 
  18. ^ Mercer, Chris (November 28, 2013). "My goal is to make Champagne flutes 'obsolete', says Maximilian Riedel". Decanter.com. Retrieved November 20, 2016. 
  19. ^ "Beverage Glasses". The Hardware Retailer. February 11, 1968. p. 183. 

Bibliography



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Basics

3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted