powered by CADENAS

Social Share

T-nut (15721 views - Mechanical Engineering)

A T-nut, T nut, or tee nut (also known as a blind nut, which can however also refer to a rivet nut or an insert nut) is a type of nut used to fasten a wood, particle or composite materials workpiece, leaving a flush surface. It has a long, thin body and a flange at one end, resembling a T in profile. The flanges of T-nuts often have hooks or serrations on the prongs that dig into a wooden work piece as the bolt is tightened from the opposite side of the piece, providing better retention. In 1969, the first four-prong T-nut with the eight-sided base was patented. Unlike the standard round base T-nuts, the eight-sided T-nuts can be fed efficiently and reliably via machine. The eight-sided T-nut base has become the standard configuration for T-nuts inserted by machine.
Go to Article

T-nut

T-nut

A T-nut, T nut, or tee nut (also known as a blind nut,[1] which can however also refer to a rivet nut or an insert nut) is a type of nut used to fasten a wood, particle or composite materials workpiece, leaving a flush surface.

It has a long, thin body and a flange at one end, resembling a T in profile. The flanges of T-nuts often have hooks or serrations on the prongs that dig into a wooden work piece as the bolt is tightened from the opposite side of the piece, providing better retention.

In 1969, the first four-prong T-nut with the eight-sided base was patented. Unlike the standard round base T-nuts, the eight-sided T-nuts can be fed efficiently and reliably via machine. The eight-sided T-nut base has become the standard configuration for T-nuts inserted by machine.[2][3][4]

See also

  • T-slot nuts, which are used in work-holding in machine tools. T-slot nuts fit in T-section slots in the machine work-table and are used in conjunction with studs and clamps to provide flexible means of holding workpieces in place.
  • Weld nuts, which are similar in appearance to t-nuts. They lack the prongs which penetrate into wood. Weld nuts are usually spot-welded into place on metal.


This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Example Part

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD