powered by CADENAS

Social Share

Amazon

Instant film (7321 views - Consumer products)

Instant film is a type of photographic film introduced by Polaroid to be used in an instant camera (and, with accessory hardware, many other professional film cameras). The film contains the chemicals needed for developing and fixing the photograph, and the instant camera exposes and initiates the developing process after a photo has been taken. In earlier Polaroid instant cameras the film is pulled through rollers which breaks open a pod containing a reagent that is spread between the exposed negative and receiving positive sheet. This film sandwich develops for some time after which the positive sheet is peeled away from the negative to reveal the developed photo. In 1972, Polaroid introduced integral film, which incorporated timing and receiving layers to automatically develop and fix the photo without any intervention from the photographer. Instant film is available in sizes from 24 mm × 36 mm (0.94 in × 1.42 in) (similar to 135 film) up to 50.8 cm × 61 cm (20 in × 24 in) size, with the most popular film sizes for consumer snapshots being approximately 83 mm × 108 mm (3.3 in × 4.3 in) (the image itself is smaller as it is surrounded by a border). Early instant film was distributed on rolls, but later and current films are supplied in packs of 8 or 10 sheets, and single sheet films for use in large format cameras with a compatible back. Though the quality of integral instant film is not as high as conventional film, peel apart black and white film, and to a lesser extent color film approached the quality of traditional film types. Instant film was used where it was undesirable to have to wait for a roll of conventional film to be finished and processed, e.g., documenting evidence in law enforcement, in health care and scientific applications, and producing photographs for passports and other identity documents, or simply for snapshots to be seen immediately. Some photographers use instant film for test shots, to see how a subject or setup looks before using conventional film for the final exposure. Instant film is also used by artists to achieve effects that are impossible to accomplish with traditional photography, by manipulating the emulsion during the developing process, or separating the image emulsion from the film base. Instant film has been supplanted for most purposes by digital photography, which allows the result to be viewed immediately on a display screen or printed with dye sublimation, inkjet, or laser home or professional printers. Instant film is notable for having had a wider range of film speeds available than other negative films of the same era, having been produced in ISO 4 to ISO 20,000. Current instant film formats typically have an ISO between 100 and 1000.Two companies manufacture instant film: Fujifilm (Instax integral film for its Instax cameras), and Polaroid Originals (previously named The Impossible Project) for older Polaroid cameras (600, SX-70, Spectra and 8×10) and its I-Type cameras.
Go to Article

Explanation by Hotspot Model

Youtube


    

Instant film

Instant film

Instant film is a type of photographic film introduced by Polaroid to be used in an instant camera (and, with accessory hardware, many other professional film cameras). The film contains the chemicals needed for developing and fixing the photograph, and the instant camera exposes and initiates the developing process after a photo has been taken.

In earlier Polaroid instant cameras the film is pulled through rollers which breaks open a pod containing a reagent that is spread between the exposed negative and receiving positive sheet. This film sandwich develops for some time after which the positive sheet is peeled away from the negative to reveal the developed photo. In 1972, Polaroid introduced integral film, which incorporated timing and receiving layers to automatically develop and fix the photo without any intervention from the photographer.

Instant film is available in sizes from 24 mm × 36 mm (0.94 in × 1.42 in) (similar to 135 film) up to 50.8 cm × 61 cm (20 in × 24 in) size, with the most popular film sizes for consumer snapshots being approximately 83 mm × 108 mm (3.3 in × 4.3 in) (the image itself is smaller as it is surrounded by a border). Early instant film was distributed on rolls, but later and current films are supplied in packs of 8 or 10 sheets, and single sheet films for use in large format cameras with a compatible back.

Though the quality of integral instant film is not as high as conventional film, peel apart black and white film, and to a lesser extent color film approached the quality of traditional film types. Instant film was used where it was undesirable to have to wait for a roll of conventional film to be finished and processed, e.g., documenting evidence in law enforcement, in health care and scientific applications, and producing photographs for passports and other identity documents, or simply for snapshots to be seen immediately. Some photographers use instant film for test shots, to see how a subject or setup looks before using conventional film for the final exposure. Instant film is also used by artists to achieve effects that are impossible to accomplish with traditional photography, by manipulating the emulsion during the developing process, or separating the image emulsion from the film base. Instant film has been supplanted for most purposes by digital photography, which allows the result to be viewed immediately on a display screen or printed with dye sublimation, inkjet, or laser home or professional printers.

Instant film is notable for having had a wider range of film speeds available than other negative films of the same era, having been produced in ISO 4 to ISO 20,000.[citation needed] Current instant film formats typically have an ISO between 100 and 1000.[citation needed]

Two companies manufacture instant film: Fujifilm (Instax integral film for its Instax cameras), and Polaroid Originals (previously named The Impossible Project) for older Polaroid cameras (600, SX-70, Spectra and 8×10) and its I-Type cameras.

How it works

Instant positive film (which produced a print) uses diffusion transfer to move the dyes from the negative to the positive via a reagent. The process varies according to the film type.

Roll/pack film

In 1947 Edwin H. Land introduced the Polaroid-Land process.[1] The first instant films produced sepia tone photos.[2] A negative sheet is exposed inside the camera, then lined up with a positive sheet and squeezed through a set of rollers which spread a reagent between the two layers, creating a developing film "sandwich". The negative develops quickly, after which some of the unexposed silver halide grains (and the latent image it contains) are solubilized by the reagent and transferred by diffusion from the negative to the positive. After a minute, depending on film type and ambient temperature, the negative is peeled away to reveal the picture which was transferred to the positive receiving sheet.[3] True black and white films were released in 1950 after problems with chemistry stabilization were overcome.[2]

Subtractive color films

Color film is much more complex due to multiple layers of emulsion and dye. The negative consists of three emulsion layers sensitive to the primary colors (red, green, and blue) each with a layer of developing dye beneath it of the complementary color (cyan, magenta, and yellow). Once light exposed the negative, the reagent is spread between the negative and positive and the developing dye layer migrates to the positive surface where it forms the photo. Emulsion layers exposed to their respective color block the complementary dye below it, reproducing the original color. For example, a photo of a blue sky would expose the blue emulsion, blocking all the yellow dye beneath it and allowing the magenta and cyan dye layers to migrate to the positive to form blue.[3]

Integral film

This process is similar to subtractive color instant film with added timing and receiving layers. Land's solution was to incorporate an opacifier, which would darken when ejected from the camera, and then become clear to reveal the photograph.[2] The film itself integrates all the layers to expose, develop, and fix the photo into a plastic envelope and frame commonly associated with a Polaroid photo.

Additive color film

Additive film (such as Polavision and Polachrome slide film) uses a color mask of microscopically thin transparent red, green, and blue lines (3000 lines per inch) and a black and white emulsion layer to reproduce color images in transparency film. The resulting dye developers (unexposed emulsion) block the colors not needed and project the color or combination of colors which form in the resulting image. Since the lines are so close to each other, the human eye easily blended the primary colors together to form the correct color, much like an LCD display or television. For instance, a photo of a yellow flower would expose the emulsion beneath the red and green masks and not the blue mask. The developing process removed the exposed emulsion (under the red and green masks) and diffused the unexposed dye developer (under the blue mask) to its receiving layer, blocking light from coming through. This resulted in the projected light shining through the red and green masks but not the blue mask, creating the color yellow. Because of the film density, film speeds were necessarily slow. High precision was required for the production of this film.

Film brands

Polaroid

Polaroid Corporation invented and produced the widest range of instant film. Roll film was distributed in two separate negative and positive rolls and developed inside the camera. It was introduced in 1948 and was manufactured until 1992. Sheet film was introduced in 1958 for 4x5" film holder #500. Each sheet contains a reagent pod, negative and receiving positive, and was loaded separately and developed outside the film holder. In 1973 Polaroid introduced 8x10" Instant film. Pack film was distributed in a film pack which contained both negative and positive sheets and was developed outside the camera. It was introduced in 1963. Integral film is also distributed in a film pack, but each film envelope contains all the chemical layers to expose, develop, and fix the photo. It was introduced in 1972.

Polavision was an instant motion picture film. Polavision was introduced by Polaroid in 1978, with an image format similar to Super 8 mm film, and based on an additive color process. Polavision required a specific camera and tabletop viewer, and was not a commercial success, but did lead to the development of an instant 35 mm color slide film. Polavision film has been taken off the market. Polachrome was an easy to develop 35 mm film, available in color, monochrome and 'blue' formats (the latter intended for making title cards). Each roll of film came with a cartridge containing developing chemicals which were pressed between the film and a developing strip by a hand-cranked machine called the AutoProcessor. The AutoProcessor was very cheap and did not require a darkroom; the results were somewhat variable, the resolution was not as good as conventional film due to the matrix of tiny red, green and blue filters required to make the monochrome emulsion work in color, and the sensitivity was low, even for slide film; in tungsten light, Polachrome CS is rated at ISO 40. It was introduced in 1983.

Polaroid integral film packs usually contain a flat "Polapulse" electrical battery, which powers systems in the camera, including exposure and focusing mechanisms, electronic flash, and a film ejection motor. The inclusion of the battery within the film pack ensures that a fresh battery is available with each new pack of film.

Polaroid no longer produces instant film. It has become an organization which licenses its brand name to other manufacturers. An example of this is the Polaroid 300 camera, which is a Polaroid branded Fuji Instax. Polaroid PIF-300 film is essentially rebranded Fuji Instax mini film.

Preservation

Polaroids have the same storage standards under ISO 18920:2000 as any other photograph.[4] Regular storage conditions should be less than 70 degrees Fahrenheit and between 50% and 30% relative humidity (RH). Cold storage (0 degrees Fahrenheit optimum) is not helpful unless RH can be controlled and cold storage RH is generally drier than required. RH below 30% will create an environment that is too dry and may cause the photograph to curl. A Polaroid transfer removes the emulsion from the plastic backing and residual chemicals, offering an alternate form of preservation.

End of production

In February 2008, Polaroid (by then under the control of Thomas J. Petters of Petters Group Worldwide) announced it would cease production of all instant film; the company shut down three factories and laid off 450 workers.[5] Sales of chemical film by all makers have dropped by at least 25% per year since 2000,[citation needed] but a new birth of interest around Fujifilm and, in particular, The Impossible Project films fulfilled demand in the market.

Integral film

  • SX-70 cameras (integral film, develops automatically, 3.1 × 3.1 inch)
  • 600 cameras (integral film, develops automatically, 3.1 × 3.1 inch)
  • Spectra / Image / 1200 cameras (integral film, develops automatically, 3.6 × 2.9 inch)
  • Captiva/Vision (integral film, for Captiva and Joycam, 4.4 × 2.5 inch, 11.1 × 6.4 cm)
  • i-Zone (integral film, for i-Zone, Tomy Xiao, 1.5 × 1 inch, 3.6 cm × 2.4 cm)
  • i-Zone200 (integral film, for i-Zone200 only, 1.5 × 1 inch, 3.6 cm × 2.4 cm)
  • Type 330 series AutoFilm (integral film for use Polaroid CB-33 backs, 3¼ × 4¼ inch).[citation needed]

Packfilm

  • Type 100 series packfilm for Land cameras (timed peel-apart development, sometimes called type 660, 10.8 × 8.3 cm; 4.25 × 3.25 inch)
  • Type 550 series packfilm, 4 × 5 inch, for Polaroid 550 film backs. Introduced in 1981.
  • Type 80 series packfilm, 8.3 × 8.6 cm, (3¼ × 3⅜ inch). Introduced in 1971; re-introduced in 2003.[citation needed]

Rollfilm

  • Type 20 series roll film, for "The Swinger" (2½" × 3¼"). Introduced 1965, discontinued 1979.
  • Type 30 series roll film, for "Highlander" (80, 80A, 80B) and J33 Electric Eye (2½" × 3¼"). Introduced 1954, discontinued 1979.
  • Type 40 series roll film (3¼" × 4¼") 8 exposures per roll (for monochrome types, 6 exposures for type 48 Polacolor), for most Polaroid cameras made before 1963. Introduced 1948, discontinued 1976 (Polacolor) and 1992 (monochrome).

Sheet film

  • Type 50 series sheetfilm for 4 × 5 inch large format (time peel-apart development, all professional grade)
  • Type 800 series sheetfilm for 8 × 10 inch cameras, processors, Daylabs and other purposes.[citation needed]

PolaChrome

PolaBlue, PolaChrome CS, PolaChrome HCP, PolaGraph HC, and PolaPan CT were 35 mm instant slide films.[citation needed]

20x24

20x24 P3 PolaColor, 20x24 P7 PolaColor, and 20x24 PolaPan.[citation needed]

40x80

  • 40x80 PolaColor ER, ISO 80, color

Misc film

  • Polaroid IJT-100 transparency film, Type 1001 radiography film, and Type 3000X radiography film.[citation needed]

Kodak

Kodak manufactured the negative component of Polaroid's instant film from 1963 to 1969, when Polaroid decided to manufacture its own. Kodak's original plan was to create packfilm type instant products. There were many prototypes and test runs of the film with many private demonstrations to their board. Plans changed when Polaroid in 1972 released the integral type film with the introduction of the SX-70 system. Kodak decided to scrap the plans for packfilm release and focus on an integral type process. A few years later Kodak introduced its own instant film products in 1976, which was different from Polaroid's in several ways:[6]

Kodak instant film was exposed from the back without a mirror, the opposite of Polaroid's film which was exposed from the front with a mirror to reverse the image. Kodak used a matte finish on the front, made possible by exposing the film through the back. The negative and empty pod could be removed by peeling it off of the back of the print. Unlike Polaroid's integral film packs, Kodak's did not contain a battery, and used conventional batteries. Kodak’s PR 10 film was found to have light fading stability issues.[7]

Polaroid filed suit against Eastman Kodak in April 1976 for the infringement of ten patents held by Edwin Land and others on his development team relating to instant photography. In September 1985, the United States District Court of Massachusetts ruled that seven patents were valid and infringed, two were invalid but infringed, and one was valid but not infringed by Kodak. Kodak appealed but was denied and an injunction prohibiting production of their instant film and cameras was put into effect. Kodak's appeal to the Supreme Court was denied a few months later, and in January 1986, Kodak announced it would no longer be producing their instant line of products. In 1991, Polaroid was awarded $925 million in damages from Kodak.[8]

Alternative Kodak instant film

While Kodak instant films have been discontinued, Fuji's instant film available in Japan since the 1980s is very similar to Kodak's. The pictures are the same size, the cartridge is almost the same, with some easy plastic modifications; the Fuji Fotorama series film can be made to fit. It was closest to the Kodak with the ISO at 160, many of the camera's brightness controls can be adjusted to work with the different ISO; However, the FI-10 series was discontinued in the 1990s. The faster ISO 800 instant films will work as well but would require the use of a filter either on the film cartridge or lens.

Fujifilm

Fujifilm equivalents of Polaroid films

In Japan, Fujifilm introduced their own line of instant photographic products in 1981 starting with the Fotorama line of cameras. The name Fotorama came from photograph and panorama, as the film was a wide format compared to the square Polaroid SX-70/600 films. These Integral films developed similar to Kodak's with the back layer first. This presented a major problem for Fujifilm because of the ongoing litigation between Kodak and Polaroid. Polaroid also has a separate suit with Fujifilm and their instant film patents in Japan. When Kodak lost, Fujifilm was able to work with Polaroid to allow their cameras and films to remain in the market,[9] provided that they have a technology sharing agreement. Polaroid was interested in branching out to magnetic media in the boom of the videotape era and had acquired a company called MagMedia Ltd. Fujifilm has a long history in magnetic media dating to the mid-1950s. This led to Polaroid having access to Fujifilm's extensive electronic, video tape and floppy disc magnetic products. This allowed Fujifilm access to Polaroid's film technology.

By the mid-1980s Fujifilm introduced the higher ISO System 800 series, followed by the ACE series in the mid-1990s. Instant ACE is nearly identical to System 800, the only difference is the design of the plastic cartridge in the ACE do not contain the spring mechanism (the spring is in the camera). Most of these products were available only in the Japanese market, until the release of Instax series of cameras was released in 1998. Fujifilm originally wanted to release the Instax series worldwide including North America and Europe simultaneously,[10] but decided to work with Polaroid on the mio camera based on the Instax mini 10 for the US market; while Canada did get the Instax Wide 100. Another product was Fujifilm's Digital Instax Pivi film for their battery powered portable printer which was made available for those who wanted to print from their mobile phone via infrared, USB and Bluetooth.

Fujifilm makes pack film for their passport camera systems, and had been available outside Japan since the mid-1980s. No legal issues arose with Fuji's peel apart instant films as Polaroid's patents had expired. While very popular in Australia as a cheaper alternative to Polaroid,[citation needed] it was generally not too well known elsewhere due to Polaroid's dominance in most countries. In 2000, Fuji decided to change the way they manufacture pack film, making the entire pack out of plastic instead of a metal and plastic combination. Fujifilm announced at PMA 2003[vague] that pack film would be made available to the North American market.

With the discontinuation of Polaroid instant film in 2008, Fuji started to export more of their instant film products to overseas markets, starting with making an increased variety of pack films available. In November 2008 the Instax Wide format was available in the US with the Instax 200 camera.[11] Instax mini series of cameras and films became available in the US during the second half of 2009, with the mini 7s,[12] also an updated Instax 210 replaced the Instax 200. Fujifilm's FP-100b45 was announced in Sept of 2009 for the US market.[13] The FP-3000b45 arrived in the North American market in Jan 2011, after Fujifilm Japan stopped manufacturing FP-100b, but was discontinued in 2012.[14] In late 2012 Fujifilm discontinued FP-3000B,[15] followed by the discontinuation of FP-100C in spring 2016.[16][17] In April 2017 Fujifilm announced the Instax SQUARE 1:1 format and compatible Instax SQ10 camera.[18][19]

Fujifilm instant films include:

Integral film

  • Instax Wide series ISO 800 films
  • Instax Mini series ISO 800 films
  • Instax Square series ISO 800 films
  • ACE series ISO 800 films. Compatible with Fujifilm's Fotorama ACE series of instant cameras. Discontinued June 2010.
  • 800 series ISO 800 films. Compatible with Fujifilm's Fotorama 800 series instant cameras. Discontinued 2010.
  • F Series ISO 160. Compatible with Fotorama F series instant cameras. Discontinued in the mid-1990s.
  • Miscellaneous discontinued films; FI-160 ISO 160 (89x114 mm) for use with MS-45 4x5 instant back.[citation needed]

Packfilm

  • 3 14 in × 4 14 in (83 mm × 108 mm). Compatible with Polaroid Type 100 packfilm (also known as "Type 660"). Discontinued February 2016.[16]
  • 4 in × 5 in (100 mm × 130 mm). For use in the Fujifilm PA-45 holder. Compatible with Polaroid Type 550 series 4x5 packfilm versions of Type 50 sheetfilm. Discontinued 2016.[20])

The Impossible Project / Polaroid Originals

A group called the Impossible Project acquired Polaroid's old equipment and factory in Enschede, in the Netherlands.[21][22] On their website[23] they stated:

We aim to re-start production of analog instant film for vintage Polaroid cameras in 2010.

and

"The Impossible mission is not to re-build Polaroid Integral film but (with the help of strategic partners) to develop a new product with new characteristics, consisting of new optimised components, produced with a streamlined modern setup. An innovative and fresh analog material, sold under a new brand name that perfectly will match the global re-positioning of Integral Films."

On March 22, 2010, it was announced they were successful in manufacturing instant film compatible with Polaroid SX-70/600 instant cameras. Two new products were announced — PX100 and PX600. Their PX100 Silver Shade instant film is a manipulable, monochromatic replacement of old Polaroid brand instant film compatible with SX-70 cameras while the PX600 Silver Shade instant film is compatible with 600 cameras.[citation needed] That formulation has since been supplanted by improved films.

The company, renamed Polaroid Originals in 2017, produces 600, SX-70, Spectra and 8×10 color and monochrome film packs with a variety of colored borders. It also produces I-Type film packs that differ from traditional 600 packs in their omission of the battery (thus lowering costs), for use in its Impossible I-1 camera (released in 2016), its Polaroid OneStep 2 camera (released in September 2017), and its Polaroid OneStep+ (released in September 2018).[24][25][26]

PLR IP Holdings, LLC

Summit Global Group, using the Polaroid brand, produced an instant photography camera and film starting with the Polaroid PIC 300, based on Fujifilm's Instax Mini 7.

  • 300, ISO 800, color (a rebranded Fujifilm Instax Mini 7)

New55 FILM

A company called New55 Holdings, LLC, ("New55 FILM") based in Ashland, Massachusetts, brought to market a black and white 4x5 positive-negative material that is exposed and processed in a Polaroid 545 holder. New55 PN provided a positive print and a 4x5 negative that could be scanned, contact printed, or enlarged. Winding up their proof-of-principle R&D phase, New55 Holdings, LLC, ceased operations in December 2017.[27]

Toxicity

The liquid chemicals for the developing process contained in the more common instant photo sheets are caustic and can cause chemical burns. For such liquid the manufacture recommendation can be to avoid contact with skin and when contact with skin is made wash immediately with much water.[28][29] Some instant films have used less common reagents and have had differing suggested responses.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Consumer products

.max, Maya, Challenge, Competition, Rendering, 3D, Blender, Autodesk Maya, 3D Studio MAX (.3DS, .MAX), Maxwell, Animation, 3D Model, Autodesk Softimage, Cinema 4D, Rendering, Animation, 3Dartist, c4d, maxon, lowpoly, 3Dart, blender3D, 3D library