powered by CADENAS

Social Share

Amazon

Twinjet (10786 views - Transportation - Air Water Earth)

A twinjet or twin-engine jet is a jet aircraft powered by two engines. A twinjet is able to fly well enough to land with a single working engine, making it safer than a single-engine aircraft in the event of failure of an engine. Fuel efficiency of a twinjet is better than that of aircraft with more engines. These considerations have led to the widespread use of aircraft of all types with twin engines, including airliners, fixed-wing military aircraft, and others.
Go to Article

Explanation by Hotspot Model

Youtube


    

Twinjet

Twinjet

A twinjet or twin-engine jet is a jet aircraft powered by two engines. A twinjet is able to fly well enough to land with a single working engine, making it safer than a single-engine aircraft in the event of failure of an engine.[1] Fuel efficiency of a twinjet is better than that of aircraft with more engines.[2] These considerations have led to the widespread use of aircraft of all types with twin engines, including airliners, fixed-wing military aircraft, and others.

Aircraft configurations

As of today, there are three most common configurations of twinjet aircraft. The first, common on large aircraft such as airliners, has a podded engine usually mounted beneath, or occasionally above or within, each wing.

The second has one engine mounted on each side of the rear fuselage, close to its empennage, used by many business jets.

In the third configuration both engines are within the fuselage, side-by-side, used by most fighters since the 1960s. Later fighters using this configuration include the Su-27 'Flanker', the F-15 Eagle, and the F-22 Raptor.

History

The first twinjet to fly was the German fighter prototype Heinkel He 280, flying in April 1941 with a pair of nacelled Heinkel HeS 8 axial-flow turbojets.

The twinjet configuration was used for short-range narrow-bodied aircraft such as the McDonnell Douglas DC-9 and Boeing 737. The Airbus A300 was initially not successful when first produced as a short-range widebody, as airlines operating the A300 on short-haul routes had to reduce frequencies to try and fill the high-capacity aircraft, and lost passengers to airlines operating more frequent narrow-body flights. However, thanks to the introduction of ETOPS rules that allowed twin-engine jets to fly long-distance routes that were previously off-limits to them, Airbus was able to further develop the A300 as a medium- to long-range airliner to increased sales; Boeing launched its widebody twinjet, the Boeing 767, in response.

In the 1980s the Boeing 727 was discontinued, as its central engine bay would require a prohibitively expensive redesign to accommodate quieter high-bypass turbofans, and it was soon supplanted by twinjets for the narrow-body market; Airbus with the A320, and Boeing with the 757 and updated "classic" variants of the 737. During that decade only McDonnell Douglas continued development of the trijet design with an update to the DC-10, the MD-11, which initially had a range advantage over its closest medium wide-body competitors which were twinjets, the in-production Boeing 767 and upcoming Airbus 330. In contrast to McDonnell Douglas sticking with their existing trijet configuration, Airbus (which never produced a trijet aircraft) and Boeing worked on new widebody twinjet designs that would become the Airbus A330 and Boeing 777, respectively. The MD-11's long range advantage was brief as it was soon nullified by the Airbus A330's four-engine derivative, the Airbus A340, and the extended-range Boeing 767-300ER and Boeing 777-200ER.

The Boeing 737 twinjet stands out as the most produced jet airliner. The Boeing 777 is the world's largest twinjet, and the 777-200LR variant is the world's longest range airliner. Other Boeing twinjets include the 767, 757 (out of production but still in commercial service) and 787. Competitor Airbus produces the A320 family, the A330, and the A350.

Some modern commercial airplanes still use four engines (quad-jets) like the Airbus A380 and Boeing 747-8, which are classified as very large aircraft (over 400 seats in mixed-class configurations). Four engines are still used on the largest cargo aircraft capable of transporting outsize cargo, including strategic airlifters. There are plans to revive production of six-engine giants like the Antonov An-225 Mriya.

Efficiency

Twin-jets tend to be more fuel-efficient than trijet (three engine) and quad-jet (four engine) aircraft. As fuel efficiency in airliners is a high priority, many airlines have been increasingly retiring trijet and quad-jet designs in favor of twinjets in the twenty-first century. The trijet designs were phased out first, in particular due to the more complicated design and maintenance issues of the middle engine mounted on the stabilizer. Early twinjets were not permitted by ETOPS restrictions to fly long-haul trans-oceanic routes, as it was thought that they were unsafe in the event of failure of one engine, so quad-jets were used. Quad-jets also had higher carrying capacity than comparable earlier twinjets. However, later twinjets such as the Boeing 777 and Airbus A350 have matched or surpassed older quad-jet designs such as the Boeing 747 and Airbus A340 in these aspects, and twinjets have been more successful in terms of sales than quad-jets.

In 2012, Airbus studied a 470-seat twinjet competitor for the B747-8 with lower operating costs expected between 2023 and 2030, revived After Boeing launched the 777X in November 2013, while then-CEO Fabrice Brégier preferred to focus on product improvement rather than all-new concepts for 10 years. It would have a 10-abreast economy like the 777; its 565 m² (6,081 sq ft) wing, slightly more than the 747-8, would have a 80 m (262 ft) span, as wide as the A380, for a 892,900 lb (405 t) MTOW compared to 775,000 lb (352 t) for the 777X, with a composite structure for an operating empty weight of 467,400 lb (212 t), and a 8,150 nmi (15,090 km) range at Mach 0.85.[3]

ETOPS

When flying far from diversionary airports (so called ETOPS/LROPS flights), the aircraft must be able to reach an alternate on the remaining engine within a specified time in case of one engine failure. When aircraft are certified according to ETOPS standards, thrust is not an issue, as one of the engines is more than powerful enough to keep the aircraft aloft (see below). Mostly, ETOPS certification involves maintenance and design requirements ensuring that a failure of one engine cannot make the other one fail also. The engines and related systems need to be independent and (in essence) independently maintained. ETOPS/LROPS is often incorrectly thought to apply only to long overwater flights, but it applies to any flight more than a specified distances from an available diversion airport. Overwater flights near diversion airports need not be ETOPS/LROPS-compliant.

Introduction to transoceanic flights

Since the 1990s, airlines have increasingly turned from four-engine or three-engine airliners to twin-engine airliners to operate transatlantic and transpacific flight routes. On a nonstop flight from America to Asia or Europe, the long-range aircraft usually follows the great circle route. Hence, in case of an engine failure in a twinjet (like Boeing 777), it is never too far from an emergency landing field in Canada, Alaska, eastern Russia, Greenland, Iceland, or the British Isles. The Boeing 777 has also been approved by the Federal Aviation Administration for flights between North America and Hawaii, which is the world's longest[citation needed] regular airline route with no diversion airports along the way.

Other advantages

On large passenger jets, the cost of the engines makes up a significant proportion of the plane's final cost. Each engine also requires separate service, paperwork, and certificates. Thus, having two larger engines as opposed to three or four smaller engines will significantly reduce both the purchase and maintenance costs of a plane. However, relative costs of two engines is double the cost of one engine.

Regulations governing the required thrust levels for transport aircraft are typically based upon the requirement that an aircraft be able to continue a takeoff if an engine fails after the takeoff decision speed is reached.[4] Thus, with all engines operating, trijets must be able to produce at least 150% of the minimum thrust required to climb and quad-jets 133%. Conversely, since a twinjet will lose half of its total thrust if an engine fails, they are required to produce 200% of the minimum thrust required to climb when both engines are operating. Because of this, twinjets typically have higher thrust-to-weight ratios than aircraft with more engines, and are thus able to accelerate and climb faster.

See also


AirbusAeromobileComandi di volo e sistemi di controllo del voloAirframeAeroplanoBoeing 737Boeing 737 Next GenerationBoeing 787 DreamlinerBoeing B-29 SuperfortressBoeing CH-47 ChinookBoeing Insitu ScanEagleBusiness jetCessna O-2 SkymasterCessna SkymasterCabina di pilotaggioEurocopter EC 725Eurofighter TyphoonAereo da cacciaHawker FuryHawker HurricaneElicotteroRotore (aeronautica)Jet engineMcDonnell Douglas F-4 Phantom IIMcDonnell Douglas MD-80Model aircraftOlga E. CustodioTwin-boom aircraftUnited States Air Force ThunderbirdsSupersonic aircraftAereo a reazioneCacciabombardiereLockheed SR-71Aereo da ricognizionePrimati mondiali di velocità di voloAirspeedRegime transonicoVelocità del suonoMcDonnell XF-85 GoblinNight fighterMcDonnell Douglas F/A-18 Super HornetAereo imbarcatoIAI KfirAereo da attacco al suoloPostbruciatoreMikoyan-Gurevich MiG-27Sukhoi Su-27Air superiority fighterSupermaneuverabilityGloster MeteorNorth American P-51 MustangNorth American P-51 Mustang variantsCompetizione aeronauticaMesserschmitt Bf 109ScoccaCupolino (aeronautica)Dassault Mirage F1Caccia intercettoreMcDonnell Douglas-BAe T-45 GoshawkMcDonnell Douglas-BAe AV-8B Harrier IIDassault Mirage 2000CheroseneAeromobile per la guerra elettronicaTattica militareGeneral Atomics RQ-1 PredatorBoeing AH-64 ApacheArmed helicopterAircraft ordnanceAdvanced Attack HelicopterTurboalberoJet airlinerJet trainerAereo da addestramentoFlight trainingAir combat manoeuvringUnited States Air ForceDecolloMcDonnell Douglas F/A-18 Hornet

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht