Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution 2.0 (Payton Chung from DC, USA).
Steelmaking is the process for producing steel from iron ore and scrap. In steelmaking, impurities such as nitrogen, silicon, phosphorus, sulfur and excess carbon are removed from the raw iron, and alloying elements such as manganese, nickel, chromium and vanadium are added to produce different grades of steel. Limiting dissolved gases such as nitrogen and oxygen, and entrained impurities (termed "inclusions") in the steel is also important to ensure the quality of the products cast from the liquid steel.[1]
Steelmaking has existed for millennia, but it was not commercialized on a massive scale until the 19th century. The ancient craft process of steelmaking was the crucible process. In the 1850s and 1860s, the Bessemer process and the Siemens-Martin process turned steelmaking into a heavy industry. Today there are two major commercial processes for making steel, namely basic oxygen steelmaking, which has liquid pig-iron from the blast furnace and scrap steel as the main feed materials, and electric arc furnace (EAF) steelmaking, which uses scrap steel or direct reduced iron (DRI) as the main feed materials. Oxygen steelmaking is fuelled predominantly by the exothermic nature of the reactions inside the vessel where as in EAF steelmaking, electrical energy is used to melt the solid scrap and/or DRI materials. In recent times, EAF steelmaking technology has evolved closer to oxygen steelmaking as more chemical energy is introduced into the process.[2]
Steelmaking has played a crucial role in the development of ancient, medieval, and modern technological societies. Early processes of steel making were made during the classical era in Ancient Iran, Ancient China, India, and Rome, but the process of ancient steelmaking was lost in the West due to the fall of the Western Roman Empire in the 5th century CE.[3]
Cast iron is a hard brittle material that is difficult to work, whereas steel is malleable, relatively easily formed and a versatile material. For much of human history, steel has only been made in small quantities. Since the invention of the Bessemer process in the 19th century and subsequent technological developments in injection technology and process control, mass production of steel has become an integral part of the global economy and a key indicator of modern technological development.[4] The earliest means of producing steel was in a bloomery.
Early modern methods of producing steel were often labour-intensive and highly skilled arts. See:
An important aspect of the Industrial Revolution was the development of large-scale methods of producing forgeable metal (bar iron or steel). The puddling furnace was initially a means of producing wrought iron, but was later applied to steel production.
The real revolution in modern steelmaking only began at the end of the 1850s when the Bessemer process became the first successful method of steelmaking in quantity, followed by the open-hearth furnace.
Modern steelmaking processes can be divided into two categories: Primary and Secondary steelmaking. Primary steelmaking involves converting liquid iron from a blast furnace and steel scrap into steel via basic oxygen steelmaking, or melting scrap steel or direct reduced iron (DRI) in an electric arc furnace. Secondary steelmaking involves refining of the crude steel before casting and the various operations are normally carried out in ladles. In secondary metallurgy, alloying agents are added, dissolved gases in the steel are lowered, and inclusions are removed or altered chemically to ensure that high-quality steel is produced after casting.[5]
Basic oxygen steelmaking is a method of primary steelmaking in which carbon-rich molten pig iron is made into steel. Blowing oxygen through molten pig iron lowers the carbon content of the alloy and changes it into steel. The process is known as basic due to the chemical nature of the refractories—calcium oxide and magnesium oxide—that line the vessel to withstand the high temperature and corrosive nature of the molten metal and slag in the vessel. The slag chemistry of the process is also controlled to ensure that impurities such as silicon and phosphorus are removed from the metal.
The process was developed in 1948 by Robert Durrer and commercialized in 1952–53 by Austrian VOEST and ÖAMG.[citation needed] The LD converter, named after the Austrian towns of Linz and Donawitz (a district of Leoben) is a refined version of the Bessemer converter where blowing of air is replaced with blowing oxygen. It reduced capital cost of the plants, time of smelting, and increased labor productivity. Between 1920 and 2000, labour requirements in the industry decreased by a factor of 1,000, from more than 3 worker-hours per tonne to just 0.003. The vast majority of steel manufactured in the world is produced using the basic oxygen furnace; in 2011, it accounted for 70% of global steel output. Modern furnaces will take a charge of iron of up to 350 tons and convert it into steel in less than 40 minutes, compared to 10–12 hours in an open hearth furnace.[6]
Electric arc furnace steelmaking is the manufacture of steel from scrap or direct reduced iron melted by electric arcs. In an electric arc furnace, a batch of steel ("heat") may be started by loading scrap or direct reduced iron into the furnace, sometimes with a "hot heel" (molten steel from a previous heat). Gas burners may be used to assist with the melt down of the scrap pile in the furnace. As in basic oxygen steelmaking, fluxes are also added to protect the lining of the vessel and help improve the removal of impurities. Electric arc furnace steelmaking typically uses furnaces of capacity around 100 tonnes that produce steel every 40 to 50 minutes for further processing.[7]
By-product gases from the steel making process can be used to generate electricity through the use of reciprocating gas engines/gas turbines.[8] These green house gases are produced by burning fossil fuels contributing to global warming.[9][10]
Secondary steelmaking is most commonly performed in ladles and often referred to as ladle (metallurgy). Some of the operations performed in ladles include de-oxidation (or "killing"), vacuum degassing, alloy addition, inclusion removal, inclusion chemistry modification, de-sulphurisation and homogenisation. It is now common to perform ladle metallurgical operations in gas stirred ladles with electric arc heating in the lid of the furnace. Tight control of ladle metallurgy is associated with producing high grades of steel in which the tolerances in chemistry and consistency are narrow.[11]
The HIsarna ironmaking process is a process for iron making in which iron ore is processed almost directly into liquid iron or hot metal. The process is based around a new type of blast furnace called a Cyclone Converter Furnace, which makes it possible to skip the process of manufacturing pig iron pellets that is necessary for the basic oxygen steelmaking process. Without the necessity for this preparatory step the HIsarna process is more energy-efficient and has a lower carbon footprint than traditional steelmaking processes.
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
Aveva Tribon, Aveva PDMS, Intergraph Smartplant, Intergraph Smartmarine, Offshore, Onshore, Marine, Shipyard, Plantdesign