powered by CADENAS

Social Share

Electrical energy (15450 views - Electrical Engineering)

Electrical energy is the energy newly derived from electric potential energy or kinetic energy. When loosely used to describe energy absorbed or maybe delivered by an electrical circuit (for example, one provided by an electric power utility) "electrical energy" talks about energy which has been converted from electric potential energy. This energy is supplied by the combination of electric current and electric potential that is delivered by the circuit. At the point that this electric potential energy has been converted to another type of energy, it ceases to be electric potential energy. Thus, all electrical energy is potential energy before it is delivered to the end-use. Once converted from potential energy, electrical energy can always be called another type of energy (heat, light, motion, etc.).
Go to Article

Youtube


    

Electrical energy

Electrical energy

Electrical energy is the energy newly derived from electric potential energy or kinetic energy. When loosely used to describe energy absorbed or maybe delivered by an electrical circuit (for example, one provided by an electric power utility) "electrical energy" talks about energy which has been converted from electric potential energy. This energy is supplied by the combination of electric current and electric potential that is delivered by the circuit. At the point that this electric potential energy has been converted to another type of energy, it ceases to be electric potential energy. Thus, all electrical energy is potential energy before it is delivered to the end-use. Once converted from potential energy, electrical energy can always be called another type of energy (heat, light, motion, etc.).

Electricity generation

Electricity generation is the process of generating electrical energy from other forms of energy.

The fundamental principle of electricity generation was discovered during the 1820s and early 1830s by the British scientist Michael Faraday. His basic method is still used today: electricity is generated by the movement of a loop of wire, or disc of copper between the poles of a magnet.[1]

For electric utilities, it is the first step in the delivery of electricity to consumers. The other processes, electricity transmission, distribution, and electrical power storage and recovery using pumped-storage methods are normally carried out by the electric power industry.[2]

Electricity is most often generated at a power station by electromechanical generators, primarily driven by heat engines fueled by chemical combustion or nuclear fission but also by other means such as the kinetic energy of flowing water and wind. There are many other technologies that can be and are used to generate electricity such as solar photovoltaics and geothermal power.

  1. ^ "Michael Faraday House". The Institution of Engineering & Technology. Retrieved 8 November 2015. 
  2. ^ "Keep the Power On" (PDF). IEC Electrical Energy. Retrieved 8 November 2015. 

Electric boilerGeneratore elettricoElectric lightVeicolo elettricoCavoConnettore elettricoElectricity meterElectronic symbolTurbine bladeImpianto solare termodinamicoEnergia da fusioneEnergie rinnovabiliElettrodoMotore ad accensione comandataRing main unitDistribuzione di energia elettricaIndustrial processesForno a induzioneInduction heatingInduction heaterInduction forgingMomento meccanicoForzaCompact fluorescent lampCircuito elettricoCorrente elettricaCarica elettricaCampo elettromagneticoIngegneria delle telecomunicazioniCircuit designElectronic switching systemTrasmissione (telecomunicazioni)Electrical telegraphTelecommunication circuitBroadcast engineeringPhotovoltaicsImpianto fotovoltaicoSolar powerSolar cell efficiencyEnergy transformationEnergiaFornello a induzioneConduzione termicaCooktopHeating elementEffetto JouleEnergia cineticaWireless routerIonePropulsione elettrica per uso spazialeElectrohydrodynamicsAmplificatore (elettronica)Brushed DC electric motorUniversal motorMacchina elettricaTrasmissione di energia elettricaCentrale elettricaMechanical powerAlimentazione elettricaCarico (elettrotecnica)SostenibilitàSviluppo sostenibileThermoelectric generatorElectric power conversionCorrente alternataConduttore elettricoIsolatoreEnergia potenziale elettricaSuperconduttivitàMotor-generatorGruppo elettrogenoTrasferimento di energia senza filiElectromagnetismOverhead projectorMajor applianceElectric switchboardQuadro elettricoElectrical roomGrowler (electrical device)AmperometroAmpereImpedenza

This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Electrical Engineering

EPLAN, Aucotec, CAE, AutoCAD Electrical, IGE XAO, ElCAD, 2D drawings, 2D symbols, 3D content, 3D catalog, EPLAN Electric P8, Zuken E3, schematics, dataportal, data portal, wscad universe, electronic, ProPanel3D, .EDZ, eClass Advanced, eCl@ss Advanced