powered by CADENAS

Social Share

Wing (5682 views - Transportation - Air Water Earth)

A wing is a type of fin that produces lift, while moving through air or some other fluid. As such, wings have streamlined cross-sections that are subject to aerodynamic forces and act as an airfoils. A wing's aerodynamic efficiency is expressed as its lift-to-drag ratio. The lift a wing generates at a given speed and angle of attack can be one to two orders of magnitude greater than the total drag on the wing. A high lift-to-drag ratio requires a significantly smaller thrust to propel the wings through the air at sufficient lift. Lifting structures used in water, include various foils, including hydrofoils. Hydrodynamics is the governing science, rather than aerodynamics. Applications of underwater foils occur in hydroplanes, sailboats and submarines.
Go to Article

Explanation by Hotspot Model

Wing

Wing

Wing

A wing is a type of fin that produces lift, while moving through air or some other fluid. As such, wings have streamlined cross-sections that are subject to aerodynamic forces and act as an airfoils. A wing's aerodynamic efficiency is expressed as its lift-to-drag ratio. The lift a wing generates at a given speed and angle of attack can be one to two orders of magnitude greater than the total drag on the wing. A high lift-to-drag ratio requires a significantly smaller thrust to propel the wings through the air at sufficient lift.

Lifting structures used in water, include various foils, including hydrofoils. Hydrodynamics is the governing science, rather than aerodynamics. Applications of underwater foils occur in hydroplanes, sailboats and submarines.

Etymology and usage

The word "wing" from the Old Norse vængr[1] for many centuries referred mainly to the foremost limbs of birds (in addition to the architectural aisle). But in recent centuries the word's meaning has extended to include lift producing appendages of insects, bats, pterosaurs, boomerangs, some sail boats and aircraft, or the inverted airfoil on a race car that generates a downward force to increase traction.[citation needed]

In nature

In nature wings have evolved in dinosaurs, birds, mammals, fish, reptiles and plants as means of locomotion.[citation needed] Various species of penguins and other flighted or flightless water birds such as auks, cormorants, guillemots, shearwaters, eider and scoter ducks and diving petrels are avid swimmers, and use their wings to propel through water.[2]

Wing forms in nature

Aerodynamics

The design and analysis of the wings of aircraft is one of the principal applications of the science of aerodynamics, which is a branch of fluid mechanics. The properties of the airflow around any moving object can – in principle – be found by solving the Navier-Stokes equations of fluid dynamics. However, except for simple geometries these equations are notoriously difficult to solve.[3] Fortunately, simpler explanations can be described.

For a wing to produce "lift", it must be oriented at a suitable angle of attack relative to the flow of air past the wing. When this occurs the wing deflects the airflow downwards, "turning" the air as it passes the wing. Since the wing exerts a force on the air to change its direction, the air must exert a force on the wing, equal in size but opposite in direction. This force manifests itself as differing air pressures at different points on the surface of the wing.[4][5][6]

A region of lower-than-normal air pressure is generated over the top surface of the wing, with a higher pressure on the bottom of the wing. (See: airfoil) These air pressure differences can be either measured directly using instrumentation, or can be calculated from the airspeed distribution using basic physical principles—including Bernoulli's Principle, which relates changes in air speed to changes in air pressure.

The lower air pressure on the top of the wing generates a smaller downward force on the top of the wing than the upward force generated by the higher air pressure on the bottom of the wing. Hence, a net upward force acts on the wing. This force is called the "lift" generated by the wing.

The different velocities of the air passing by the wing, the air pressure differences, the change in direction of the airflow, and the lift on the wing are intrinsically one phenomenon. It is, therefore, possible to calculate lift from any of the other three. For example, the lift can be calculated from the pressure differences, or from different velocities of the air above and below the wing, or from the total momentum change of the deflected air. Fluid dynamics offers other approaches to solving these problems—and all produce the same answers if done correctly. Given a particular wing and its velocity through the air, debates over which mathematical approach is the most convenient to use can be mistaken by novices as differences of opinion about the basic principles of flight.[7]

Cross-sectional shape

Wings with an asymmetrical cross section are the norm in subsonic flight. Wings with a symmetrical cross section can also generate lift by using a positive angle of attack to deflect air downward. Symmetrical airfoils have higher stalling speeds than cambered airfoils of the same wing area[8] but are used in aerobatic aircraft[citation needed] as they provide practical performance whether the aircraft is upright or inverted. Another example comes from sailboats, where the sail is a thin membrane with no path-length difference between one side and the other.[9]

For flight speeds near the speed of sound (transonic flight), airfoils with complex asymmetrical shapes are used to minimize the drastic increase in drag associated with airflow near the speed of sound.[10] Such airfoils, called supercritical airfoils, are flat on top and curved on the bottom.[11]

Design features

Aircraft wings may feature some of the following:

  • A rounded leading edge cross-section
  • A sharp trailing edge cross-section
  • Leading-edge devices such as slats, slots, or extensions
  • Trailing-edge devices such as flaps or flaperons (combination of flaps and ailerons)
  • Winglets to keep wingtip vortices from increasing drag and decreasing lift
  • Dihedral, or a positive wing angle to the horizontal, increases spiral stability around the roll axis, whereas anhedral, or a negative wing angle to the horizontal, decreases spiral stability.

Aircraft wings may have various devices, such as flaps or slats that the pilot uses to modify the shape and surface area of the wing to change its operating characteristics in flight.

Applications

Besides fixed-wing aircraft, applications for wing shapes include:[citation needed]

Tensile structures

In 1948, Francis Rogallo invented the fully limp flexible wing, which ushered in new possibilities for aircraft. Near in time, Domina Jalbert invented flexible un-sparred ram-air airfoiled thick wings. These two new branches of wings have been since extensively studied and applied in new branches of aircraft, especially altering the personal recreational aviation landscape.[citation needed]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht