powered by CADENAS

Social Share

Audi S and RS models (2725 views - Cars & Motorbikes & Trucks & Buse)

Audi S and RS models are a range of high performance versions of certain car models of the German automotive company AUDI AG. These cars primarily focus on enhanced "sport" performance. Production of Audi "S" cars began in 1990 with the S2 Coupé, whilst the first "RS" car appeared four years later with the Audi RS 2 Avant. Today's S and RS models are based on the A/TT/Q models with the same number (e.g S4/RS 4 is based on the A4 or the TT RS based on the TT), but the "Ur-S4" from 1991 — 1994 was based on the Audi 100/200 later named A6 and the first S2/RS2 generation from 1990 — 1995 was based on the Audi 80/90 platform later replaced by the A4.
Go to Article

Explanation by Hotspot Model

Youtube


    

Audi S and RS models

Audi S and RS models

Audi S, Audi RS
Overview
Manufacturer Audi AG
Production 1983 — present
Assembly Audi Sport GmbH
Neckarsulm, Germany
Body and chassis
Class Sports cars (S)
Layout Front-engine, all-wheel-drive
Quattro

Audi S and RS models are a range of high performance versions of certain car models of the German automotive company AUDI AG. These cars primarily focus on enhanced "sport" performance.[1] Production of Audi "S" cars began in 1990 with the S2 Coupé, whilst the first "RS" car appeared four years later with the Audi RS 2 Avant.

Today's S and RS models are based on the A/TT/Q[2] models with the same number (e.g S4/RS 4 is based on the A4 or the TT RS based on the TT), but the "Ur-S4" from 1991 — 1994 was based on the Audi 100/200 later named A6 and the first S2/RS2 generation from 1990 — 1995 was based on the Audi 80/90 platform later replaced by the A4.

History

The history of road versions of Audi racing cars begins in the 1980s. from models Audi Quattro and Audi Sport Quattro made by concern Audi AG in the city of Ingolstadt. In 1983, the company Quattro GmbH was founded (since November 2016, "Audi Sport GmbH") in the city of Neckarsulm responsible for the development of sports models of cars of Audi brand. In 1990, appeared based on the model Audi 80 sports model S2 as a receiver Audi Quattro but already under the designation of the series "S" in the name and having a capacity of 220 hp. And in 1994 there was even more powerful model Audi RS2 Avant based on Audi 80 model of joint development of Audi and Porsche having 315 hp. The model was equipped with components from Porsche. As in 1973, Audi, together with Porsche, also developed a prototype based on the Audi 100 Coupé S, produced in 1968, which has 112 hp. the "Grand tourer" class. which received the name "100 Coupé S V3" and was equipped with a V8 engine with a power of 350 hp.

Since 1994, the development of the Audi S and RS sports series was started directly from the Quattro GmbH (Audi Sport GmbH)[3]

S models

Numerous "S" models, from most of Audi's mainstream model ranges have been produced over the years. These cars are recognisable by their "S" badges, and unique emphasis lines on their front grills and on the back side, instead of the letter "A" in the designation of numbers and also in use in the notation "S3", "TTS" and "SQ5".[4]

All Audi "S" models are equipped with Audi's 'trademark' quattro four-wheel drive system as standard.[5] Unique internal combustion engines, along with larger, more powerful brakes, stiffer suspension systems, additional exterior body styling, and carbon fibre interior trims set them apart from their related "siblings" of their respective model range.[6]

In the past, some Audi S models competed directly with BMW M and Mercedes-AMG models, such as the B6 Audi S4 4.2 FSI versus the BMW M3 and Mercedes-Benz C32 AMG.[1] Since 2010 however, Audi S models have been positioned more as optional engine trims. For instance the base Audi A4 (B8) engine is the 2.0 TFSI turbo four-cylinder, and with the discontinuation of the 3.2 FSI V6, that makes the Audi S4's 3.0 TFSI V6 the performance option (the B8 Audi S4 3.0 TFSI positioned closer to the E90 BMW 335i than the BMW M3). The Audi A6 (C7) no longer has a V8 engine upgrade in the non "S" range, with the discontinuation of the C6 Audi A6 4.2 FSI that was offered from 2004 – 2011, one must go to the C7 Audi S6 4.0 TFSI [2].

Audi "S" models should not be confused with the Audi "A, Q, TT" series, equipped with a package "S line" models, which feature leather trim, S-line badging, sports steering wheel and sports suspension, but they are not equipped with a high-power engine.[4][7]

RS models

Audi Sport GmbH (formerly quattro GmbH), AUDI AGs high performance private subsidiary, creates even higher performance versions, known by their "RS" badging. The "RS" initials are taken from the German: RennSport — literally translated as "racing sport". The characteristics and cost of these cars are close and equal to cars belonging to the supercar class.[8]

RS is Audi's highest performance 'top-tier' trim level, positioned distinctly above the "S" ("Sport") specification level of Audi's regular model range. All "RS" cars pioneer some of Audi's latest and most advanced technology and engineering prowess, therefore, "RS" cars could be described[by whom?] as "halo vehicles". Audi RS cars are some of the most powerful vehicles ever offered by Audi as well as R8. Audi RS 6 (5.0 TFSI quattro), for instance, is more powerful than the physically larger Audi S8 (5.2 FSI quattro)[5] However, the 2012 — 2015 Audi S8 shares the same engine as the 2013 — ... Audi RS 6 and Audi RS7, albeit in a lower state of tune, while for the 2016 — 2017 model years, the Audi S8 plus features an uprated engine with the same output as the smaller RS 6 and RS7.

Available for limited time and only in select markets, on a restricted model range, these "RS" (and "S" models)[9] models are wholly designed, developed and produced in—house by Audi AG's high performance private subsidiary company, Audi Sport GmbH, at its Neckarsulm factory.[10]

Unlike Audi "S" models whose interiors well-furnished in order to retain the feel of sport luxury, the interior of Audi "RS" models are often spartan by comparison as the emphasis is more on track performance than luxury. The 2008 Audi RS 4 sold in Europe had lightweight racing-style front seats and roll-up windows for the rear doors, although its counterpart sold in the United States has luxurious power-adjustable front seats and power windows for all doors [3].

Audi "RS" models are considered direct competitors to similar sized hardcore sport models from BMW M and Mercedes-AMG, whereas the Audi "S" models (as of 2010) have been positioned more as engine upgrades. Taking the 2012 model year for example, the Audi RS 5 competes directly with the BMW M3, M4[11] whereas the Audi S5 competes with the BMW 335i, while the Audi RS 6 competes with the BMW M5 and the Audi S6 competes with the BMW 550i. However the Audi RS 6 (C6) was never exported to the United States due to emissions regulations, leaving the Audi S6 (C6) as the top performing trim to compete against the BMW M5 (E60) in that market [4].

There used to be only one RS model in production at a time, but recently Audi has revised its policies and decided to make more than one RS model at a time, claiming that "customers want them, then why not give it to them". However, RS models are not available in all markets; for instance the North American market only has the RS7 available and not the RS6 Avant.

Сomparison A / S / RS series Audi by example 6—line of models[12]
Model name Engine type Engine displacement Power Acceleration 0—62 mph (0–100 km/h) Top speed Image
A6 I4 — V6 1.8 — 3.0 l. 190 — 333 PS 7.9 — 5.1 sec. 145 —155 mph

(233 – 250 km/h)

S6 V8 4.0 l. 450 PS 4.4 sec. 155 mph

(250 km/h)

RS 6 V8 4.0 l. 560 — 605 PS 3.9 — 3.7 sec. 190 mph

(305 km/h)

Model range

The following Audi "S" and "RS" high performance models are being, or have been produced, or are speculated to be in future production:

Current models

(In model range order)

Audi
model name
VW Group
platform
Typ
code
engine type max.motive power acceleration

0—62 mph

(0–100 km/h)

top speed car body style(s) weight production
year(s)
image
Audi RS 4[13] MLB Evo B9 2,9 V6 TFSI 331 kW (450 PS; 444 bhp) 4.1 sec. 155 mph (250 km/h)

174 mph (280 km/h)

5 dr, 5 seat Avant (estate/wagon)
1,790 kg
2018
Audi RS 5 MLB Evo F5 2,9 V6 TFSI 331 kW (450 PS; 444 bhp) 3.9 sec. 174 mph

(280 km/h)

2 dr, 4 seat mid-size Coupé
1,730 kg
2018
Audi S5 MLB Evo F5 2,995 cc V6 TFSI 260 kW (354 PS; 349 bhp) 4.7 sec. 155 mph

(250 km/h)

2 dr, 4 seat mid-size Coupé


4 dr, 4 seat Sportback (fastback)


2 dr, 4 seat mid-size Cabriolet

1,690 kg
1,735 kg
1,840 kg
2018
Audi S1 PQ25 8X EA888 2.0 litre turbo 170 kW (231 PS; 228 bhp) 5.8 sec. 155 mph

(250 km/h)

3 dr, 5 seat Supermini


5 dr, 5 seat Supermini (sportback)

1,315 kg
2015
Audi TTS MQB 8S 1,984 cc I4 TFSI 228 kW (310 PS; 306 bhp) 4,9 — 4,6 sec.

(coupé)


5,2 — 5,9 sec.

(roadster)

155 mph

(250 km/h)

2 dr 2 seat compact Coupé


2 dr, 2 seat compact
Roadster (convertible)

1,440 kg
1,525 kg
2014
Audi TT RS MQB 8S 2,480 cc R5 20v TFSI 294 kW (400 PS; 394 bhp) 3,7 sec. (coupé)

3,9 sec. (roadster)

174 mph

(280 km/h)

2 dr, 2 seat compact Coupé


2 dr, 2 seat compact
Roadster (convertible)

1,515 kg
1,605 kg
2017
Audi S3 MQB 8V 2.0 I4 TFSI 228 kW (310 PS; 306 bhp) 5.4 — 5.1 sec.

(hatch. 3 dr.)

5.3 — 4.9 sec.

(hatch. 5 dr.)

5.3 — 4.9 sec. (sedan)

5.4 sec. (cabriolet)

155 mph

(250 km/h)

3 dr, 5 seat Hatchback


5 dr, 5 seat Hatchback

4 dr, 5 seat Saloon

(sedan)

2 dr, 4 seat Cabriolet

1,150
1,520 kg
2014


2017 (facelift)




Audi RS 3 Sportback & Sedan MQB 8V 2,5 cc R5 20v TFSI 294 kW (400 PS; 394 bhp) 3.9 sec. 155 mph

(250 km/h)

174 mph

(280 km/h)

5 dr, 5 seat Hatchback


4 dr, 5 seat Saloon (sedan)

1,585 kg
1,590 kg
2017
Audi S4 B9 (PL48)
(Audi MLB/MLP)
8W 2,998 cc V6 TFSI 260 kW (354 PS; 349 bhp) 4.4 sec. 155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)

5 dr, 5 seat Avant (estate/wagon)

1,705 kg
1,750 kg
2016
Audi S6 MLB 4G 3,993 cc V8 TFSI 331 kW (450 PS; 444 bhp) 4.9 / 4.8 sec. (2012)

(avant/sedan)

4.6 / 4.4 sec. (2014)

(avant/sedan)

155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)

1,970 kg
2,035 kg
2012

2014 (facelift)


Audi RS 6 MLB 4G 4.0 V8 TFSI 412 kW (560 PS; 553 bhp)
445 kW (605 PS; 597 bhp) (performance)
3.9 sec.

3.7 sec. (performance)

190 mph

(305 km/h)

5 dr, 5 seat Avant (estate/wagon)
2,025 kg
2014


2015 (facelift)


2016 (performance)


Audi S7 MLB 4G 3,993 cc V8 TFSI 309 kW (420 PS; 414 bhp)
331 kW (450 PS; 444 bhp)

(facelift)

4.7 sec. (2012)

4.6 sec. (2014)

155 mph

(250 km/h)

5 dr, 4 seat Sportback (fastback)
2,030 kg
2012


2014 (facelift)


Audi RS 7 MLB 4G 3,993 cc V8 TFSI 412 kW (560 PS; 553 bhp)
445 kW (605 PS; 597 bhp)

(performance) (2016)

3.9 sec.

3.7 sec. (performance)

190 mph

(305 km/h)

5 dr, 4 seat Sportback (fastback)
2,005 kg
2013

2014 (facelift)


2016 (performance)


Audi S8 MLB Evo 4H 3,993 cc V8 TFSI 382 kW (519 PS; 512 bhp)
445 kW (605 PS; 597 bhp)

(plus) (2016)

4.1 sec.

3.8 sec. (plus)

190 mph

(305 km/h)

4 dr, 5 seat Saloon (sedan)
2,065 kg
2012


2016 (plus)

Audi RS Q3 A5 (PQ35) 8U 2,485 cc R5 TFSI 228 kW (310 PS; 306 bhp)

(2013)


250 kW (340 PS; 335 bhp)

(2014)


270 kW (367 PS; 362 bhp) (performance)

5.2 sec. (2013)

4.8 sec. (2014)

155 mph

(250 km/h)

4 dr, 5 seat Crossover
1,655 kg
2013


2014 (facelift)


Audi SQ5 MLB Evo FY 3.0 V6 TFSI 260 kW (354 PS; 349 bhp) 5.4 sec. 155 mph

(250 km/h)

4 dr, 5 seat Crossover
1,945 kg
2017
Audi SQ7 MLB 4M 3,956 cc V8 TDI 320 kW (435 PS; 429 bhp) 4.8 sec. 155 mph

(250 km/h)

4 dr, 5 seat Crossover
2,270 kg
2017

Former models

(In chronological order of production end — oldest first)

Audi
model name
VW Group
platform
Typ
code
engine type max. motive power acceleration

0—62 mph

(0–100 km/h)

top speed car body style(s) weight production
year(s)
image
Audi 80 S2 B3, B4 8B, 8C 2.2L l5 20vT 162–169 kW (220–230 PS; 217–227 bhp) 6.1 — 5.8 sec. 150 — 153 mph

(242 – 246 km/h)

2 dr, 5 seat Coupé


5 dr, 5 seat Avant (estate/wagon)


4 dr, 5 seat Saloon (sedan)

1,525 kg[14]
1990 — 1995
Audi 100 S4
("Ur-S4")
C4 4A 2.2L l5 20vT 169 kW (230 PS; 227 bhp) 6.8 sec. 152 mph

(244 km/h)

4 dr, 5 seat Saloon (sedan)
1,610

1,730 kg
1991 — 1994
Audi 80 RS 2 B4 8C 2.2L l5 20vT 232 kW (315 PS; 311 bhp) 4.8 sec. 163 mph

(262 km/h)

5 dr, 5 seat Avant (estate/wagon)
2,100 kg
1994 — 1995
Audi S6

("Ur-S6")

C4 4A 2.2L l5 20vT
4.2 V8
169 kW (230 PS; 227 bhp)
213 kW (290 PS; 286 bhp)
6.9 — 5.9 sec. 150 — 155 mph

(241 – 250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)

1,730 kg 
1,780 kg
1995 — 1997
Audi S6 plus C4 4A 4.2 V8 240 kW (326 PS; 322 bhp) 5.6 sec. (sedan)

5.7 sec. (avant)

155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)

1,730 kg 
1,780 kg
1996 — 1997
Audi RS 4 Avant B5 (PL45) 8D 2.7 V6 T 280 kW (381 PS; 375 bhp) 4.9 sec. 155 mph

(250 km/h)

5 dr, 5 seat Avant (estate/wagon)
1,620 kg
2000 — 2001
Audi S8 D2 (PL62) 4D 4.2 V8 250–265 kW (340–360 PS; 335–355 bhp) 6.8 — 5.5 sec. (1996)

6.6 — 5.4 sec. (1999)

155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)
1,730 kg

-

1,845 kg
1996 — 2002
Audi S4 B5 (PL45) 8D 2.7 V6 T 195 kW (265 PS; 261 bhp) 5.8 — 5.6 sec. 155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)

1,535 kg

-

1,680 kg
1997 — 2002
Audi S6 C5 4B 4.2 V8 250 kW (340 PS; 335 bhp) 6.7 — 5.7 sec. (sedan)

6.8 — 5.8 sec. (avant)

155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)

1,815 kg 
1,825 kg
1999 — 2002
Audi S3 A4 (PQ34) 8L 1.8 I4 20vT 154–165 kW (209–224 PS; 207–221 bhp) 6.9 sec. (1999)

6.6 sec. (2001)

148 mph

238 km/h (1999)

151 mph

243 km/h (2001)

3 dr, 5 seat Hatchback
1,375

1,420 kg
1999 — 2003
Audi RS 6 C5 4B 4.2 V8 40vT 331 kW (450 PS; 444 bhp) 4.9 sec. 155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)

1,840 kg 
1,865 kg
2002 — 2004
Audi RS 6 plus C5 4B 4.2 V8 40vT 353 kW (480 PS; 473 bhp) 4.4 sec. 174 mph

(280 km/h)

5 dr, 5 seat Avant (estate/wagon)
1,880[15] 
2004 (like a previous photo)
Audi S4 B6 (PL46) 8E 4.2 V8 40v 253 kW (344 PS; 339 bhp) 5.8 — 5.6 sec. (sedan)

5.9 — 5.8 sec. (avant)

6.2 — 5.9 sec. (cabrio.)

155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)


2 dr, 4 seat Cabriolet

(convertible)

1,660 kg 
1,720 kg 
1,855 kg
2003 — 2005

Audi RS 4 B7 (PL47) 8E 4,163 cc V8 FSI 309 kW (420 PS; 414 bhp) 4.8 sec. (sedan)

4.9 sec. (avant)

4.9 sec. (cabrio.)

155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)

2 dr, 4 seat Cabriolet

(convertible)

 1,650 - 1,680 kg
1,710 kg
 1,845 kg
2006 — 2008 (saloon)


2006 - 2007 (Avant)

2007 — 2008 (Cabrio.)



Audi S4 B7 (PL47) 8E 4.2 V8 40v 253 kW (344 PS; 339 bhp) 5.8 — 5.6 sec. (sedan)

5.9 — 5.8 sec. (avant)

6.2 — 5.9 sec. (cabrio.)

155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)

2 dr, 4 seat Cabriolet

(convertible)

1,660

1,895 kg
2005 — 2008,


2006 — 2009 (Cabrio.)



Audi S6 C6 4F 5,204 cc V10 FSI

(Lamborghini V10)

320 kW (435 PS; 429 bhp) 5.2 sec. (sedan)

5.3 sec. (avant)

155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)

1,910 kg 
1,970 kg 
2006 — 2011
Audi RS 6 C6 4F 4,991 cc V10 TFSI

(Lamborghini V10)

427 kW (581 PS; 573 bhp) 4.6 sec. 155 mph

(250 km/h)

188 mph

(303 km/h) (Plus)

4 dr, 5 seat Saloon (sedan)

5 dr, 5 seat Avant (estate/wagon)

1985 

2,025 kg
2008 — 2010
Audi S8 D3 (PL63) 4E 5,204 cc V10 FSI

(Lamborghini V10)[16]

331 kW (450 PS; 444 bhp) 5.1 sec. 155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)
1,940 kg
2006 — 2010
Audi S4 B8 8E 3.0 V6 TFSI 245 kW (333 PS; 329 bhp) 5.3 — 5.1 sec. (sedan)

5.4 — 5.2 sec. (avant)

155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)

1,725 

1,825 kg
2009 — 2011
Audi S3 A5 (PQ35) 8P 1,984 cc I4 TFSI 195 kW (265 PS; 261 bhp) 5.7 sec. 155 mph

(250 km/h)

3 dr, 5 seat Hatchback

5 dr, 5 seat Hatchback

1,530 

-

 1,590 kg
2006 — 2012

2008 — 2012


Audi RS 3 Sportback A5 (PQ35) 8P 2,480 cc R5 TFSI 250 kW (340 PS; 335 bhp) 4.6 sec. 155 mph

(250 km/h)

5 dr, 5 seat Hatchback
1,650 kg
2011 — 2012
Audi S8 D4 4H 3,993 cc V8 TFSI 382 kW (519 PS; 512 bhp) 4.2 sec. 155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)
2,050

2,065 kg
2012 — 2013
Audi TTS A5 (PQ35) 8J 1,984 cc I4 TFSI 200 kW (272 PS; 268 bhp) 5.4 — 5.2 sec. (coupé)

5,6 — 5,4 sec. (roadster)

155 mph

(250 km/h)

2 dr, 2 seat compact Coupé

2 dr, 2 seat compact Roadster (convertible)

1,470

1,570 kg
2008 — 2014
Audi TT RS A5 (PQ35) 8J 2,480 cc R5 TFSI 250–265 kW (340–360 PS; 335–355 bhp) 4.6 — 4.3 sec. (coupé)

4.7 — 4.4 sec. (roadster)

4.3 — 4.1 sec.

(coupé) (plus)

4.4 — 4.2 sec. (roadster) (plus)

155 mph

(250 km/h)

174 mph

(280 km/h) (plus)

2 dr, 2 seat compact Coupé


2 dr, 2 seat compact Roadster (convertible)

1,525

1,610 kg
2009 — 2014
Audi RS 3 Sportback MQB 8V 2,480 cc R5 20v TFSI 270 kW (367 PS; 362 bhp) 4.3 sec. 174 mph

(280 km/h)

5 dr, 5 seat Hatchback
1,595 kg
2015
Audi S4 B8 (PL48)
(Audi MLB/MLP)
8K 2,998 cc V6 TFSI 245 kW (333 PS; 329 bhp) 5.1 sec. 155 mph

(250 km/h)

4 dr, 5 seat Saloon (sedan)


5 dr, 5 seat Avant (estate/wagon)

1,725

1,825 kg
2012 — 2015
Audi S5 B8 (PL48)
(Audi MLB/MLP)
8T 2,998 cc V6 TFSI
4,163 cc V8 FSI
245 kW (333 PS; 329 bhp)
260 kW (354 PS; 349 bhp)
5.6 — 4.9 sec. 155 mph

(250 km/h)

2 dr, 4 seat mid—size Coupé


2 dr, 4 seat Cabriolet

(convertible)


4 dr, 4 seat Sportback (fastback)

1,750 kg 
1,955 kg 
1,820 kg
2007


2011(facelift)



Audi RS 5[17] B8 (PL48)

(Audi MLB/MLP)

8T 4,163 cc V8 FSI 331 kW (450 PS; 444 bhp) 4.6 sec. (2010)

4.5 sec. (2012)

4.9 sec. (2012 — ...)

(cabriolet)

250 km/h

280 km/h (with raised speed limiter)

2 dr, 4 seat mid—size Coupé

2 dr, 4 seat Cabriolet

(convertible)

1,790 –1,800 kg

1,995 kg
2010

2013 (facelift)


Audi RS 4 B8 (PL48)
(Audi MLB/MLP)
8K 4,163 cc V8 FSI 331 kW (450 PS; 444 bhp) 4.7 sec. 174 mph

(280 km/h)

5 dr, 5 seat Avant (estate/wagon)
1,795 kg
2012 — 2015
Audi SQ5 MLB 8R 2,995 cc V6 TFSI


2,967 cc V6 BiTDI

260 kW (354 PS; 349 bhp)
230–250 kW

(313–340 PS; 308–335 bhp)

5.4 sec. (gasoline)

5.1 sec. (diesel)

155 mph

(250 km/h)

4 dr, 5 seat Crossover
1,830 kg
2013

Audi S line

"S line" badge in front grille

Audi produce a specification of optional sports trim packages to their mainstream models A/Q/TT, known as the S line. This is merely a trim specification which allows customers to effect a sporty appearance in their mainstream Audi model. Whilst the specific S line trim parts are designed and produced by Audi Sport GmbH at its Neckarsulm factory, these mainstream cars are still manufactured and assembled by AUDI AG at their relevant factories on the same production lines alongside their other standard models.

Cars with S line trim are not to be confused with the specific high performance offerings — the "S" models (made by AUDI AG), and the "RS" models (made by Audi Sport GmbH); Audi cars with S line trim bear identical performance figures to their counterparts with base or SE trim levels.[4]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Cars & Motorbikes & Trucks & Buse

Car, Truck,MotorBike, Bicycle, Engine, Racer, Bus