powered by CADENAS

Social Share

Purlin (6260 views - Architecure & BIM & MEP)

In architecture, structural engineering or building, a purlin (or historically purline, purloyne, purling, perling) is any longitudinal, horizontal, structural member in a roof except a type of framing with what is called a crown plate. In traditional timber framing there are three basic types of purlin: purlin plate, principal purlin and common purlin.
Go to Article

Explanation by Hotspot Model

Purlin

Purlin

In architecture, structural engineering or building, a purlin (or historically purline, purloyne, purling, perling) is any longitudinal, horizontal, structural member in a roof except a type of framing with what is called a crown plate. In traditional timber framing there are three basic types of purlin: purlin plate, principal purlin and common purlin.

Purlin plates in wooden construction

A purlin plate in wooden construction is also called an "arcade plate" in European English,[1] "under purlin", and "principal purlin". The term plate means a major, horizontal, supporting timber. Purlin plates are beams which support the mid-span of rafters and are supported by posts. By supporting the rafters they allow longer spans than the rafters alone could span thus allowing a wider building. Purlin plates are very commonly found in large, old barns in North America. A crown plate has similarities to a purlin plate but supports collar beams in the middle of a timber framed building.

Principal purlins in wood construction

Principal purlins in wood construction, also called "major purlin", "side purlin". Principal purlins are supported by principal rafters and support common rafters in what is known as a "double roof" (a roof framed with a layer of principal rafters and a layer of common rafters). Principal purlins are further classified by how they connect to the principal rafters: "Through purlins" pass over the top; "butt purlins" tenon into the sides of the principal rafters; "clasped purlins," of which only one historic U.S. example is known,[citation needed]) are captured by a collar beam. Through purlins are further categorized as trenched, back, or clasped; butt purlins are classified as threaded, tenoned, and/or[clarification needed] staggered.[2]

Common purlins in wood construction

Common purlins in wood construction, also called a "major-rafter minor-purlin system".[3] Common purlins are typically "trenched through" the top sides (backs) of principal rafters and carry vertical roof sheathing (The key to identifying this type of roof system). Common purlin roofs in North America are found in areas settled by Englishmen and may have been a new invention in the Massachusetts Bay Colony. No examples of framed buildings with common purlin roofs have been reported in England, however some stone barns in England have vertically boarded, common purlin roofs. Historically, these roofs are found in New England, the highest concentration in Maine, and isolated parts of New York and along the St. Lawrence River in Canada. One of the oldest extant (surviving) examples is in the Coffin House in Newbury, Massachusetts from 1678. The purpose of a common purlin roof may be they allow a board roof, that is a roof of nothing but vertically laid boards with seams covered with battens or another layer of boards.[4]

Steel construction

In steel construction, the term purlin typically refers to roof framing members that span parallel to the building eave, and support the roof decking or sheeting. The purlins are in turn supported by rafters or walls. Purlins are most commonly used in Metal Building Systems, where Z-shapes are utilized in a manner that allows flexural continuity between spans.

It is the practice in the steel industry that structural shapes are assigned representative designations for convenient shorthand description on drawings and documentation: Channel sections, with or without flange stiffeners, are usually referenced as C shapes; Channel sections without flange stiffeners are also referenced as U shapes; Point symmetric sections that are shaped similar to the letter Z are referenced as Z shapes. Section designations can be regional and even specific to a manufacturer. In steel building construction, secondary members such as purlins (roof) and girts (wall) are frequently cold-formed steel C, Z or U sections, (or mill rolled) C sections.

Cold formed members can be efficient on a weight basis relative to mill rolled sections for secondary member applications. Additionally, Z sections can be nested for transportation bundling and, on the building, lapped at the supports to develop a structurally efficient continuous beam across multiple supports.

Etymology

Information on the origin of the term "purlin" is scant. The Oxford Dictionary suggests a French origin, with the earliest quote using a variation of purlin in 1447.

Gallery

Note: The sketches in this section reference terminology commonly used in the UK and Australia.[5]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Architecure & BIM & MEP

Autodesk Revit, Nemetschek ArchiCAD, Nemetschek Allplan, Vectorworks, Bentley AECOMSIM, Bentley Microstation, Trimble Tekla, Trimble Sketchup, EliteCAD, Ascon Renga, BricsCAD, Hexagon, Rhinoceros CAD, Sweet Home 3D, BIM Object, BIM component, BIM library, BIM family, BIM catalog, GIS, Advanced Steel, AutoCAD MEP, linear, MagiCAD, Relux, TGA, VDI 3805, Lod100, Lod200, Lod300, Lod350, Lod400, Lod500, Loi, IFC, BuildingSmart, BIM family creation, 3D, Download, MEP BIM product library