powered by CADENAS

Social Share

Amazon

Capsule hotel (3422 views - Foodservice / Horeca)

A capsule hotel (Japanese: カプセルホテル, romanized: kapuseru hoteru), also known as a pod hotel, is a type of hotel developed in Japan that features a large number of small bed-sized rooms known as capsules. Capsule hotels provide cheap, basic overnight accommodation for guests who do not require or who cannot afford larger, more expensive rooms offered by more conventional hotels.
Go to Article

Explanation by Hotspot Model

Youtube


    

Capsule hotel

Capsule hotel

A capsule hotel (Japanese: カプセルホテル, romanizedkapuseru hoteru), also known as a pod hotel, is a type of hotel developed in Japan that features a large number of small bed-sized rooms known as capsules. Capsule hotels provide cheap, basic overnight accommodation for guests who do not require or who cannot afford larger, more expensive rooms offered by more conventional hotels.

Description

The guest room is a chamber roughly the length and width of a single bed, with sufficient height for a hotel guest to crawl in and sit up on the bed. The chamber walls may be made of wood, metal or any rigid material, but are often fibreglass or plastic. Amenities within the room generally include a small television, air conditioning, an electronic console, and power sockets. The capsules are stacked side-by-side, two units high, with steps or ladders providing access to the second level rooms, similar to bunk beds. The open end of the capsule can be closed with a curtain or a solid door for privacy, but cannot be locked.[1]

Like a hostel, many amenities are communally shared, including toilets, showers, wireless internet, and dining rooms. In Japan, a capsule hotel may have a communal bath and sauna. Some hotels also provide restaurants, snack bars or bars (or at least vending machines), pools, and other entertainment facilities. There may be a lounge with upholstered chairs for relaxing, along with newspapers and reading material.[2]

Capsule hotels vary in size, from fifty or so capsules to 700, and primarily cater to men.[3] Some capsule hotels offer separate sections for male and female guests, or even separate floors and separate elevators. Clothes and shoes are exchanged for a yukata and slippers on entry, and a towel and bathrobe may also be provided. Luggage and valuables are usually stored in lockers or — if available — in-room safes.[1] Guests are asked not to smoke or eat in the capsules.[4]

Customer base

The benefit of these hotels is convenience and low price, usually around ¥2000–4000 (USD 18–36) a night.

In Japan, capsule hotels have been stereotypically used by Japanese salarymen who may be too drunk to return home safely, have missed the last train of the day to make a return trip home, or are too embarrassed to face their spouses.[5] During the Japanese Recession, unemployed or underemployed workers who had become homeless during the crisis temporarily rented capsules by the month. As of 2010, these customers made up 30% of visitors at the Capsule Hotel Shinjuku 510 in Tokyo.[6]

In the West, such hotels are known as pod hotels.[7]

History

The first capsule hotel in the world opened in 1979 and was the Capsule Inn Osaka, located in the Umeda district of Osaka, Japan and designed by Kisho Kurokawa.[8][9] From there, it spread to other cities within Japan.

Since then, concept has further spread to various other territories, including China,[10] Belgium,[11] Iceland,[12] Hong Kong,[13] Indonesia,[14] and India.[15]

Criticism and disadvantages

Due to the arrangement of capsules, Web Urbanist has compared the beds in capsule hotels to corpse drawers in a morgue.[16] In addition, because of the small interior space, Forbes advised that claustrophobic guests should not use capsule hotels.[1]

Some capsules may not have air conditioning in the capsules, leading to poor air flow, especially with the privacy curtain or door shut; furthermore, due to the close proximity of guests, pods with thin plastic walls easily transmit sounds made by other guests bumping into the walls.[1]

Because some capsule hotels are designed around single-night stays, guests intending to stay for more than one day must check out and check in again every day.[1]

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Foodservice / Horeca

FCSI, HKI, EFCEBIM, food services, food equipement, hotel, recreation, catering, kitchen appliances, dining, cooking, baking, furniture, oven, cafeterias, hospital