Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This article has multiple issues. Please help improve it or discuss these issues on the talk page. (Learn how and when to remove these template messages)
(Learn how and when to remove this template message)
|
Teaware is a broad international spectrum of equipment used in the brewing and consumption of tea. Many components make up that spectrum, and vary greatly based upon the type of tea being prepared, and the cultural setting in which it is being prepared. This is often referred to as the tea ceremony, and holds much significance in many cultures, particularly in northwestern Europe and in eastern Asia.
The following are a few of the essential components:
Tea bowl (茶碗, chawan)- Tea bowls are available in a wide range of sizes and styles, and different styles are used for thick and thin tea. Shallow bowls, which allow the tea to cool rapidly, are used in summer; deep bowls are used in winter. Bowls are frequently named by their creators or owners, or by a tea master. Bowls over four hundred years old are in use today, but only on unusually special occasions. The best bowls are thrown by hand, and some bowls are extremely valuable. Irregularities and imperfections are prized: they are often featured prominently as the "front" of the bowl.
Tea whisk (茶筅, chasen)- This is the implement used to mix the powdered tea with the hot water. Tea whisks are carved from a single piece of bamboo. There are various types. Tea whisks quickly become worn and damaged with use, and the host should use a new one when holding a chakai or chaji.
Tea caddy (棗, Natsume)- The small lidded container in which the powdered tea is placed for use in the tea-making procedure ([お]手前; [お]点前; [御]手前, [o]temae).
Tea scoop (茶杓, chashaku)- Tea scoops generally are carved from a single piece of bamboo, although they may also be made of ivory or wood. They are used to scoop tea from the tea caddy into the tea bowl. Bamboo tea scoops in the most casual style have a nodule in the approximate center. Larger scoops are used to transfer tea into the tea caddy in the mizuya (preparation area), but these are not seen by guests. Different styles and colours are used in various tea traditions.
Chakin (茶巾)- The "chakin" is a small rectangular white linen or hemp cloth mainly used to wipe the tea bowl.
Tea equipment may be constructed of many materials, from iron in Japan to porcelain and clay in China, and also bamboo and other woods. Of particular repute are the Yixing clay teapots produced in eastern China. (See: Yixing clay teapot).
The above tea wares were also mentioned by Lu Yu except for the stone mill (石磨) and tea whisk (茶筅)in The Classic of Tea .[citation needed]
This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
FCSI, HKI, EFCEBIM, food services, food equipement, hotel, recreation, catering, kitchen appliances, dining, cooking, baking, furniture, oven, cafeterias, hospital