powered by CADENAS

Social Share

Amazon

Turboshaft (20746 views - Mechanical Engineering)

A turboshaft engine is a form of gas turbine that is optimized to produce shaft power rather than jet thrust. In concept, turboshaft engines are very similar to turbojets, with additional turbine expansion to extract heat energy from the exhaust and convert it into output shaft power. They are even more similar to turboprops, with only minor differences, and a single engine is often sold in both forms. Turboshaft engines are commonly used in applications that require a sustained high power output, high reliability, small size, and light weight. These include helicopters, auxiliary power units, boats and ships, tanks, hovercraft, and stationary equipment.
Go to Article

Explanation by Hotspot Model

Youtube


    

Turboshaft

Turboshaft

A turboshaft engine is a form of gas turbine that is optimized to produce shaft power rather than jet thrust.

In concept, turboshaft engines are very similar to turbojets, with additional turbine expansion to extract heat energy from the exhaust and convert it into output shaft power. They are even more similar to turboprops, with only minor differences, and a single engine is often sold in both forms.

Turboshaft engines are commonly used in applications that require a sustained high power output, high reliability, small size, and light weight. These include helicopters, auxiliary power units, boats and ships, tanks, hovercraft, and stationary equipment.

Overview

A turboshaft engine may be made up of two major parts assemblies: the 'gas generator' and the 'power section'. The gas generator consists of the compressor, combustion chambers with ignitors and fuel nozzles, and one or more stages of turbine. The power section consists of additional stages of turbines, a gear reduction system, and the shaft output. The gas generator creates the hot expanding gases to drive the power section. Depending on the design, the engine accessories may be driven either by the gas generator or by the power section.

In most designs, the gas generator and power section are mechanically separate so they can each rotate at different speeds appropriate for the conditions, referred to as a 'free power turbine'. A free power turbine can be an extremely useful design feature for vehicles, as it allows the design to forgo the weight and cost of complex multiple-ratio transmissions and clutches.

The general layout of a turboshaft is similar to that of a turboprop. The main difference is a turboprop is structurally designed to support the loads created by a rotating propeller, as the propeller is not attached to anything but the engine itself. In contrast, turboshaft engines usually drive a transmission which is not structurally attached to the engine. The transmission is attached to the vehicle structure and supports the loads created instead of the engine. In practice, though, many of the same engines are built in both turboprop and turboshaft versions, with only minor differences.

An unusual example of the turboshaft principle is the Pratt & Whitney F135-PW-600 turbofan engine for the STOVL F-35B – in conventional mode it operates as a turbofan, but when powering the LiftFan, it switches partially to turboshaft mode to send 29,000 horsepower forward through a shaft[1] and partially to turbofan mode to continue to send thrust to the main engine's fan and rear nozzle.

Large helicopters use two or three turboshaft engines for redundancy. The Mil Mi-26 uses two Lotarev D-136 at 11,400 hp each,[2] while the Sikorsky CH-53E Super Stallion uses three General Electric T64 at 4,380 hp each.[3]

Early turboshaft engines were adaptations of turboprop engines, delivering power through a shaft driven directly from the gas generator shafts, via a reduction gearbox. Examples of direct-drive turboshafts include marinised or industrial Rolls-Royce Dart engines.

History

The first examples of a gas turbine engine design ever considered for armoured fighting vehicles, the BMW 003-based GT 101, were tested in Nazi Germany's Panther tanks in mid-1944.[4] The first true turboshaft engine for helicopters was built by the French engine firm Turbomeca, led by the founder, Joseph Szydlowski. In 1948, they built the first French-designed turbine engine, the 100-shp 782. Originally conceived as an auxiliary power unit, it was soon adapted to aircraft propulsion, and found a niche as a powerplant for turboshaft-driven helicopters in the 1950s. In 1950, this work was used to develop the larger 280-shp Artouste, which was widely used on the Aérospatiale Alouette II and other helicopters. This was following the experimental installation of a Boeing T50 turboshaft in an example of the Kaman K-225 synchropter on December 11, 1951, as the world's first-ever turboshaft-powered helicopter of any type to fly.[5] The T-80 tank, which entered service with the Soviet Army in 1976, was the first tank using a gas turbine as the main engine. Since 1980 the US Army has operated the M1 Abrams tank. Designed and built in the late 1970s, this tank makes use of a gas turbine engine compared to most tanks using reciprocating diesels. The engine has considerably fewer parts, mechanically is very reliable, produces reduced exterior noise, and runs on virtually any fuel: petrol (gasoline), diesel fuel, aviation fuels. Similarly, the Swedish Stridsvagn 103 was the first tank to utilize a gas turbine, in this case as a secondary, high-horsepower "sprint" engine to augment the primary piston engine's performance.

See also



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Mechanical Engineering

AutoCAD, SolidWorks, Autodesk Inventor, FreeCAD, Catia, Siemens NX, PTC Creo, Siemens Solid Edge, Microstation, TurboCAD, Draftsight, IronCAD, Spaceclaim, VariCAD, OnShape, IntelliCAD,T-FLEX, VariCAD, TenadoCAD, ProgeCAD, Cadra, ME10, Medusa, Designspark, KeyCreator, Caddy, GstarCAD, Varimetrix, ASCON Kompas-3D, Free Download, Autocad, 2D Library, DXF, DWG, 2D drawing, 3D digital library, STEP, IGES, 3D CAD Models, 3D files, CAD library, 3D CAD files, BeckerCAD, MegaCAD, Topsolid Missler, Vero VisiCAD, Acis SAT, Cimatron, Cadceus, Solidthinking, Unigraphics, Cadkey, ZWCAD, Alibre, Cocreate, MasterCAM, QCAD.org, QCAD, NanoCAD