powered by CADENAS

Social Share

Sea Jet (2760 views - Transportation - Air Water Earth)

Sea Jet, or Advanced Electric Ship Demonstrator (AESD), is a naval testbed funded by the U.S. Navy's Office of Naval Research. The 133-foot (41 m) vessel is operated out of the Carderock Division's Acoustic Research Detachment in Bayview, Idaho. Sea Jet was operated on Lake Pend Oreille, where she was used for test and demonstration of various technologies. Among the first technologies tested was an underwater discharge water jet from Rolls-Royce Naval Marine, Inc., called AWJ-21, a propulsion concept with the goals of providing increased propulsive efficiency, reduced acoustic signature, and improved maneuverability over previous Destroyer Class combatants.Sea Jet demonstrates a few technologies that will be integrated into the Zumwalt-class destroyer. Notable among these is the return of the tumblehome hull design.
Go to Article

Explanation by Hotspot Model

Sea Jet

Sea Jet

Sea Jet
Sea Jet, an Advanced Electric Ship Demonstrator
History
Name: Sea Jet
Christened: August 24, 2005[1]
In service: December 2005
Status: Active
General characteristics
Type: Experimental testbed
Displacement: 239,900 lb (108,800 kg)[2]
Length: 133 ft (41 m)[2]
Propulsion: RIMJET
Speed:
  • Diesel: 8 kn (15 km/h; 9.2 mph)
  • Electric: 16 kn (30 km/h; 18 mph)[2]
Armament: None

Sea Jet, or Advanced Electric Ship Demonstrator (AESD),[1] is a naval testbed funded by the U.S. Navy's Office of Naval Research. The 133-foot (41 m) vessel is operated out of the Carderock Division's Acoustic Research Detachment in Bayview, Idaho.[2] Sea Jet was operated on Lake Pend Oreille, where she was used for test and demonstration of various technologies. Among the first technologies tested was an underwater discharge water jet from Rolls-Royce Naval Marine, Inc., called AWJ-21, a propulsion concept with the goals of providing increased propulsive efficiency, reduced acoustic signature, and improved maneuverability over previous Destroyer Class combatants.[3]

Sea Jet demonstrates a few technologies that will be integrated into the Zumwalt-class destroyer.[1] Notable among these is the return of the tumblehome hull design.

  1. ^ a b c "Sea Jet Advanced Electric Ship Demonstrator (AESD)". GlobalSecurity.org. Retrieved 16 March 2015. 
  2. ^ a b c d Palmer, William (Fall 2005). "Advanced Electric Ship Demonstrator" (PDF). SEAFRAME. United States Navy, Carderock Division. 1 (2): 12–13. 
  3. ^ Hanlon, Mike (26 August 2005). "US Navy unveils Advanced Electric Stealth Ship Demonstrator". Gizmag. 


This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Transportation - Air Water Earth

3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht