powered by CADENAS

Social Share

Dragonfly (12787 views - Animals)

A dragonfly is an insect belonging to the order Odonata, infraorder Anisoptera (from Greek ἄνισος anisos, "uneven" and πτερόν pteron, "wing", because the hindwing is broader than the forewing). Adult dragonflies are characterized by large, multifaceted eyes, two pairs of strong, transparent wings, sometimes with coloured patches, and an elongated body. Dragonflies can be mistaken for the related group, damselflies (Zygoptera), which are similar in structure, though usually lighter in build; however, the wings of most dragonflies are held flat and away from the body, while damselflies hold the wings folded at rest, along or above the abdomen. Dragonflies are agile fliers, while damselflies have a weaker, fluttery flight. Many dragonflies have brilliant iridescent or metallic colours produced by structural coloration, making them conspicuous in flight. An adult dragonfly's compound eyes have nearly 24,000 ommatidia each. Fossils of very large dragonfly ancestors in the Protodonata are found from 325 million years ago (Mya) in Upper Carboniferous rocks; these had wingspans up to about 750 mm (30 in). About 3000 species of Anisoptera are in the world today. Most are tropical, with fewer species in temperate regions. Dragonflies are predators, both in their aquatic larval stage, when they are known as nymphs or naiads, and as adults. Several years of their lives are spent as nymphs living in fresh water; the adults may be on the wing for just a few days or weeks. They are fast, agile fliers, sometimes migrating across oceans, and are often found near water. They have a uniquely complex mode of reproduction involving indirect insemination, delayed fertilization, and sperm competition. During mating, the male grasps the female at the back of the head or on the prothorax, and the female curls her abdomen under her body to pick up sperm from the male's secondary genitalia at the front of his abdomen, forming the "heart" or "wheel" posture. Loss of wetland habitat threatens dragonfly populations around the world. Dragonflies are represented in human culture on artifacts such as pottery, rock paintings, and Art Nouveau jewellery. They are used in traditional medicine in Japan and China, and caught for food in Indonesia. They are symbols of courage, strength, and happiness in Japan, but seen as sinister in European folklore. Their bright colours and agile flight are admired in the poetry of Alfred, Lord Tennyson and the prose of H. E. Bates.
Go to Article

Explanation by Hotspot Model

Dragonfly

Dragonfly

Dragonfly

Licensed under Creative Commons Attribution-Share Alike 2.5 (André Karwath aka Aka).

Dragonfly
Temporal range: 325–0 Ma
Late Carboniferous – recent
Yellow-winged darter
Sympetrum flaveolum
Scientific classification
Kingdom: Animalia
Clade: Euarthropoda
Class: Insecta
Order: Odonata
Suborder: Epiprocta
Infraorder: Anisoptera
Selys, 1854
Families
$Not a clade

A dragonfly is an insect belonging to the order Odonata, infraorder Anisoptera (from Greek ἄνισος anisos, "uneven" and πτερόν pteron, "wing", because the hindwing is broader than the forewing). Adult dragonflies are characterized by large, multifaceted eyes, two pairs of strong, transparent wings, sometimes with coloured patches, and an elongated body. Dragonflies can be mistaken for the related group, damselflies (Zygoptera), which are similar in structure, though usually lighter in build; however, the wings of most dragonflies are held flat and away from the body, while damselflies hold the wings folded at rest, along or above the abdomen. Dragonflies are agile fliers, while damselflies have a weaker, fluttery flight. Many dragonflies have brilliant iridescent or metallic colours produced by structural coloration, making them conspicuous in flight. An adult dragonfly's compound eyes have nearly 24,000 ommatidia each.

Fossils of very large dragonfly ancestors in the Protodonata are found from 325 million years ago (Mya) in Upper Carboniferous rocks; these had wingspans up to about 750 mm (30 in). About 3000 species of Anisoptera are in the world today. Most are tropical, with fewer species in temperate regions.

Dragonflies are predators, both in their aquatic larval stage, when they are known as nymphs or naiads, and as adults. Several years of their lives are spent as nymphs living in fresh water; the adults may be on the wing for just a few days or weeks. They are fast, agile fliers, sometimes migrating across oceans, and are often found near water. They have a uniquely complex mode of reproduction involving indirect insemination, delayed fertilization, and sperm competition. During mating, the male grasps the female at the back of the head or on the prothorax, and the female curls her abdomen under her body to pick up sperm from the male's secondary genitalia at the front of his abdomen, forming the "heart" or "wheel" posture.

Loss of wetland habitat threatens dragonfly populations around the world. Dragonflies are represented in human culture on artifacts such as pottery, rock paintings, and Art Nouveau jewellery. They are used in traditional medicine in Japan and China, and caught for food in Indonesia. They are symbols of courage, strength, and happiness in Japan, but seen as sinister in European folklore. Their bright colours and agile flight are admired in the poetry of Alfred, Lord Tennyson and the prose of H. E. Bates.

Phylogeny

Dragonflies and their relatives are an ancient group. The oldest fossils are of the Protodonata from the 325 Mya Upper Carboniferous of Europe, a group that included the largest insect that ever lived, Meganeuropsis permiana from the early Permian, with a wingspan around 750 mm (30 in);[2] their fossil record ends with the Permian–Triassic extinction event (about 247 Mya). The Protanisoptera, another ancestral group which lacks certain wing vein characters found in modern Odonata, lived from the Early to Late Permian age until the end Permian event, and are known from fossil wings from current day United States, Russia, and Australia, suggesting they might have been cosmopolitan in distribution. The forerunners of modern Odonata are included in a clade called the Panodonata, which include the basal Zygoptera (damselflies) and the Anisoptera (true dragonflies)[3] Today there are some 3000 species extant around the world.[4][5]

The relationships of anisopteran families are not fully resolved as of 2013, but all the families are monophyletic except the Corduliidae; the Gomphidae are a sister taxon to all other Anisoptera, the Austropetaliidae are sister to the Aeshnoidea, and the Chlorogomphidae are sister to a clade that includes the Synthemistidae and Libellulidae.[6] On the cladogram, dashed lines indicate unresolved relationships; English names are given (in parentheses):

Anisoptera


Gomphidae (clubtails)





Austropetaliidae



Aeshnoidea (hawkers)



Petaluridae (petaltails)





Macromiidae (cruisers)






Libelluloidea


Neopetaliidae



Cordulegastridae (goldenrings)




Libellulidae (skimmers)



"Corduliidae" [not a clade] (emeralds)




Synthemistidae (tigertails)




Chlorogomphidae







Distribution and diversity

About 3012 species of dragonflies were known in 2010; these are classified into 348 genera in 11 families. The distribution of diversity within the biogeographical regions are summarised below (the world numbers are not ordinary totals, as overlaps in species occur).[7]

Family Oriental Neotropical Australasian Afrotropical Palaearctic Nearctic Pacific World
Aeshnidae 149 129 78 44 58 40 13 456
Austropetaliidae 7 4 11
Petaluridae 1 6 1 2 10
Gomphidae 364 277 42 152 127 101 980
Chlorogomphidae 46 5 47
Cordulegastridae 23 1 18 46
Neopetaliidae 1 1
Corduliidae 23 20 33 6 18 51 12 154
Libellulidae 192 354 184 251 120 105 31 1037
Macromiidae 50 2 17 37 7 10 125
Synthemistidae 37 9 46
Incertae sedis 37 24 21 15 2 99

Dragonflies are found on every continent except Antarctica. In contrast to the damselflies (Zygoptera), which tend to have restricted distributions, some genera and species are found across continents. For example, the blue-eyed darner Rhionaeschna multicolor is found all across North America, and in Central America;[8] emperors Anax are found throughout the Americas from as far north as Newfoundland to as far south as Bahia Blanca in Argentina,[9] across Europe to central Asia, North Africa, and the Middle East.[10] The globe skimmer Pantala flavescens is probably the most widespread dragonfly species in the world; it is cosmopolitan, occurring on all continents in the warmer regions. Most Anisoptera species are tropical, with far fewer species in temperate regions.[11]

Dragonflies including libellulids and aeshnids are found in desert pools, for example in the Mojave Desert, where they are active in shade temperatures between 18 and 45 °C (64.4 to 113 °F); these insects were able to survive body temperatures above the thermal death point of insects of the same species found in cooler places.[12]

Dragonflies can be found from sea level up to the mountains, decreasing in species diversity with altitude.[13] Their altitudinal limit is about 3700 m, represented by a species of Aeshna in the Pamirs.[14]

Dragonflies become scarce at higher latitudes. They are not native to Iceland, but individuals are occasionally swept in by strong winds, including a Hemianax ephippiger native to North Africa, and an unidentified darter species.[15] In Kamchatka, only a few species of dragonfly including the treeline emerald Somatochlora arctica and some aeshnids such as Aeshna subarctica are found, possibly because of the low temperature of the lakes there.[16] The treeline emerald is also found in northern Alaska, within the Arctic Circle, making it the most northerly of all dragonflies.[17]

General description

Damselflies, like this Ischnura senegalensis, are more slender in build than dragonflies, and most hold their wings closed over their bodies.

Dragonflies (suborder Anisoptera) are heavy-bodied, strong-flying insects that hold their wings horizontally both in flight and at rest. By contrast, damselflies (suborder Zygoptera) have slender bodies and fly more weakly; most species fold their wings over the abdomen when stationary, and the eyes are well separated on the sides of the head.[7][18]

An adult dragonfly has three distinct segments, the head, thorax, and abdomen as in all insects. It has a chitinous exoskeleton of hard plates held together with flexible membranes. The head is large with very short antennae. It is dominated by the two compound eyes, which cover most of its surface. The compound eyes are made up of ommatidia, the numbers being greater in the larger species. Aeshna interrupta has 22650 ommatidia of two varying sizes, 4500 being large. The facets facing downward tend to be smaller. Petalura gigantea has 23890 ommatidia of just one size. These facets provide complete vision in the frontal hemisphere of the dragonfly.[19] The compound eyes meet at the top of the head (except in the Petaluridae and Gomphidae, as also in the genus Epiophlebia). Also, they have three simple eyes or ocelli. The mouthparts are adapted for biting with a toothed jaw; the flap-like labrum, at the front of the mouth, can be shot rapidly forward to catch prey.[20][21] The head has a system for locking it in place that consists of muscles and small hairs on the back of the head that grip structures on the front of the first thoracic segment. This arrester system is unique to the Odonata, and is activated when feeding and during tandem flight.[7]

The thorax consists of three segments as in all insects. The prothorax is small and is flattened dorsally into a shield-like disc which has two transverse ridges. The mesothorax and metathorax are fused into a rigid, box-like structure with internal bracing, and provides a robust attachment for the powerful wing muscles inside it.[22] The thorax bears two pairs of wings and three pairs of legs. The wings are long, veined, and membranous, narrower at the tip and wider at the base. The hindwings are broader than the forewings and the venation is different at the base.[23] The veins carry haemolymph, which is analogous to blood in vertebrates and carries out many similar functions, but which also serves a hydraulic function to expand the body between nymphal stages (instars) and to expand and stiffen the wings after the adult emerges from the final nymphal stage. The leading edge of each wing has a node where other veins join the marginal vein, and the wing is able to flex at this point. In most large species of dragonflies, the wings of females are shorter and broader than those of males.[21] The legs are rarely used for walking, but are used to catch and hold prey, for perching, and for climbing on plants. Each has two short basal joints, two long joints, and a three-jointed foot, armed with a pair of claws. The long leg joints bear rows of spines, and in males, one row of spines on each front leg is modified to form an "eyebrush", for cleaning the surface of the compound eye.[22]

Migrant hawker, Aeshna mixta, has the long slender abdomen of aeshnid dragonflies.

The abdomen is long and slender and consists of 10 segments and a terminal appendage-bearing segment. The second and third segments are enlarged, and in males, a cleft on the underside of the second segment contains a pair of claspers and the penis. The spermaries open on the 9th segment. In females, the genital opening is on the underside of the eighth segment and is covered by a simple flap or an ovipositor, depending on species and the method of egg-laying.[22]

Dragonfly nymphs vary in form with species and are loosely classed into claspers, sprawlers, hiders, and burrowers.[7] The first instar is known as a prolarva, a relatively inactive stage from which it quickly moults into the more active nymphal form.[24] The general body plan is similar to that of an adult, but the nymph lacks wings and reproductive organs. The lower jaw has a huge, extensible labium, armed with hooks and spines, which is used for catching prey. This labium is folded under the body at rest and struck out at great speed by hydraulic pressure created by the abdominal muscles.[7] Whereas damselfly nymphs have three feathery external gills, dragonfly nymphs have internal gills, located around the fourth and fifth abdominal segments. Water is pumped in and out of the abdomen through an opening at the tip. The naiads of some clubtails (Gomphidae) that burrow into the sediment, have a snorkel-like tube at the end of the abdomen enabling them to draw in clean water while they are buried in mud. Naiads can forcefully expel a jet of water to propel themselves with great rapidity.[25]

Coloration

Iridescent structural coloration in a dragonfly's eyes

Many adult dragonflies have brilliant iridescent or metallic colours produced by structural coloration, making them conspicuous in flight. Their overall coloration is often a combination of yellow, red, brown, and black pigments, with structural colours. Blues are typically created by microstructures in the cuticle that reflect blue light. Greens often combine a structural blue with a yellow pigment. Freshly emerged adults, known as tenerals, are often pale-coloured and obtain their typical colours after a few days,[23] some have their bodies covered with a pale blue, waxy powderiness called pruinosity; it wears off when scraped during mating, leaving darker areas.[26]

Some dragonflies, such as the green darner, Anax junius, have a noniridescent blue which is produced structurally by scatter from arrays of tiny spheres in the endoplasmic reticulum of epidermal cells underneath the cuticle.[27]

The wings of dragonflies are generally clear, apart from the dark veins and pterostigmata. In the chasers (Libellulidae), however, many genera have areas of colour on the wings: for example, groundlings (Brachythemis) have brown bands on all four wings, while some scarlets (Crocothemis) and dropwings (Trithemis) have bright orange patches at the wing bases. Some aeshnids such as the brown hawker (Aeshna grandis) have translucent, pale yellow wings.[28]

Dragonfly nymphs are usually a well-camouflaged blend of dull brown, green, and grey.[25]

Biology

Ecology

Dragonflies and damselflies are predatory both in the aquatic nymphal and adult stages. Nymphs feed on a range of freshwater invertebrates and larger ones can prey on tadpoles and small fish.[29] Adults capture insect prey in the air, making use of their acute vision and highly controlled flight. The mating system of dragonflies is complex and they are among the few insect groups that have a system of indirect sperm transfer along with sperm storage, delayed fertilization, and sperm competition.[29]

Adult males vigorously defend territories near water; these areas provide suitable habitat for the larvae to develop, and for females to lay their eggs. Swarms of feeding adults aggregate to prey on swarming prey such as emerging flying ants or termites.[29]

Dragonflies as a group occupy a considerable variety of habitats, but many species, and some families, have their own specific environmental requirements.[30] Some species prefer flowing waters, while others prefer standing water. For example, the Gomphidae (clubtails) live in running water, and the Libellulidae (skimmers) live in still water.[30] Some species are found in temporary water pools and are capable of tolerating changes in water level, desiccation, and the resulting variations in temperature, but some genera such as Sympetrum (darters) have eggs and larvae that can resist drought and are stimulated to grow rapidly in warm, shallow pools, also often benefiting from the absence of predators there.[30] Vegetation and its characteristics including submerged, floating, emergent, or waterside are also important. Adults may require emergent or waterside plants to use as perches; others may need specific submerged or floating plants on which to lay eggs. Requirements may be highly specific, as in Aeshna viridis (green hawker), which lives in swamps with the water-soldier, Stratiotes aloides.[30] The chemistry of the water, including its trophic status (degree of enrichment with nutrients) and pH can also affect its use by dragonflies. Most species need moderate conditions, not too eutrophic, not too acid;[30] a few species such as Sympetrum danae (black darter) and Libellula quadrimaculata (four-spotted chaser) prefer acidic waters such as peat bogs,[31] while others such as Libellula fulva (scarce chaser) need slow-moving, eutrophic waters with reeds or similar waterside plants.[32][33]

Behaviour

Many dragonflies, particularly males, are territorial. Some defend a territory against others of their own species, some against other species of dragonfly and a few against insects in unrelated groups. A particular perch may give a dragonfly a good view over an insect-rich feeding ground, and the blue dasher (Pachydiplax longipennis) jostles other dragonflies to maintain the right to alight there.[34]

Defending a breeding territory is fairly common among male dragonflies, especially among species that congregate around ponds in large numbers. The territory contains desirable features such as a sunlit stretch of shallow water, a special plant species, or a particular substrate necessary for egg-laying. The territory may be small or large, depending on its quality, the time of day, and the number of competitors, and may be held for a few minutes or several hours. Some dragonflies signal ownership with striking colours on the face, abdomen, legs, or wings. The common whitetail (Plathemis lydia) dashes towards an intruder holding its white abdomen aloft like a flag. Other dragonflies engage in aerial dogfights or high-speed chases. A female must mate with the territory holder before laying her eggs.[34] There is also conflict between the males and females. Females may sometimes be harassed by males to the extent that it affects their normal activities including foraging and in some dimorphic species females have evolved multiple forms with some forms appearing deceptively like males.[35] In some species females have evolved behavioural responses such as feigning death to escape the attention of males.[36]

Reproduction

Mating in dragonflies is a complex, precisely choreographed process. First, the male has to attract a female to his territory, continually driving off rival males. When he is ready to mate, he transfers a packet of sperm from his primary genital opening on segment 9, near the end of his abdomen, to his secondary genitalia on segments 2–3, near the base of his abdomen. The male then grasps the female by the head with the claspers at the end of his abdomen; the structure of the claspers varies between species, and may help to prevent interspecific mating.[37] The pair flies in tandem with the male in front, typically perching on a twig or plant stem. The female then curls her abdomen downwards and forwards under her body to pick up the sperm from the male's secondary genitalia, while the male uses his "tail" claspers to grip the female behind the head: this distinctive posture is called the "heart" or "wheel";[29][38] the pair may also be described as being "in cop".[39]

Egg-laying (ovipositing) involves not only the female darting over floating or waterside vegetation to deposit eggs on a suitable substrate, but also the male hovering above her or continuing to clasp her and flying in tandem. The male attempts to prevent rivals from removing his sperm and inserting their own,[40] something made possible by delayed fertilisation[29][38] and driven by sexual selection.[37] If successful, a rival male uses his penis to compress or scrape out the sperm inserted previously; this activity takes up much of the time that a copulating pair remains in the heart posture.[39] Flying in tandem has the advantage that less effort is needed by the female for flight and more can be expended on egg-laying, and when the female submerges to deposit eggs, the male may help to pull her out of the water.[40]

Egg-laying takes two different forms depending on the species. The female in some families has a sharp-edged ovipositor with which she slits open a stem or leaf of a plant on or near the water, so she can push her eggs inside. In other families such as clubtails (Gomphidae), cruisers (Macromiidae), emeralds (Corduliidae), and skimmers (Libellulidae), the female lays eggs by tapping the surface of the water repeatedly with her abdomen, by shaking the eggs out of her abdomen as she flies along, or by placing the eggs on vegetation.[39] In a few species, the eggs are laid on emergent plants above the water, and development is delayed until these have withered and become immersed.[25]

Life cycle

Nymph of emperor dragonfly, Anax imperator

Dragonflies are hemimetabolous insects; they do not have a pupal stage and undergo an incomplete metamorphosis with a series of nymphal stages from which the adult emerges.[41] Eggs laid inside plant tissues are usually shaped like grains of rice, while other eggs are the size of a pinhead, ellipsoidal, or nearly spherical. A clutch may have as many as 1500 eggs, and they take about a week to hatch into aquatic nymphs or naiads which moult between six and 15 times (depending on species) as they grow.[7] Most of a dragonfly's life is spent as a nymph, beneath the water's surface. The nymph extends its hinged labium (a toothed mouthpart similar to a lower mandible, which is sometimes termed as a "mask" as it is normally folded and held before the face) that can extend forward and retract rapidly to capture prey such as mosquito larvae, tadpoles, and small fish.[41] They breathe through gills in their rectum, and can rapidly propel themselves by suddenly expelling water through the anus.[42] Some naiads, such as the later stages of Antipodophlebia asthenes, hunt on land.[43]

Parts of a dragonfly nymph including the labial "mask"

The larval stage of dragonflies lasts up to five years in large species, and between two months and three years in smaller species. When the naiad is ready to metamorphose into an adult, it stops feeding and makes its way to the surface, generally at night. It remains stationary with its head out of the water, while its respiration system adapts to breathing air, then climbs up a reed or other emergent plant, and moults (ecdysis). Anchoring itself firmly in a vertical position with its claws, its skin begins to split at a weak spot behind the head. The adult dragonfly crawls out of its larval skin, the exuvia, arching backwards when all but the tip of its abdomen is free, to allow its exoskeleton to harden. Curling back upwards, it completes its emergence, swallowing air, which plumps out its body, and pumping haemolymph into its wings, which causes them to expand to their full extent.[44]

Dragonflies in temperate areas can be categorized into two groups, an early group and a later one. In any one area, individuals of a particular "spring species" emerge within a few days of each other. The springtime darner (Basiaeschna janata), for example, is suddenly very common in the spring, but has disappeared a few weeks later and is not seen again until the following year. By contrast, a "summer species" emerges over a period of weeks or months, later in the year. They may be seen on the wing for several months, but this may represent a whole series of individuals, with new adults hatching out as earlier ones complete their short lifespans which is an average of 7 months[45].[46]


Sex ratios

The sex ratio of male to female dragonflies varies both temporally and spatially. Adult dragonflies have a high male-biased ratio at breeding habitats. The male-bias ratio has contributed partially to the females using different habitats to avoid male harassment. As seen in Hine's emerald dragonfly (Somatochlora hineana), male populations use wetland habitats, while females use dry meadows and marginal breeding habitats, only migrating to the wetlands to lay their eggs or to find mating partners. Unwanted mating is energetically costly for females because it affects the amount of time that they are able to spend foraging.[47]

Flight

Dragonflies are powerful and agile fliers, capable of migrating across oceans, moving in any direction, and changing direction suddenly. In flight, the adult dragonfly can propel itself in six directions: upward, downward, forward, back, to left and to right.[48] They have four different styles of flight:[49] A number of flying modes are used that include counter-stroking, with forewings beating 180° out of phase with the hindwings, is used for hovering and slow flight. This style is efficient and generates a large amount of lift; phased-stroking, with the hindwings beating 90° ahead of the forewings, is used for fast flight. This style creates more thrust, but less lift than counter-stroking; synchronised-stroking, with forewings and hindwings beating together, is used when changing direction rapidly, as it maximises thrust; and gliding, with the wings held out, is used in three situations: free gliding, for a few seconds in between bursts of powered flight; gliding in the updraft at the crest of a hill, effectively hovering by falling at the same speed as the updraft; and in certain dragonflies such as darters, when "in cop" with a male, the female sometimes simply glides while the male pulls the pair along by beating his wings.[49]

Southern hawker, Aeshna cyanea: its wings at this instant are synchronised for agile flight.

The wings are powered directly, unlike most families of insects, with the flight muscles attached to the wing bases. Dragonflies have a high power/weight ratio, and have been documented accelerating at 4 G linearly and 9 G in sharp turns while pursuing prey.[49]

Dragonflies generate lift in at least four ways at different times, including classical lift like an aircraft wing; supercritical lift with the wing above the critical angle, generating high lift and using very short strokes to avoid stalling; creating vortices; and vortex shedding. Some families appear to use special mechanisms, as for example the Libellulidae which take off rapidly, their wings beginning pointed far forward and twisted almost vertically. Dragonfly wings behave highly dynamically during flight, flexing and twisting during each beat. Among the variables are wing curvature, length and speed of stroke, angle of attack, forward/back position of wing, and phase relative to the other wings.[49]

Flight speed

Old and unreliable claims are made that dragonflies such as the southern giant darner can fly up to 60 miles per hour (97 km/h).[50] However, the greatest reliable flight speed records are for other types of insects.[51] In general, large dragonflies like the hawkers have a maximum speed of 10–15 metres per second (22–34 mph) with average cruising speed of about 4.5 metres per second (10 mph).[52] Dragonflies can fly at 100 body-lengths per second, and three lengths per second backwards.[20]

Motion camouflage

In high-speed territorial battles between male Australian emperors (Hemianax papuensis), the fighting dragonflies adjust their flight paths to appear stationary to their rivals, minimizing the chance of being detected as they approach.[a][53][54] To achieve the effect, the attacking dragonfly flies towards his rival, choosing his path to remain on a line between the rival and the start of his attack path. The attacker thus looms larger as he closes on the rival, but does not otherwise appear to move. Researchers found that six of 15 encounters involved motion camouflage.[55]

Temperature control

The flight muscles need to be kept at a suitable temperature for the dragonfly to be able to fly. Being cold-blooded, they can raise their temperature by basking in the sun. Early in the morning, they may choose to perch in a vertical position with the wings outstretched, while in the middle of the day, a horizontal stance may be chosen. Another method of warming up used by some larger dragonflies is wing-whirring, a rapid vibration of the wings that causes heat to be generated in the flight muscles. The green darner (Anax junius) is known for its long-distance migrations, and often resorts to wing-whirring before dawn to enable it to make an early start.[56]

Becoming too hot is another hazard, and a sunny or shady position for perching can be selected according to the ambient temperature. Some species have dark patches on the wings which can provide shade for the body, and a few use the obelisk posture to avoid overheating. This behaviour involves doing a "handstand", perching with the body raised and the abdomen pointing towards the sun, thus minimising the amount of solar radiation received. On a hot day, dragonflies sometimes adjust their body temperature by skimming over a water surface and briefly touching it, often three times in quick succession. This may also help to avoid desiccation.[56]

Feeding

Adult dragonflies hunt on the wing using their exceptionally acute eyesight and strong, agile flight.[38] They are almost exclusively carnivorous, eating a wide variety of insects ranging from small midges and mosquitoes to butterflies, moths, damselflies, and smaller dragonflies.[52] A large prey item is subdued by being bitten on the head and is carried by the legs to a perch. Here, the wings are discarded and the prey usually ingested head first.[57] A dragonfly may consume as much as a fifth of its body weight in prey per day.[58]

The larvae are voracious predators, eating most living things that are smaller than they are. Their staple diet is mostly bloodworms and other insect larvae, but they also feed on tadpoles and small fish.[52] A few species, especially those that live in temporary waters, are likely to leave water. Nymphs of Cordulegaster bidentata sometimes hunt small arthropods on the ground at night.[7]

Predators and parasites

Although dragonflies are swift and agile fliers, some predators are fast enough to catch them. These include falcons such as the American kestrel, the merlin,[59] and the hobby;[60] nighthawks, swifts, flycatchers and swallows also take some adults; some species of wasps, too, prey on dragonflies, using them to provision their nests, laying an egg on each captured insect. In the water, various species of ducks and herons eat dragonfly larvae[59] and they are also preyed on by newts, frogs, fish, and water spiders.[61] Amur falcons, which migrate over the Indian Ocean at a period that coincides with the migration of the globe skimmer dragonfly, Pantala flavescens, may actually be feeding on them while on the wing.[62]

Dragonflies are affected by three major groups of parasites: water mites, gregarine protozoa, and trematode flatworms (flukes). Water mites, Hydracarina, can kill smaller dragonfly larvae, and may also be seen on adults.[63] Gregarines infect the gut and may cause blockage and secondary infection.[64] Trematodes are parasites of vertebrates such as frogs, with complex life cycles often involving a period as a stage called a cercaria in a secondary host, a snail. Dragonfly nymphs may swallow cercariae, or these may tunnel through a nymph's body wall; they then enter the gut and form a cyst or metacercaria, which remains in the nymph for the whole of its development. If the nymph is eaten by a frog, the amphibian becomes infected by the adult or fluke stage of the trematode.[65]

Dragonflies and humans

Conservation

Most odonatologists live in temperate areas and the dragonflies of North America and Europe have been the subject of much research. However, the majority of species live in tropical areas and have been little studied. With the destruction of rainforest habitats, many of these species are in danger of becoming extinct before they have even been named. The greatest cause of decline is forest clearance with the consequent drying up of streams and pools which become clogged with silt. The damming of rivers for hydroelectric schemes and the drainage of low-lying land has reduced suitable habitat, as has pollution and the introduction of alien species.[66]

In 1997, the International Union for Conservation of Nature set up a status survey and conservation action plan for dragonflies. This proposes the establishment of protected areas around the world and the management of these areas to provide suitable habitat for dragonflies. Outside these areas, encouragement should be given to modify forestry, agricultural, and industrial practices to enhance conservation. At the same time, more research into dragonflies needs to be done, consideration should be given to pollution control and the public should be educated about the importance of biodiversity.[66]

Habitat degradation has reduced dragonfly populations across the world, for example in Japan.[67] Over 60% of Japan's wetlands were lost in the 20th century, so its dragonflies now depend largely on rice fields, ponds, and creeks. Dragonflies feed on pest insects in rice, acting as a natural pest control.[68][69] Dragonflies are steadily declining in Africa, and represent a conservation priority.[70]

The dragonfly's long lifespan and low population density makes it vulnerable to disturbance, such as from collisions with vehicles on roads built near wetlands. Species that fly low and slow may be most at risk.[71]

Dragonflies are attracted to shiny surfaces that produce polarization which they can mistake for water, and they have been known to aggregate close to polished gravestones, solar panels, automobiles, and other such structures on which they attempt to lay eggs. These can have a local impact on dragonfly populations; methods of reducing the attractiveness of structures such as solar panels are under experimentation.[72][73]

In culture

A blue-glazed faience dragonfly amulet was found by Flinders Petrie at Lahun, from the Late Middle Kingdom of ancient Egypt.[74]

Dragonfly symbol on a Hopi bowl from Sikyátki, Arizona

For some Native American tribes, dragonflies represent swiftness and activity; for the Navajo, they symbolize pure water. They are a common motif in Zuni pottery; stylized as a double-barred cross, they appear in Hopi rock art and on Pueblo necklaces.[75]:20–26 They have been used in traditional medicine in Japan and China. In Indonesia, adults are caught on poles made sticky with birdlime, then fried in oil as a delicacy.[76]

In the United States, dragonflies and damselflies are sought out as a hobby similar to birding and butterflying, known as oding, from the Latin name of the dragonfly order, Odonata. Oding is especially popular in Texas, where 225 different species of odonates have been observed. With care, and with dry fingers, dragonflies can be handled and released by oders, as can be done with butterflies, though it is not encouraged.[77]

Tiffany & Co. Japonism vase with dragonfly handles, circa 1879, Walters Art Museum

Images of dragonflies are common in Art Nouveau, especially in jewellery designs.[78] They have also been used as a decorative motif on fabrics and home furnishings.[79] Douglas, a British motorcycle manufacturer based in Bristol, named its innovatively designed postwar 350-cc flat-twin model the Dragonfly.[80]

Among the classical names of Japan are Akitsukuni (秋津国), Akitsushima (秋津島), Toyo-akitsushima (豊秋津島). Akitu or akidu are archaic or dialectal Japanese words for dragonfly, so one interpretation of Akitsushima is "Dragonfly Island".[81] This is attributed to a legend in which Japan's mythical founder, Emperor Jinmu, was bitten by a mosquito, which was then eaten by a dragonfly.[82][83]

As a seasonal symbol in Japan, the dragonfly is associated with autumn.[84] More generally, dragonflies are symbols of courage, strength, and happiness, and they often appear in art and literature, especially haiku. Japanese children catch large dragonflies as a game, using a hair with a small pebble tied to each end, which they throw into the air. The dragonfly mistakes the pebbles for prey, gets tangled in the hair, and is dragged to the ground by the weight.[75]:38

In Europe, dragonflies have often been seen as sinister. Some English vernacular names, such as "horse-stinger",[85] "devil's darning needle", and "ear cutter", link them with evil or injury.[86] Swedish folklore holds that the devil uses dragonflies to weigh people's souls.[75]:25–27 The Norwegian name for dragonflies is Øyenstikker ("eye-poker"), and in Portugal, they are sometimes called tira-olhos ("eyes-snatcher"). They are often associated with snakes, as in the Welsh name gwas-y-neidr, "adder's servant".[86] The Southern United States term "snake doctor" refers to a folk belief that dragonflies follow snakes around and stitch them back together if they are injured.[87]

The watercolourist Moses Harris (1731–1785), known for his The Aurelian or natural history of English insects (1766), published in 1780, the first scientific descriptions of several Odonata including the banded demoiselle, Calopteryx splendens. He was the first English artist to make illustrations of dragonflies accurate enough to be identified to species (Aeshna grandis at top left of plate illustrated), though his rough drawing of a larva (at lower left) with the mask extended appears to be plagiarised.[b][88]

In poetry and literature

Lafcadio Hearn wrote in his 1901 book A Japanese Miscellany that Japanese poets had created dragonfly haiku "almost as numerous as are the dragonflies themselves in the early autumn."[89] The poet Matsuo Bashō (1644–1694) wrote haiku such as "Crimson pepper pod / add two pairs of wings, and look / darting dragonfly", relating the autumn season to the dragonfly.[90] Hori Bakusui (1718–1783) similarly wrote "Dyed he is with the / Colour of autumnal days, / O red dragonfly."[89]

The poet Alfred, Lord Tennyson, described a dragonfly splitting its old skin and emerging shining metallic blue like "sapphire mail" in his 1842 poem "The Two Voices", with the lines "An inner impulse rent the veil / Of his old husk: from head to tail / Came out clear plates of sapphire mail."[91]

The novelist H. E. Bates described the rapid, agile flight of dragonflies in his 1937 nonfiction book[92] Down the River:[93]

I saw, once, an endless procession, just over an area of water-lilies, of small sapphire dragonflies, a continuous play of blue gauze over the snowy flowers above the sun-glassy water. It was all confined, in true dragonfly fashion, to one small space. It was a continuous turning and returning, an endless darting, poising, striking and hovering, so swift that it was often lost in sunlight.[94]

In technology

A dragonfly has been genetically modified with light-sensitive "steering neurons" in its nerve cord to create a cyborg-like "DragonflEye". The neurons contain genes like those in the eye to make them sensitive to light. Miniature sensors, a computer chip and a solar panel were fitted in a "backpack" over the insect's thorax in front of its wings. Light is sent down flexible light-pipes named optrodes[c] from the backpack into the nerve cord to give steering commands to the insect. The result is a "micro-aerial vehicle that's smaller, lighter and stealthier than anything else that's manmade".[95][96]

Notes

  1. ^ This is not to say that other species may not use the same technique, only that this species has been studied.
  2. ^ Reviewing his artwork, the odonatologists Albert Orr and Matti Hämäläinen comment that his drawing of a 'large brown' (Aeshna grandis, top left of image) was "superb", while the "perfectly natural colours of the eyes indicate that Harris had examined living individuals of these aeshnids and either coloured the printed copper plates himself or supervised the colourists." However, they consider the larva on the same plate far less good, "a very stiff dorso-lateral view of an aeshnid larva with mask extended. No attempt has been made to depict the eyes, antennae or hinge on the mask or labial palps, all inconceivable omissions for an artist of Harris' talent had he actually examined a specimen", and they suggest he copied it from August Johann Rösel von Rosenhof.[88]
  3. ^ Optrode is a portmanteau of "optical electrode".
  1. ^ The Biology of Dragonflies. CUP Archive. p. 324. GGKEY:0Z7A1R071DD. No Dragonfly at present existing can compare with the immense Meganeura monyi of the Upper Carboniferous, whose expanse of wing was somewhere about twenty-seven inches. 
  2. ^ Resh, Vincent H.; Cardé, Ring T. (22 July 2009). Encyclopedia of Insects. Academic Press. p. 722. ISBN 978-0-08-092090-0. 
  3. ^ Grimaldi, David; Engel, Michael S. (2005). Evolution of the Insects. Cambridge University Press. pp. 175–187. 
  4. ^ Zhang, Z.-Q. (2011). "Phylum Arthropoda von Siebold, 1848 In: Zhang, Z.-Q. (Ed.) Animal biodiversity: An outline of higher-level classification and survey of taxonomic richness" (PDF). Zootaxa. 3148: 99–103. 
  5. ^ Dunkle, Sidney W. (2000). Dragonflies Through Binoculars: a field guide to the dragonflies of North America. Oxford University Press. ISBN 0-19-511268-7. 
  6. ^ Blanke, Alexander; Greve, Carola; Mokso, Rajmund; Beckmann, Felix; Misof, Bernhard (July 2013). "An updated phylogeny of Anisoptera including formal convergence analysis of morphological characters". Systematic Entomology. 38 (3): 474–490. doi:10.1111/syen.12012. 
  7. ^ a b c d e f g Suhling, F.; Sahlén, G.; Gorb, S.; Kalkman, V.J.; Dijkstra, K-D.B.; van Tol, J. (2015). "Order Odonata". In Thorp, James & D. Christopher Rogers. Ecology and general biology. Thorp and Covich's Freshwater Invertebrates (4 ed.). Academic Press. pp. 893–932. ISBN 9780123850263. 
  8. ^ Bybee, Seth (May 2012) [August 2005]. "Featured Creatures: dragonflies and damselflies". University of Florida. Retrieved 26 February 2015. 
  9. ^ Garrison, Rosser W.; Ellenrieder, Natalia von; Louton, Jerry A. (16 August 2006). Dragonfly Genera of the New World: An Illustrated and Annotated Key to the Anisoptera. JHU Press. p. 40. ISBN 978-0-8018-8446-7. 
  10. ^ "Emperor dragonfly (Anax imperator)". Arkive.org. Retrieved 26 February 2015. 
  11. ^ Powell 1999, p. 9.
  12. ^ Polcyn, D. M. (August 1994). "Thermoregulation During Summer Activity in Mojave Desert Dragonflies (Odonata: Anisoptera)". Functional Ecology. 8 (4): 441–449. doi:10.2307/2390067. JSTOR 2390067. 
  13. ^ Carchini, G.; Solimini, Angelo; Ruggiero, A. (2005). "Habitat Characteristics and Odonata Diversity in Mountain Ponds of Central Italy". Aquatic Conservation: Marine and Freshwater Ecosystems. 15 (6): 573–581. doi:10.1002/aqc.741. 
  14. ^ Mani, M.S. (1968). Ecology and Biogeography of High Altitude Insects. Springer. p. 246. ISBN 978-90-6193-114-0. 
  15. ^ "Dragonfly Spotted In Iceland". Reykjavik Grapevine. 26 August 2011. Retrieved 15 March 2015. 
  16. ^ Smetanin, A. N. (2013). "On the Insect Fauna of the Kichiga River Basin, Northeastern Kamchatka". Entomological Review. 93 (2): 160–173. doi:10.1134/s0013873813020048. 
  17. ^ Hudson, John; Armstrong, Robert H. (2010). Dragonflies of Alaska (PDF) (Second ed.). Nature Alaska Images. pp. 5, 32. ISBN 1-57833-302-4. 
  18. ^ Ruppert, Edward E.; Fox, Richard, S.; Barnes, Robert D. (2004). Invertebrate Zoology, 7th edition. Cengage Learning. p. 745. ISBN 978-81-315-0104-7. 
  19. ^ Pritchard, Gordon (1966). "On the morphology of the compound eyes of dragonflies (Odonata: Anisoptera), with special reference to their role in prey capture". Proceedings of the Royal Entomological Society of London. 41: 1–8. doi:10.1111/j.1365-3032.1966.tb01126.x. 
  20. ^ a b "Introduction to the Odonata". UCMP Berkeley. Retrieved 24 February 2015. 
  21. ^ a b Berger 2004, pp. 5–6.
  22. ^ a b c Needham, J.G. (1975). A Manual of the Dragonflies of North America. University of California Press. pp. 10–21. GGKEY:5YCUC2C45TH. 
  23. ^ a b Paulson, Dennis (2011). Dragonflies and Damselflies of the East. Princeton University Press. pp. 29–32. ISBN 1-4008-3966-1. 
  24. ^ Tennessen, K.J. (2009). "Odonata (Dragonflies, Damselflies)". In Resh, Vincent H. & Ring T. Carde. Encyclopedia of Insects (2 ed.). Academic Press. pp. 721–729. 
  25. ^ a b c Lawlor, Elizabeth P. (1999). Discover Nature in Water & Wetlands: Things to Know and Things to Do. Stackpole Books. pp. 88, 94–96. ISBN 978-0-8117-2731-0. 
  26. ^ Powell 1999, p. 102.
  27. ^ Prum, Richard O.; Cole, Jeff A.; Torres, Rodolfo H. (15 October 2004). "Blue integumentary structural colours in dragonflies (Odonata) are not produced by incoherent Tyndall scattering". Journal of Experimental Biology. 207 (22): 3999–4009. doi:10.1242/jeb.01240. PMID 15472030. 
  28. ^ Dijkstra 2006, pp. 26–35.
  29. ^ a b c d e Dijkstra 2006, pp. 8–9.
  30. ^ a b c d e Dijkstra 2006, pp. 13–14.
  31. ^ Dijkstra 2006, pp. 243, 272.
  32. ^ Dijkstra 2006, p. 246.
  33. ^ Ratcliffe, Derek (26 January 2012). A Nature Conservation Review: Volume 1: The Selection of Biological Sites of National Importance to Nature Conservation in Britain. Cambridge University Press. pp. 378–379. ISBN 978-0-521-20329-6. 
  34. ^ a b Berger 2004, pp. 32–34.
  35. ^ Fincke, Ola M (2004). "Polymorphic signals of harassed female odonates and the males that learn them support a novel frequency-dependent model". Animal Behaviour. 67 (5): 833. doi:10.1016/j.anbehav.2003.04.017. 
  36. ^ Khelifa, Rassim (2017). "Faking death to avoid male coercion: Extreme sexual conflict resolution in a dragonfly". Ecology. doi:10.1002/ecy.1781. 
  37. ^ a b Cordero-Rivera, Adolfo; Cordoba-Aguilar, Alex (2010). 15. Selective Forces Propelling Genitalic Evolution in Odonata (PDF). p. 343. 
  38. ^ a b c Trueman & Rowe 2009, p. Life Cycle and Behavior.
  39. ^ a b c Berger 2004, p. 39.
  40. ^ a b Cardé, Ring T.; Resh, Vincent H. (2012). A World of Insects: The Harvard University Press Reader. Harvard University Press. pp. 195–197. ISBN 978-0-674-04619-1. 
  41. ^ a b Bybee, Seth (1 May 2012). "Dragonflies and damselflies: Odonata". Featured Creatures. University of Florida: Entomology and Nematology. Retrieved 1 March 2015. 
  42. ^ Mill, P. J.; Pickard, R. S. (1975). "Jet-propulsion in anisopteran dragonfly larvae". Journal of Comparative Physiology A. 97 (4): 329–338. doi:10.1007/BF00631969. 
  43. ^ Corbet, Philip S. (1980). "Biology of odonata". Annual Review of Entomology. 25: 189–217. doi:10.1146/annurev.en.25.010180.001201. 
  44. ^ Berger 2004, pp. 10–11.
  45. ^ "How Long Do Dragonflies Live? Article Explains Their Lifespan". Retrieved 2017-11-28. 
  46. ^ Berger 2004, p. 9.
  47. ^ Foster, S.E; Soluk, D.A (2006). "Protecting more than the wetland: The importance of biased sex ratios and habitat segregation for conservation of the Hine's emerald dragonfly, Somatochlora hineana Williamson". Biological Conservation. 127: 158–166. doi:10.1016/j.biocon.2005.08.006. 
  48. ^ Waldbauer, Gilbert (2006). A Walk Around the Pond: Insects in and Over the Water. Harvard University Press. p. 105. ISBN 9780674022119. 
  49. ^ a b c d Rowe, Richard J. "Dragonfly Flight". Tree of Life. Retrieved 26 February 2015. 
  50. ^ Tillyard, Robert John (1917). The Biology of Dragonflies (PDF). pp. 322–323. Retrieved 15 December 2010. I doubt if any greater speed than this occurs amongst Odonata 
  51. ^ Dean, T. J. (2003-05-01). "Chapter 1 — Fastest Flyer". Book of Insect Records. University of Florida. Archived from the original on 2011-07-20. 
  52. ^ a b c "Frequently Asked Questions about Dragonflies". British Dragonfly Society. Retrieved 28 February 2015. 
  53. ^ Hopkin, Michael (June 5, 2003). "Nature News". Dragonfly flight tricks the eye. Nature.com. Retrieved January 16, 2012. 
  54. ^ Mizutani, A. K., Chahl, J. S. & Srinivasan, M. V. (June 5, 2003). "Insect behaviour: Motion camouflage in dragonflies". Nature. 65 (423): 604. doi:10.1038/423604a. 
  55. ^ Glendinning, Paul (27 January 2004). "Motion Camouflage" (PDF). The mathematics of motion camouflage. The Royal Society. 271: 477–81. doi:10.1098/rspb.2003.2622. PMC 1691618. PMID 15129957. 
  56. ^ a b Berger 2004, pp. 44–46.
  57. ^ Berger 2004, p. 31.
  58. ^ Powell 1999, p. 12.
  59. ^ a b Berger 2004, pp. 48–49.
  60. ^ "Hobby". BBC Nature. Retrieved 26 February 2015. 
  61. ^ Meister 2001, p. 16.
  62. ^ Anderson, R. Charles (2009). "Do dragonflies migrate across the western Indian Ocean?". Journal of Tropical Ecology. 25 (4): 347–358. doi:10.1017/S0266467409006087. 
  63. ^ Mead, Kurt. "Dragonfly Biology 101". Minnesota Dragonfly Society. Archived from the original on 27 February 2015. Retrieved 27 February 2015. 
  64. ^ Córdoba-Aguilar, Alex (28 August 2008). Dragonflies and Damselflies: Model Organisms for Ecological and Evolutionary Research. OUP Oxford. p. 176. ISBN 978-0-19-155223-6. 
  65. ^ "An Introduction To The Study of Invertebrate Zoology. Platyhelminthes". University of California, Riverside. Retrieved 27 February 2015. 
  66. ^ a b Moore, N.W. (1997). "Dragonflies: status survey and conservation action plan" (PDF). International Union for Conservation of Nature. Retrieved 13 September 2017. 
  67. ^ Taku, Kadoya; Shin-ichi, Suda; Izumi, Washitani (2009). "Dragonfly Crisis in Japan: A likely Consequence of Recent Agricultural Habitat Degradation". Biological Conservation. 142 (9): 1889–1905. doi:10.1016/j.biocon.2009.02.033. 
  68. ^ Channa N. B. Bambaradeniya; Felix P. Amerasinghe (2004). Biodiversity associated with the rice field agroecosystem in Asian countries: A brief review. IWMI. p. 10. ISBN 978-92-9090-532-5. 
  69. ^ Washitani, Izumi (2008). "Restoration of Biologically-Diverse Floodplain Wetlands Including Paddy Fields". Global Environmental Research. 12: 95–99. 
  70. ^ Simaika, John P.; Samways, Michael J.; Kipping, Jens; Suhling, Frank; Dijkstra, Klaas-Douwe B.; Clausnitzer, Viola; Boudot, Jean Pierre; Domisch, Sami (2013). "Continental-Scale Conservation Prioritization of African Dragonflies". Biological Conservation. 157: 245–254. doi:10.1016/j.biocon.2012.08.039. 
  71. ^ Soluk, Daniel A.; Zercher, Deanna S.; Worthington, Amy M. (2011). "Influence of roadways on patterns of mortality and flight behavior of adult dragonflies near wetland areas". Biological Conservation. 144 (5): 1638–1643. doi:10.1016/j.biocon.2011.02.015. 
  72. ^ Horvath, Gabor; Blaho, Miklos; Egri, Adam; Kriska, Gyorgy; Seres, Istvan; Robertson, Bruce (2010). "Reducing the Maladaptive Attractiveness of Solar Panels to Polarotactic Insects". Conservation Biology. 24 (6): 1644–1653. doi:10.1111/j.1523-1739.2010.01518.x. PMID 20455911. 
  73. ^ Horvath, Gabor; Malik, Peter; Kriska, Gyorgy; Wildermuth, Hansruedi (2007). "Ecological traps for dragonflies in a cemetery: the attraction of Sympetrum species (Odonata: Libellulidae)by horizontally polarizing black gravestones". Freshwater Biology. 52: 1700–1709. doi:10.1111/j.1365-2427.2007.01798.x. 
  74. ^ "Beads UC7549". Petrie Museum Catalogue. The Petrie Museum, UCL. Retrieved 10 June 2015.  There is a photograph in the catalogue; it is free for non-commercial usage.
  75. ^ a b c Mitchell, Forrest L.; Lasswell, James L. (2005). A Dazzle of Dragonflies. College Station, TX: Texas A&M University Press. ISBN 1-58544-459-6. 
  76. ^ Corbet 1999, p. 559.
  77. ^ Lehmann, Tracy Hobson (19 June 2008). "Dragonflying: the new birding". San Antonio Express-News. 
  78. ^ Moonan, Wendy (August 13, 1999). "Dragonflies Shimmering as Jewelry". New York Times. pp. E2:38. 
  79. ^ Large, Elizabeth (June 27, 1999). "The latest buzz; In the world of design, dragonflies are flying high". The Sun (Baltimore, MD). pp. 6N. 
  80. ^ Brown, Roland (November–December 2007). "1955 Douglas Dragonfly". Motorcycle Classics. Retrieved 2009-08-10. 
  81. ^ Nussbaum, Louis Frédéric; Käthe Roth (2005). "Akitsushima". Japan Encyclopedia. Cambridge: Harvard University Press. p. 20. 
  82. ^ Nihonto
  83. ^ 杉浦洋一 (Youichi Sugiura); John K. Gillespie (ジョン・K・ギレスピー) (1999). 日本文化を英語で紹介する事典: A Bilingual Handbook on Japanese Culture (in Japanese and English). 日本国東京都千代田区 (Chiyoda, JP-13): 株式会社ナツメ社 (Kabushiki gaisha Natsume Group). p. 305. ISBN 4-8163-2646-4. Retrieved 2010-04-26. 
  84. ^ Baird, Merrily (2001). Symbols of Japan: Thematic Motifs in Art and Design. New York: Rizzoli. pp. 108–9. ISBN 0-8478-2361-X. 
  85. ^ Trueman, John W. H.; Rowe, Richard J. "Odonata: Dragonflies and Damselflies". Tree of Life. Retrieved 27 February 2015. 
  86. ^ a b Corbet 1999, pp. 559–561.
  87. ^ Hand, Wayland D. (1973). "From Idea to Word: Folk Beliefs and Customs Underlying Folk Speech". American Speech. 48 (1/2): 67–76. doi:10.2307/3087894. JSTOR 3087894. 
  88. ^ a b Orr, Albert G.; Hämäläinen, Matti (July 2014). "Plagiarism or pragmatism – who cares? An analysis of some 18th century dragonfly illustrations" (PDF). Agrion. 18 (2): 26–30. 
  89. ^ a b Waldbauer, Gilbert; Waldbauer, Gilbert (30 June 2009). A Walk around the Pond: insects in and over the water. Harvard University Press. p. 247. ISBN 978-0-674-04477-7. 
  90. ^ Mitchell, Forrest Lee; Lasswell, James (2005). A Dazzle Of Dragonflies. Texas A&M University Press. p. 36. ISBN 978-1-58544-459-5. 
  91. ^ Tennyson, Alfred, Lord (17 November 2013). Delphi Complete Works of Alfred, Lord Tennyson (Illustrated). Delphi Classics. pp. 544–545. ISBN 978-1-909496-24-8. 
  92. ^ "Down the River". H. E. Bates Companion. Retrieved 27 February 2015. 
  93. ^ Powell 1999, p. 7.
  94. ^ Bates, H. E. (12 February 1937). "Country Life: Pike and Dragonflies". The Spectator (5668): 269 (online p. 17). 
  95. ^ "Equipping Insects for Special Service". Draper. 19 January 2017. 
  96. ^ Ackerman, Evan (1 June 2017). "Draper's Genetically Modified Cyborg DragonflEye Takes Flight". IEEE Spectrum. 

Further reading



This article uses material from the Wikipedia article "", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Animals

3D,data,libary,model,catalog,rendering,skull,bone,animal,reptile,bird,insect,mammal,class,classification,order,family,species,genus